ON THIS PAGE

  • Depth Crop Control
  • Similar samples:
  • Demo
  • Setup
  • Source code
  • Pipeline

Depth Crop Control

This example shows usage of depth camera in crop mode with the possibility to move the crop. You can manipulate the movement of the cropped frame by using the following keys:
  • w will move the crop up
  • a will move the crop left
  • s will move the crop down
  • d will move the crop right

Similar samples:

Demo

Setup

This example requires the DepthAI v3 API, see installation instructions.

Source code

Python
C++

Python

Python
GitHub
1#!/usr/bin/env python3
2
3"""
4This example shows usage of depth camera in crop mode with the possibility to move the crop.
5Use 'WASD' in order to do it.
6"""
7
8import cv2
9import depthai as dai
10import numpy as np
11
12# Step size ('W','A','S','D' controls)
13stepSize = 0.02
14
15# Create pipeline
16pipeline = dai.Pipeline()
17
18# Define sources and outputs
19monoRight = pipeline.create(dai.node.MonoCamera)
20monoLeft = pipeline.create(dai.node.MonoCamera)
21manip = pipeline.create(dai.node.ImageManip)
22stereo = pipeline.create(dai.node.StereoDepth)
23
24configIn = pipeline.create(dai.node.XLinkIn)
25xout = pipeline.create(dai.node.XLinkOut)
26
27configIn.setStreamName('config')
28xout.setStreamName("depth")
29
30# Crop range
31topLeft = dai.Point2f(0.2, 0.2)
32bottomRight = dai.Point2f(0.8, 0.8)
33
34# Properties
35monoRight.setCamera("right")
36monoLeft.setCamera("left")
37monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
38monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
39
40manip.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
41manip.setMaxOutputFrameSize(monoRight.getResolutionHeight()*monoRight.getResolutionWidth()*3)
42stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
43stereo.setSubpixel(True)
44
45# Linking
46configIn.out.link(manip.inputConfig)
47stereo.depth.link(manip.inputImage)
48manip.out.link(xout.input)
49monoRight.out.link(stereo.right)
50monoLeft.out.link(stereo.left)
51
52# Connect to device and start pipeline
53with dai.Device(pipeline) as device:
54
55    # Queues
56    q = device.getOutputQueue(xout.getStreamName(), maxSize=4, blocking=False)
57    configQueue = device.getInputQueue(configIn.getStreamName())
58
59    sendCamConfig = False
60
61    while True:
62        inDepth = q.get()
63        depthFrame = inDepth.getFrame() # depthFrame values are in millimeters
64
65        # Frame is transformed, the color map will be applied to highlight the depth info
66        depth_downscaled = depthFrame[::4]
67        if np.all(depth_downscaled == 0):
68            min_depth = 0  # Set a default minimum depth value when all elements are zero
69        else:
70            min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1)
71        max_depth = np.percentile(depth_downscaled, 99)
72        depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8)
73        depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT)
74
75        # Frame is ready to be shown
76        cv2.imshow("depth", depthFrameColor)
77
78        # Update screen
79        key = cv2.waitKey(10)
80        if key == ord('q'):
81            break
82        elif key == ord('w'):
83            if topLeft.y - stepSize >= 0:
84                topLeft.y -= stepSize
85                bottomRight.y -= stepSize
86                sendCamConfig = True
87        elif key == ord('a'):
88            if topLeft.x - stepSize >= 0:
89                topLeft.x -= stepSize
90                bottomRight.x -= stepSize
91                sendCamConfig = True
92        elif key == ord('s'):
93            if bottomRight.y + stepSize <= 1:
94                topLeft.y += stepSize
95                bottomRight.y += stepSize
96                sendCamConfig = True
97        elif key == ord('d'):
98            if bottomRight.x + stepSize <= 1:
99                topLeft.x += stepSize
100                bottomRight.x += stepSize
101                sendCamConfig = True
102
103        # Send new config to camera
104        if sendCamConfig:
105            cfg = dai.ImageManipConfig()
106            cfg.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
107            configQueue.send(cfg)
108            sendCamConfig = False

Pipeline

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.