Depth Post-Processing
This example shows how you can run depth post-processing filters on the device itself to reduce noise, smooth the depth map and overall improve the depth map quality. Post-processing can be added to StereoDepth node.Demo

Depth filters
Median
This is a non-edge preserving Median filter, which can be used to reduce noise and smoothen the depth map. Median filter is implemented in hardware, so it's the fastest filter.class
depthai.StereoDepthConfig.MedianFilter
variable
variable
variable
variable
variable
method
method
method
method
method
method
method
method
method
method
property
property
Speckle
Speckle Filter is used to reduce the speckle noise. Speckle noise is a region with huge variance between neighboring disparity/depth pixels, and speckle filter tries to filter this region.class
depthai.StereoDepthConfig.PostProcessing.SpeckleFilter
method
method
property
differenceThreshold
Maximum difference between neighbor disparity pixels to put them into the same blob. Units in disparity integer levels.
method
property
enable
Whether to enable or disable the filter.
method
property
speckleRange
Speckle search range.
method
Temporal
Temporal Filter is intended to improve the depth data persistency by manipulating per-pixel values based on previous frames. The filter performs a single pass on the data, adjusting the depth values while also updating the tracking history. In cases where the pixel data is missing or invalid, the filter uses a user-defined persistency mode to decide whether the missing value should be rectified with stored data. Note that due to its reliance on historic data, the filter may introduce visible blurring/smearing artifacts, and therefore is best-suited for static scenes.class
depthai.StereoDepthConfig.PostProcessing.TemporalFilter
class
PersistencyMode
Persistency algorithm type. Members: PERSISTENCY_OFF : VALID_8_OUT_OF_8 : VALID_2_IN_LAST_3 : VALID_2_IN_LAST_4 : VALID_2_OUT_OF_8 : VALID_1_IN_LAST_2 : VALID_1_IN_LAST_5 : VALID_1_IN_LAST_8 : PERSISTENCY_INDEFINITELY :
method
method
property
alpha
The Alpha factor in an exponential moving average with Alpha=1 - no filter. Alpha = 0 - infinite filter. Determines the extent of the temporal history that should be averaged.
method
property
delta
Step-size boundary. Establishes the threshold used to preserve surfaces (edges). If the disparity value between neighboring pixels exceed the disparity threshold set by this delta parameter, then filtering will be temporarily disabled. Default value 0 means auto: 3 disparity integer levels. In case of subpixel mode it's 3*number of subpixel levels.
method
property
enable
Whether to enable or disable the filter.
method
property
persistencyMode
Persistency mode. If the current disparity/depth value is invalid, it will be replaced by an older value, based on persistency mode.
method
class
depthai.StereoDepthConfig.PostProcessing.TemporalFilter.PersistencyMode
variable
variable
variable
variable
variable
variable
variable
variable
variable
variable
method
method
method
method
method
method
method
method
method
method
property
property
Spatial
Spatial Edge-Preserving Filter will fill invalid depth pixels with valid neighboring depth pixels. It performs a series of 1D horizontal and vertical passes or iterations, to enhance the smoothness of the reconstructed data. It is based on this research paper.class
depthai.StereoDepthConfig.PostProcessing.SpatialFilter
method
method
property
alpha
The Alpha factor in an exponential moving average with Alpha=1 - no filter. Alpha = 0 - infinite filter. Determines the amount of smoothing.
method
property
delta
Step-size boundary. Establishes the threshold used to preserve "edges". If the disparity value between neighboring pixels exceed the disparity threshold set by this delta parameter, then filtering will be temporarily disabled. Default value 0 means auto: 3 disparity integer levels. In case of subpixel mode it's 3*number of subpixel levels.
method
property
enable
Whether to enable or disable the filter.
method
property
holeFillingRadius
An in-place heuristic symmetric hole-filling mode applied horizontally during the filter passes. Intended to rectify minor artefacts with minimal performance impact. Search radius for hole filling.
method
property
numIterations
Number of iterations over the image in both horizontal and vertical direction.
method
Threshold
Threshold Filter filters out all disparity/depth pixels outside the configured min/max threshold values.Python
1class ThresholdFilter:
2'''
3 Spatial Edge-Preserving Filter will fill invalid depth pixels with valid neighboring depth pixels.
4 It performs a series of 1D horizontal and vertical passes or iterations, to enhance the smoothness of the reconstructed data. It is based on [this research paper](https://www.inf.ufrgs.br/~eslgastal/DomainTransform/).
5'''
Similar samples
Setup
This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5import numpy as np
6
7# Closer-in minimum depth, disparity range is doubled (from 95 to 190):
8extended_disparity = False
9# Better accuracy for longer distance, fractional disparity 32-levels:
10subpixel = False
11# Better handling for occlusions:
12lr_check = True
13
14# Create pipeline
15pipeline = dai.Pipeline()
16
17# Define sources and outputs
18monoLeft = pipeline.create(dai.node.MonoCamera)
19monoRight = pipeline.create(dai.node.MonoCamera)
20depth = pipeline.create(dai.node.StereoDepth)
21xout = pipeline.create(dai.node.XLinkOut)
22
23xout.setStreamName("disparity")
24
25# Properties
26monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
27monoLeft.setCamera("left")
28monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
29monoRight.setCamera("right")
30
31# Create a node that will produce the depth map (using disparity output as it's easier to visualize depth this way)
32depth.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
33# Options: MEDIAN_OFF, KERNEL_3x3, KERNEL_5x5, KERNEL_7x7 (default)
34depth.initialConfig.setMedianFilter(dai.MedianFilter.KERNEL_7x7)
35depth.setLeftRightCheck(lr_check)
36depth.setExtendedDisparity(extended_disparity)
37depth.setSubpixel(subpixel)
38
39config = depth.initialConfig.get()
40config.postProcessing.speckleFilter.enable = False
41config.postProcessing.speckleFilter.speckleRange = 50
42config.postProcessing.temporalFilter.enable = True
43config.postProcessing.spatialFilter.enable = True
44config.postProcessing.spatialFilter.holeFillingRadius = 2
45config.postProcessing.spatialFilter.numIterations = 1
46config.postProcessing.thresholdFilter.minRange = 400
47config.postProcessing.thresholdFilter.maxRange = 15000
48config.postProcessing.decimationFilter.decimationFactor = 1
49depth.initialConfig.set(config)
50
51# Linking
52monoLeft.out.link(depth.left)
53monoRight.out.link(depth.right)
54depth.disparity.link(xout.input)
55
56# Connect to device and start pipeline
57with dai.Device(pipeline) as device:
58
59 # Output queue will be used to get the disparity frames from the outputs defined above
60 q = device.getOutputQueue(name="disparity", maxSize=4, blocking=False)
61
62 while True:
63 inDisparity = q.get() # blocking call, will wait until a new data has arrived
64 frame = inDisparity.getFrame()
65 # Normalization for better visualization
66 frame = (frame * (255 / depth.initialConfig.getMaxDisparity())).astype(np.uint8)
67
68 cv2.imshow("disparity", frame)
69
70 # Available color maps: https://docs.opencv.org/3.4/d3/d50/group__imgproc__colormap.html
71 frame = cv2.applyColorMap(frame, cv2.COLORMAP_JET)
72 cv2.imshow("disparity_color", frame)
73
74 if cv2.waitKey(1) == ord('q'):
75 break
Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.