# Feature Tracker with Motion Estimation

This example demonstrates the capabilities of the
[FeatureTracker](https://docs.luxonis.com/software-v3/depthai/examples/feature_tracker/feature_tracker.md) combined with motion
estimation. It detects and tracks features between consecutive frames using optical flow. Each feature is assigned a unique ID.
The motion of the camera is estimated based on the tracked features, and the estimated motion (e.g., Up, Down, Left, Right,
Rotating) is displayed on screen.

The [Feature Detector](https://docs.luxonis.com/software-v3/depthai/examples/feature_detector.md) example only detects features
without estimating motion.

## Demo

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import numpy as np
import cv2
from collections import deque
import depthai as dai

class CameraMotionEstimator:
    def __init__(self, filter_weight=0.5, motion_threshold=0.01, rotation_threshold=0.05):
        self.last_avg_flow = np.array([0.0, 0.0])
        self.filter_weight = filter_weight
        self.motion_threshold = motion_threshold
        self.rotation_threshold = rotation_threshold

    def estimate_motion(self, feature_paths):
        most_prominent_motion = "Camera Staying Still"
        max_magnitude = 0.0
        avg_flow = np.array([0.0, 0.0])
        total_rotation = 0.0
        vanishing_point = np.array([0.0, 0.0])
        num_features = len(feature_paths)

        print(f"Number of features: {num_features}")

        if num_features == 0:
            return most_prominent_motion, vanishing_point

        for path in feature_paths.values():
            if len(path) >= 2:
                src = np.array([path[-2].x, path[-2].y])
                dst = np.array([path[-1].x, path[-1].y])
                avg_flow += dst - src
                motion_vector = dst + (dst - src)
                vanishing_point += motion_vector
                rotation = np.arctan2(dst[1] - src[1], dst[0] - src[0])
                total_rotation += rotation

        avg_flow /= num_features
        avg_rotation = total_rotation / num_features
        vanishing_point /= num_features

        print(f"Average Flow: {avg_flow}")
        print(f"Average Rotation: {avg_rotation}")

        avg_flow = (self.filter_weight * self.last_avg_flow +
                    (1 - self.filter_weight) * avg_flow)
        self.last_avg_flow = avg_flow

        flow_magnitude = np.linalg.norm(avg_flow)
        rotation_magnitude = abs(avg_rotation)

        if flow_magnitude > max_magnitude and flow_magnitude > self.motion_threshold:
            if abs(avg_flow[0]) > abs(avg_flow[1]):
                most_prominent_motion = 'Right' if avg_flow[0] < 0 else 'Left'
            else:
                most_prominent_motion = 'Down' if avg_flow[1] < 0 else 'Up'
            max_magnitude = flow_magnitude

        if rotation_magnitude > max_magnitude and rotation_magnitude > self.rotation_threshold:
            most_prominent_motion = 'Rotating'

        return most_prominent_motion, vanishing_point

class FeatureTrackerDrawer:

    lineColor = (200, 0, 200)
    pointColor = (0, 0, 255)
    vanishingPointColor = (255, 0, 255)  # Violet color for vanishing point
    circleRadius = 2
    maxTrackedFeaturesPathLength = 30
    trackedFeaturesPathLength = 10

    trackedIDs = None
    trackedFeaturesPath = None

    def trackFeaturePath(self, features):

        newTrackedIDs = set()
        for currentFeature in features:
            currentID = currentFeature.id
            newTrackedIDs.add(currentID)

            if currentID not in self.trackedFeaturesPath:
                self.trackedFeaturesPath[currentID] = deque()

            path = self.trackedFeaturesPath[currentID]
            path.append(currentFeature.position)

            while(len(path) > max(1, FeatureTrackerDrawer.trackedFeaturesPathLength)):
                path.popleft()

            self.trackedFeaturesPath[currentID] = path

        featuresToRemove = set()
        for oldId in self.trackedIDs:
            if oldId not in newTrackedIDs:
                featuresToRemove.add(oldId)

        for id in featuresToRemove:
            self.trackedFeaturesPath.pop(id)

        self.trackedIDs = newTrackedIDs

    def drawVanishingPoint(self, img, vanishing_point):
        cv2.circle(img, (int(vanishing_point[0]), int(vanishing_point[1])), self.circleRadius, self.vanishingPointColor, -1, cv2.LINE_AA, 0)

    # Define color mapping for directions
    direction_colors = {
        "Up": (0, 255, 255),  # Yellow
        "Down": (0, 255, 0),  # Green
        "Left": (255, 0, 0),  # Blue
        "Right": (0, 0, 255), # Red
    }

    def drawFeatures(self, img, vanishing_point=None, prominent_motion=None):

        # Get the appropriate point color based on the prominent motion
        if prominent_motion in self.direction_colors:
            point_color = self.direction_colors[prominent_motion]
        else:
            point_color = self.pointColor

        for featurePath in self.trackedFeaturesPath.values():
            path = featurePath

            for j in range(len(path) - 1):
                src = (int(path[j].x), int(path[j].y))
                dst = (int(path[j + 1].x), int(path[j + 1].y))
                cv2.line(img, src, dst, point_color, 1, cv2.LINE_AA, 0)

            j = len(path) - 1
            cv2.circle(img, (int(path[j].x), int(path[j].y)), self.circleRadius, point_color, -1, cv2.LINE_AA, 0)

        # Draw the direction text on the image
        if prominent_motion:
            font = cv2.FONT_HERSHEY_SIMPLEX
            font_scale = 1
            font_thickness = 2
            text_size = cv2.getTextSize(prominent_motion, font, font_scale, font_thickness)[0]
            text_x = (img.shape[1] - text_size[0]) // 2
            text_y = text_size[1] + 20  # 20 pixels from the top

            # Get the appropriate color based on the prominent motion
            text_color = self.direction_colors.get(prominent_motion, (255, 255, 255))  # Default to white

            # Draw the text
            cv2.putText(img, prominent_motion, (text_x, text_y), font, font_scale, text_color, font_thickness, cv2.LINE_AA)

        # Draw vanishing point if provided
        if vanishing_point is not None:
            self.drawVanishingPoint(img, vanishing_point)

    def __init__(self, windowName):
        self.windowName = windowName
        cv2.namedWindow(windowName)
        self.trackedIDs = set()
        self.trackedFeaturesPath = dict()

def create_pipeline():
    pipeline = dai.Pipeline()

    # Create a MonoCamera node and set its properties
    mono_left = pipeline.create(dai.node.MonoCamera)
    mono_left.setCamera("left")
    mono_left.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
    mono_left.setFps(15)

    # Create a FeatureTracker node
    feature_tracker_left = pipeline.create(dai.node.FeatureTracker)

    # Create XLinkOut nodes for output streams
    xout_tracked_features_left = pipeline.create(dai.node.XLinkOut)
    xout_passthrough_left = pipeline.create(dai.node.XLinkOut)

    # Set stream names
    xout_tracked_features_left.setStreamName("trackedFeaturesLeft")
    xout_passthrough_left.setStreamName("passthroughLeft")

    # Allocate resources for improved performance
    num_shaves = 2
    num_memory_slices = 2
    feature_tracker_left.setHardwareResources(num_shaves, num_memory_slices)

    # Link the nodes
    mono_left.out.link(feature_tracker_left.inputImage)
    feature_tracker_left.passthroughInputImage.link(xout_passthrough_left.input)
    feature_tracker_left.outputFeatures.link(xout_tracked_features_left.input)

    return pipeline

if __name__ == '__main__':
    pipeline = create_pipeline()
    with dai.Device(pipeline) as device:
        output_features_left_queue = device.getOutputQueue(
            "trackedFeaturesLeft", maxSize=4, blocking=False)
        passthrough_image_left_queue = device.getOutputQueue(
            "passthroughLeft", maxSize=4, blocking=False)

        left_window_name = "Left"
        left_feature_drawer = FeatureTrackerDrawer(left_window_name)
        camera_estimator_left = CameraMotionEstimator(
            filter_weight=0.5, motion_threshold=0.3, rotation_threshold=0.5)

        while True:
            in_passthrough_frame_left = passthrough_image_left_queue.get()
            passthrough_frame_left = in_passthrough_frame_left.getFrame()
            left_frame = cv2.cvtColor(passthrough_frame_left, cv2.COLOR_GRAY2BGR)

            tracked_features_left = output_features_left_queue.get().trackedFeatures
            motions_left, vanishing_pt_left = camera_estimator_left.estimate_motion(
                left_feature_drawer.trackedFeaturesPath)

            left_feature_drawer.trackFeaturePath(tracked_features_left)
            left_feature_drawer.drawFeatures(left_frame, vanishing_pt_left, motions_left)

            print("Motions:", motions_left)
            cv2.imshow(left_window_name, left_frame)

            if cv2.waitKey(1) == ord('q'):
                break
```

## Pipeline

### examples/feature_motion_estimation.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 1,
        "node2Input": "inputImage",
        "node2InputGroup": ""
      },
      {
        "node1Id": 1,
        "node1Output": "passthroughInputImage",
        "node1OutputGroup": "",
        "node2Id": 3,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 1,
        "node1Output": "outputFeatures",
        "node1OutputGroup": "",
        "node2Id": 2,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 1,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 2,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 3,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 4,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "MonoCamera",
          "properties": {
            "boardSocket": -1,
            "cameraName": "left",
            "fps": 15.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "isp3aFps": 0,
            "numFramesPool": 3,
            "numFramesPoolRaw": 3,
            "rawPacked": null,
            "resolution": 0
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "inputConfig"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 5,
                "name": "inputConfig",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "inputImage"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 6,
                "name": "inputImage",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": true
              }
            ],
            [
              [
                "",
                "outputFeatures"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 7,
                "name": "outputFeatures",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "passthroughInputImage"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 8,
                "name": "passthroughInputImage",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "FeatureTracker",
          "properties": {
            "initialConfig": {
              "cornerDetector": {
                "cellGridDimension": 4,
                "enableSobel": true,
                "enableSorting": true,
                "numMaxFeatures": 0,
                "numTargetFeatures": 320,
                "thresholds": {
                  "decreaseFactor": 0.8999999761581421,
                  "increaseFactor": 1.100000023841858,
                  "initialValue": 0.0,
                  "max": 0.0,
                  "min": 0.0
                },
                "type": 0
              },
              "featureMaintainer": {
                "enable": true,
                "lostFeatureErrorThreshold": 50000.0,
                "minimumDistanceBetweenFeatures": 50.0,
                "trackedFeatureThreshold": 200000.0
              },
              "motionEstimator": {
                "enable": true,
                "opticalFlow": {
                  "epsilon": 0.009999999776482582,
                  "maxIterations": 9,
                  "pyramidLevels": 0,
                  "searchWindowHeight": 5,
                  "searchWindowWidth": 5
                },
                "type": 0
              }
            },
            "numMemorySlices": 2,
            "numShaves": 2
          }
        }
      ],
      [
        2,
        {
          "id": 2,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 9,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "trackedFeaturesLeft"
          }
        }
      ],
      [
        3,
        {
          "id": 3,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 10,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "passthroughLeft"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.