OpenCV support
getFrame and getCvFrame.Demo
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6# Create pipeline
7pipeline = dai.Pipeline()
8
9# Define source and outputs
10camRgb = pipeline.create(dai.node.ColorCamera)
11xoutVideo = pipeline.create(dai.node.XLinkOut)
12xoutPreview = pipeline.create(dai.node.XLinkOut)
13
14xoutVideo.setStreamName("video")
15xoutPreview.setStreamName("preview")
16
17# Properties
18camRgb.setPreviewSize(300, 300)
19camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
20camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
21camRgb.setInterleaved(True)
22camRgb.setColorOrder(dai.ColorCameraProperties.ColorOrder.BGR)
23
24# Linking
25camRgb.video.link(xoutVideo.input)
26camRgb.preview.link(xoutPreview.input)
27
28# Connect to device and start pipeline
29with dai.Device(pipeline) as device:
30
31 video = device.getOutputQueue('video')
32 preview = device.getOutputQueue('preview')
33
34 while True:
35 videoFrame = video.get()
36 previewFrame = preview.get()
37
38 # Get BGR frame from NV12 encoded video frame to show with opencv
39 cv2.imshow("video", videoFrame.getCvFrame())
40 # Show 'preview' frame as is (already in correct format, no copy is made)
41 cv2.imshow("preview", previewFrame.getFrame())
42
43 if cv2.waitKey(1) == ord('q'):
44 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.