RGB Full Resolution Saver
.jpeg images when c key is pressed. It serves as an example of recording high resolution frames to disk for the purposes of high-resolution ground-truth data.Note that each frame consumes above 2MB of storage, so "spamming" capture key could fill up your storage.Similar samples:
Demo
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import time
4from pathlib import Path
5import cv2
6import depthai as dai
7
8# Create pipeline
9pipeline = dai.Pipeline()
10
11camRgb = pipeline.create(dai.node.ColorCamera)
12camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
13camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)
14
15xoutRgb = pipeline.create(dai.node.XLinkOut)
16xoutRgb.setStreamName("rgb")
17camRgb.video.link(xoutRgb.input)
18
19xin = pipeline.create(dai.node.XLinkIn)
20xin.setStreamName("control")
21xin.out.link(camRgb.inputControl)
22
23# Properties
24videoEnc = pipeline.create(dai.node.VideoEncoder)
25videoEnc.setDefaultProfilePreset(1, dai.VideoEncoderProperties.Profile.MJPEG)
26camRgb.still.link(videoEnc.input)
27
28# Linking
29xoutStill = pipeline.create(dai.node.XLinkOut)
30xoutStill.setStreamName("still")
31videoEnc.bitstream.link(xoutStill.input)
32
33# Connect to device and start pipeline
34with dai.Device(pipeline) as device:
35
36 # Output queue will be used to get the rgb frames from the output defined above
37 qRgb = device.getOutputQueue(name="rgb", maxSize=30, blocking=False)
38 qStill = device.getOutputQueue(name="still", maxSize=30, blocking=True)
39 qControl = device.getInputQueue(name="control")
40
41 # Make sure the destination path is present before starting to store the examples
42 dirName = "rgb_data"
43 Path(dirName).mkdir(parents=True, exist_ok=True)
44
45 while True:
46 inRgb = qRgb.tryGet() # Non-blocking call, will return a new data that has arrived or None otherwise
47 if inRgb is not None:
48 frame = inRgb.getCvFrame()
49 # 4k / 4
50 frame = cv2.pyrDown(frame)
51 frame = cv2.pyrDown(frame)
52 cv2.imshow("rgb", frame)
53
54 if qStill.has():
55 fName = f"{dirName}/{int(time.time() * 1000)}.jpeg"
56 with open(fName, "wb") as f:
57 f.write(qStill.get().getData())
58 print('Image saved to', fName)
59
60 key = cv2.waitKey(1)
61 if key == ord('q'):
62 break
63 elif key == ord('c'):
64 ctrl = dai.CameraControl()
65 ctrl.setCaptureStill(True)
66 qControl.send(ctrl)
67 print("Sent 'still' event to the camera!")Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.