# RGB & Mono Encoding

This example shows how to set up the encoder node to encode the RGB camera and both grayscale cameras (of DepthAI/OAK-D) at the
same time. The RGB is set to 1920x1080 and the grayscale are set to 1280x720 each, all at 30FPS. Each encoded video stream is
transferred over XLINK and saved to a respective file.

Pressing Ctrl+C will stop the recording and then convert it using ffmpeg into an mp4 to make it playable. Note that ffmpeg will
need to be installed and runnable for the conversion to mp4 to succeed.

Be careful, this example saves encoded video to your host storage. So if you leave it running, you could fill up your storage on
your host.

### Similar samples:

 * [RGB Encoding](https://docs.luxonis.com/software-v3/depthai/examples/rgb_encoding.md)
 * [Encoding Max Limit](https://docs.luxonis.com/software-v3/depthai/examples/encoding_max_limit.md)
 * [RGB Encoding & YOLO](https://docs.luxonis.com/software-v3/depthai/examples/detection_network/detection_network.md)

## Demo

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import depthai as dai

# Create pipeline
pipeline = dai.Pipeline()

# Define sources and outputs
camRgb = pipeline.create(dai.node.ColorCamera)
monoLeft = pipeline.create(dai.node.MonoCamera)
monoRight = pipeline.create(dai.node.MonoCamera)
ve1 = pipeline.create(dai.node.VideoEncoder)
ve2 = pipeline.create(dai.node.VideoEncoder)
ve3 = pipeline.create(dai.node.VideoEncoder)

ve1Out = pipeline.create(dai.node.XLinkOut)
ve2Out = pipeline.create(dai.node.XLinkOut)
ve3Out = pipeline.create(dai.node.XLinkOut)

ve1Out.setStreamName('ve1Out')
ve2Out.setStreamName('ve2Out')
ve3Out.setStreamName('ve3Out')

# Properties
camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
monoLeft.setCamera("left")
monoRight.setCamera("right")
# Create encoders, one for each camera, consuming the frames and encoding them using H.264 / H.265 encoding
ve1.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H264_MAIN)
ve2.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H265_MAIN)
ve3.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H264_MAIN)

# Linking
monoLeft.out.link(ve1.input)
camRgb.video.link(ve2.input)
monoRight.out.link(ve3.input)
ve1.bitstream.link(ve1Out.input)
ve2.bitstream.link(ve2Out.input)
ve3.bitstream.link(ve3Out.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as dev:

    # Output queues will be used to get the encoded data from the outputs defined above
    outQ1 = dev.getOutputQueue(name='ve1Out', maxSize=30, blocking=True)
    outQ2 = dev.getOutputQueue(name='ve2Out', maxSize=30, blocking=True)
    outQ3 = dev.getOutputQueue(name='ve3Out', maxSize=30, blocking=True)

    # The .h264 / .h265 files are raw stream files (not playable yet)
    with open('mono1.h264', 'wb') as fileMono1H264, open('color.h265', 'wb') as fileColorH265, open('mono2.h264', 'wb') as fileMono2H264:
        print("Press Ctrl+C to stop encoding...")
        while True:
            try:
                # Empty each queue
                while outQ1.has():
                    outQ1.get().getData().tofile(fileMono1H264)

                while outQ2.has():
                    outQ2.get().getData().tofile(fileColorH265)

                while outQ3.has():
                    outQ3.get().getData().tofile(fileMono2H264)
            except KeyboardInterrupt:
                # Keyboard interrupt (Ctrl + C) detected
                break

    print("To view the encoded data, convert the stream file (.h264/.h265) into a video file (.mp4), using commands below:")
    cmd = "ffmpeg -framerate 30 -i {} -c copy {}"
    print(cmd.format("mono1.h264", "mono1.mp4"))
    print(cmd.format("mono2.h264", "mono2.mp4"))
    print(cmd.format("color.h265", "color.mp4"))
```

#### C++

```cpp
#include <csignal>
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

// Keyboard interrupt (Ctrl + C) detected
static std::atomic<bool> alive{true};
static void sigintHandler(int signum) {
    alive = false;
}

int main() {
    using namespace std;
    std::signal(SIGINT, &sigintHandler);

    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto monoLeft = pipeline.create<dai::node::MonoCamera>();
    auto monoRight = pipeline.create<dai::node::MonoCamera>();
    auto ve1 = pipeline.create<dai::node::VideoEncoder>();
    auto ve2 = pipeline.create<dai::node::VideoEncoder>();
    auto ve3 = pipeline.create<dai::node::VideoEncoder>();

    auto ve1Out = pipeline.create<dai::node::XLinkOut>();
    auto ve2Out = pipeline.create<dai::node::XLinkOut>();
    auto ve3Out = pipeline.create<dai::node::XLinkOut>();

    ve1Out->setStreamName("ve1Out");
    ve2Out->setStreamName("ve2Out");
    ve3Out->setStreamName("ve3Out");

    // Properties
    camRgb->setBoardSocket(dai::CameraBoardSocket::CAM_A);
    monoLeft->setCamera("left");
    monoRight->setCamera("right");
    // Create encoders, one for each camera, consuming the frames and encoding them using H.264 / H.265 encoding
    ve1->setDefaultProfilePreset(30, dai::VideoEncoderProperties::Profile::H264_MAIN);
    ve2->setDefaultProfilePreset(30, dai::VideoEncoderProperties::Profile::H265_MAIN);
    ve3->setDefaultProfilePreset(30, dai::VideoEncoderProperties::Profile::H264_MAIN);

    // Linking
    monoLeft->out.link(ve1->input);
    camRgb->video.link(ve2->input);
    monoRight->out.link(ve3->input);
    ve1->bitstream.link(ve1Out->input);
    ve2->bitstream.link(ve2Out->input);
    ve3->bitstream.link(ve3Out->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queues will be used to get the encoded data from the output defined above
    auto outQ1 = device.getOutputQueue("ve1Out", 30, true);
    auto outQ2 = device.getOutputQueue("ve2Out", 30, true);
    auto outQ3 = device.getOutputQueue("ve3Out", 30, true);

    // The .h264 / .h265 files are raw stream files (not playable yet)
    auto videoFile1 = std::ofstream("mono1.h264", std::ios::binary);
    auto videoFile2 = std::ofstream("color.h265", std::ios::binary);
    auto videoFile3 = std::ofstream("mono2.h264", std::ios::binary);
    cout << "Press Ctrl+C to stop encoding..." << endl;

    while(alive) {
        auto out1 = outQ1->get<dai::ImgFrame>();
        videoFile1.write((char*)out1->getData().data(), out1->getData().size());
        auto out2 = outQ2->get<dai::ImgFrame>();
        videoFile2.write((char*)out2->getData().data(), out2->getData().size());
        auto out3 = outQ3->get<dai::ImgFrame>();
        videoFile3.write((char*)out3->getData().data(), out3->getData().size());
    }

    cout << "To view the encoded data, convert the stream file (.h264/.h265) into a video file (.mp4), using a command below:" << endl;
    cout << "ffmpeg -framerate 30 -i mono1.h264 -c copy mono1.mp4" << endl;
    cout << "ffmpeg -framerate 30 -i mono2.h264 -c copy mono2.mp4" << endl;
    cout << "ffmpeg -framerate 30 -i color.h265 -c copy color.mp4" << endl;

    return 0;
}
```

## Pipeline

### examples/rgb_mono_encoding.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 1,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 3,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 0,
        "node1Output": "video",
        "node1OutputGroup": "",
        "node2Id": 4,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 2,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 5,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 3,
        "node1Output": "bitstream",
        "node1OutputGroup": "",
        "node2Id": 6,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 4,
        "node1Output": "bitstream",
        "node1OutputGroup": "",
        "node2Id": 7,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 5,
        "node1Output": "bitstream",
        "node1OutputGroup": "",
        "node2Id": 8,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "inputConfig"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 1,
                "name": "inputConfig",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 6,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "still"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 7,
                "name": "still",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "video"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 3,
                "name": "video",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "isp"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 4,
                "name": "isp",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "preview"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 5,
                "name": "preview",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 8,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "ColorCamera",
          "properties": {
            "boardSocket": 0,
            "cameraName": "",
            "colorOrder": 0,
            "fp16": false,
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "interleaved": true,
            "isp3aFps": 0,
            "ispScale": {
              "horizDenominator": 0,
              "horizNumerator": 0,
              "vertDenominator": 0,
              "vertNumerator": 0
            },
            "numFramesPoolIsp": 3,
            "numFramesPoolPreview": 4,
            "numFramesPoolRaw": 3,
            "numFramesPoolStill": 4,
            "numFramesPoolVideo": 4,
            "previewHeight": 300,
            "previewKeepAspectRatio": true,
            "previewWidth": 300,
            "rawPacked": null,
            "resolution": 0,
            "sensorCropX": -1.0,
            "sensorCropY": -1.0,
            "stillHeight": -1,
            "stillWidth": -1,
            "videoHeight": -1,
            "videoWidth": -1
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 9,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 10,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 11,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 12,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "MonoCamera",
          "properties": {
            "boardSocket": -1,
            "cameraName": "left",
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "isp3aFps": 0,
            "numFramesPool": 3,
            "numFramesPoolRaw": 3,
            "rawPacked": null,
            "resolution": 0
          }
        }
      ],
      [
        2,
        {
          "id": 2,
          "ioInfo": [
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 13,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 14,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 15,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 16,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "MonoCamera",
          "properties": {
            "boardSocket": -1,
            "cameraName": "right",
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "isp3aFps": 0,
            "numFramesPool": 3,
            "numFramesPoolRaw": 3,
            "rawPacked": null,
            "resolution": 0
          }
        }
      ],
      [
        3,
        {
          "id": 3,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 17,
                "name": "in",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": true
              }
            ],
            [
              [
                "",
                "bitstream"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 18,
                "name": "bitstream",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 19,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "VideoEncoder",
          "properties": {
            "bitrate": 0,
            "frameRate": 30.0,
            "keyframeFrequency": 30,
            "lossless": false,
            "maxBitrate": 0,
            "numBFrames": 0,
            "numFramesPool": 0,
            "outputFrameSize": 0,
            "profile": 2,
            "quality": 80,
            "rateCtrlMode": 0
          }
        }
      ],
      [
        4,
        {
          "id": 4,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 20,
                "name": "in",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": true
              }
            ],
            [
              [
                "",
                "bitstream"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 21,
                "name": "bitstream",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 22,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "VideoEncoder",
          "properties": {
            "bitrate": 0,
            "frameRate": 30.0,
            "keyframeFrequency": 30,
            "lossless": false,
            "maxBitrate": 0,
            "numBFrames": 0,
            "numFramesPool": 0,
            "outputFrameSize": 0,
            "profile": 3,
            "quality": 80,
            "rateCtrlMode": 0
          }
        }
      ],
      [
        5,
        {
          "id": 5,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 23,
                "name": "in",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": true
              }
            ],
            [
              [
                "",
                "bitstream"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 24,
                "name": "bitstream",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 25,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "VideoEncoder",
          "properties": {
            "bitrate": 0,
            "frameRate": 30.0,
            "keyframeFrequency": 30,
            "lossless": false,
            "maxBitrate": 0,
            "numBFrames": 0,
            "numFramesPool": 0,
            "outputFrameSize": 0,
            "profile": 2,
            "quality": 80,
            "rateCtrlMode": 0
          }
        }
      ],
      [
        6,
        {
          "id": 6,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 26,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "ve1Out"
          }
        }
      ],
      [
        7,
        {
          "id": 7,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 27,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "ve2Out"
          }
        }
      ],
      [
        8,
        {
          "id": 8,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 28,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "ve3Out"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.