Stereo Depth Align
This example shows how to align the stereo depth map to the RGB frame to get RGB-D frames.Demo

Source code
Python
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import numpy as np
4import cv2
5import depthai as dai
6import time
7from datetime import timedelta
8FPS = 25.0
9
10RGB_SOCKET = dai.CameraBoardSocket.CAM_A
11LEFT_SOCKET = dai.CameraBoardSocket.CAM_B
12RIGHT_SOCKET = dai.CameraBoardSocket.CAM_C
13
14class FPSCounter:
15 def __init__(self):
16 self.frameTimes = []
17
18 def tick(self):
19 now = time.time()
20 self.frameTimes.append(now)
21 self.frameTimes = self.frameTimes[-10:]
22
23 def getFps(self):
24 if len(self.frameTimes) <= 1:
25 return 0
26 return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])
27
28pipeline = dai.Pipeline()
29
30platform = pipeline.getDefaultDevice().getPlatform()
31
32# Define sources and outputs
33camRgb = pipeline.create(dai.node.Camera).build(RGB_SOCKET)
34left = pipeline.create(dai.node.Camera).build(LEFT_SOCKET)
35right = pipeline.create(dai.node.Camera).build(RIGHT_SOCKET)
36stereo = pipeline.create(dai.node.StereoDepth)
37sync = pipeline.create(dai.node.Sync)
38if platform == dai.Platform.RVC4:
39 align = pipeline.create(dai.node.ImageAlign)
40
41stereo.setExtendedDisparity(True)
42sync.setSyncThreshold(timedelta(seconds=1/(2*FPS)))
43
44rgbOut = camRgb.requestOutput(size = (1280, 960), fps = FPS, enableUndistortion=True)
45leftOut = left.requestOutput(size = (640, 400), fps = FPS)
46rightOut = right.requestOutput(size = (640, 400), fps = FPS)
47
48# Linking
49rgbOut.link(sync.inputs["rgb"])
50leftOut.link(stereo.left)
51rightOut.link(stereo.right)
52if platform == dai.Platform.RVC4:
53 stereo.depth.link(align.input)
54 rgbOut.link(align.inputAlignTo)
55 align.outputAligned.link(sync.inputs["depth_aligned"])
56else:
57 stereo.depth.link(sync.inputs["depth_aligned"])
58 rgbOut.link(stereo.inputAlignTo)
59
60queue = sync.out.createOutputQueue()
61
62def colorizeDepth(frameDepth):
63 invalidMask = frameDepth == 0
64 # Log the depth, minDepth and maxDepth
65 try:
66 minDepth = np.percentile(frameDepth[frameDepth != 0], 3)
67 maxDepth = np.percentile(frameDepth[frameDepth != 0], 95)
68 logDepth = np.log(frameDepth, where=frameDepth != 0)
69 logMinDepth = np.log(minDepth)
70 logMaxDepth = np.log(maxDepth)
71 np.nan_to_num(logDepth, copy=False, nan=logMinDepth)
72 # Clip the values to be in the 0-255 range
73 logDepth = np.clip(logDepth, logMinDepth, logMaxDepth)
74
75 # Interpolate only valid logDepth values, setting the rest based on the mask
76 depthFrameColor = np.interp(logDepth, (logMinDepth, logMaxDepth), (0, 255))
77 depthFrameColor = np.nan_to_num(depthFrameColor)
78 depthFrameColor = depthFrameColor.astype(np.uint8)
79 depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_JET)
80 # Set invalid depth pixels to black
81 depthFrameColor[invalidMask] = 0
82 except IndexError:
83 # Frame is likely empty
84 depthFrameColor = np.zeros((frameDepth.shape[0], frameDepth.shape[1], 3), dtype=np.uint8)
85 except Exception as e:
86 raise e
87 return depthFrameColor
88
89
90rgbWeight = 0.4
91depthWeight = 0.6
92
93
94def updateBlendWeights(percentRgb):
95 """
96 Update the rgb and depth weights used to blend depth/rgb image
97
98 @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
99 """
100 global depthWeight
101 global rgbWeight
102 rgbWeight = float(percentRgb) / 100.0
103 depthWeight = 1.0 - rgbWeight
104
105
106# Connect to device and start pipeline
107with pipeline:
108 pipeline.start()
109
110 # Configure windows; trackbar adjusts blending ratio of rgb/depth
111 windowName = "rgb-depth"
112
113 # Set the window to be resizable and the initial size
114 cv2.namedWindow(windowName, cv2.WINDOW_NORMAL)
115 cv2.resizeWindow(windowName, 1280, 720)
116 cv2.createTrackbar(
117 "RGB Weight %",
118 windowName,
119 int(rgbWeight * 100),
120 100,
121 updateBlendWeights,
122 )
123 fpsCounter = FPSCounter()
124 while True:
125 messageGroup = queue.get()
126 fpsCounter.tick()
127 assert isinstance(messageGroup, dai.MessageGroup)
128 frameRgb = messageGroup["rgb"]
129 assert isinstance(frameRgb, dai.ImgFrame)
130 frameDepth = messageGroup["depth_aligned"]
131 assert isinstance(frameDepth, dai.ImgFrame)
132
133 # Blend when both received
134 if frameDepth is not None:
135 cvFrame = frameRgb.getCvFrame()
136 # Colorize the aligned depth
137 alignedDepthColorized = colorizeDepth(frameDepth.getFrame())
138 # Resize depth to match the rgb frame
139 cv2.imshow("Depth aligned", alignedDepthColorized)
140
141 if len(cvFrame.shape) == 2:
142 cvFrameUndistorted = cv2.cvtColor(cvFrame, cv2.COLOR_GRAY2BGR)
143 blended = cv2.addWeighted(
144 cvFrame, rgbWeight, alignedDepthColorized, depthWeight, 0
145 )
146 cv2.putText(
147 blended,
148 f"FPS: {fpsCounter.getFps():.2f}",
149 (10, 30),
150 cv2.FONT_HERSHEY_SIMPLEX,
151 1,
152 (255, 255, 255),
153 2,
154 )
155 cv2.imshow(windowName, blended)
156
157 key = cv2.waitKey(1)
158 if key == ord("q"):
159 break
Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.