Stereo Depth Video
withDepth: if you turn it off it will became Mono Preview, so it will show only the 2 mono camerasoutputDepth: if you turn it on it will show the depthlrcheck: used for better occlusion handling. For more information click hereextended: suitable for short range objects. For more information click heresubpixel: suitable for long range. For more information click here
Stereo Alpha Param
--alpha you can select scaling during the rectification. Values between 0 and 1:- 0.0 (default value) means that the rectified images are zoomed and shifted so that only valid pixels are visible (no black areas after rectification)
- 1.0 means that the rectified image is decimated and shifted so that all the pixels from the original images from the cameras are retained in the rectified images (no source image pixels are lost).
Similar samples:
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import numpy as np
5import depthai as dai
6import argparse
7
8parser = argparse.ArgumentParser()
9parser.add_argument(
10 "-res",
11 "--resolution",
12 type=str,
13 default="720",
14 help="Sets the resolution on mono cameras. Options: 800 | 720 | 400",
15)
16parser.add_argument(
17 "-md",
18 "--mesh_dir",
19 type=str,
20 default=None,
21 help="Output directory for mesh files. If not specified mesh files won't be saved",
22)
23parser.add_argument(
24 "-lm",
25 "--load_mesh",
26 default=False,
27 action="store_true",
28 help="Read camera intrinsics, generate mesh files and load them into the stereo node.",
29)
30parser.add_argument(
31 "-rect",
32 "--out_rectified",
33 default=False,
34 action="store_true",
35 help="Generate and display rectified streams",
36)
37parser.add_argument(
38 "-lr",
39 "--lrcheck",
40 default=False,
41 action="store_true",
42 help="Better handling for occlusions",
43)
44parser.add_argument(
45 "-e",
46 "--extended",
47 default=False,
48 action="store_true",
49 help="Closer-in minimum depth, disparity range is doubled",
50)
51parser.add_argument(
52 "-s",
53 "--subpixel",
54 default=False,
55 action="store_true",
56 help="Better accuracy for longer distance, fractional disparity 32-levels",
57)
58parser.add_argument(
59 "-m",
60 "--median",
61 type=str,
62 default="7x7",
63 help="Choose the size of median filtering. Options: OFF | 3x3 | 5x5 | 7x7 (default)",
64)
65parser.add_argument(
66 "-d",
67 "--depth",
68 default=False,
69 action="store_true",
70 help="Display depth frames",
71)
72parser.add_argument(
73 "-swlr",
74 "--swap_left_right",
75 default=False,
76 action="store_true",
77 help="Swap left right frames",
78)
79parser.add_argument(
80 "-a",
81 "--alpha",
82 type=float,
83 default=None,
84 help="Alpha scaling parameter to increase FOV",
85)
86args = parser.parse_args()
87
88RES_MAP = {
89 '800': {'w': 1280, 'h': 800, 'res': dai.MonoCameraProperties.SensorResolution.THE_800_P },
90 '720': {'w': 1280, 'h': 720, 'res': dai.MonoCameraProperties.SensorResolution.THE_720_P },
91 '400': {'w': 640, 'h': 400, 'res': dai.MonoCameraProperties.SensorResolution.THE_400_P }
92}
93if args.resolution not in RES_MAP:
94 exit("Unsupported resolution!")
95
96resolution = RES_MAP[args.resolution]
97
98meshDirectory = args.mesh_dir # Output dir for mesh files
99generateMesh = args.load_mesh # Load mesh files
100
101outRectified = args.out_rectified # Output and display rectified streams
102lrcheck = args.lrcheck # Better handling for occlusions
103extended = args.extended # Closer-in minimum depth, disparity range is doubled
104subpixel = args.subpixel # Better accuracy for longer distance, fractional disparity 32-levels
105depth = args.depth # Display depth frames
106
107medianMap = {
108 "OFF": dai.StereoDepthProperties.MedianFilter.MEDIAN_OFF,
109 "3x3": dai.StereoDepthProperties.MedianFilter.KERNEL_3x3,
110 "5x5": dai.StereoDepthProperties.MedianFilter.KERNEL_5x5,
111 "7x7": dai.StereoDepthProperties.MedianFilter.KERNEL_7x7,
112}
113if args.median not in medianMap:
114 exit("Unsupported median size!")
115
116median = medianMap[args.median]
117
118print("StereoDepth config options:")
119print(f" Resolution: {resolution['w']}x{resolution['h']}")
120print(" Left-Right check: ", lrcheck)
121print(" Extended disparity:", extended)
122print(" Subpixel: ", subpixel)
123print(" Median filtering: ", median)
124print(" Generating mesh files: ", generateMesh)
125print(" Outputting mesh files to: ", meshDirectory)
126
127
128def getMesh(calibData):
129 M1 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_B, resolution[0], resolution[1]))
130 d1 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_B))
131 R1 = np.array(calibData.getStereoLeftRectificationRotation())
132 M2 = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_C, resolution[0], resolution[1]))
133 d2 = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_C))
134 R2 = np.array(calibData.getStereoRightRectificationRotation())
135 mapXL, mapYL = cv2.initUndistortRectifyMap(M1, d1, R1, M2, resolution, cv2.CV_32FC1)
136 mapXR, mapYR = cv2.initUndistortRectifyMap(M2, d2, R2, M2, resolution, cv2.CV_32FC1)
137
138 meshCellSize = 16
139 meshLeft = []
140 meshRight = []
141
142 for y in range(mapXL.shape[0] + 1):
143 if y % meshCellSize == 0:
144 rowLeft = []
145 rowRight = []
146 for x in range(mapXL.shape[1] + 1):
147 if x % meshCellSize == 0:
148 if y == mapXL.shape[0] and x == mapXL.shape[1]:
149 rowLeft.append(mapYL[y - 1, x - 1])
150 rowLeft.append(mapXL[y - 1, x - 1])
151 rowRight.append(mapYR[y - 1, x - 1])
152 rowRight.append(mapXR[y - 1, x - 1])
153 elif y == mapXL.shape[0]:
154 rowLeft.append(mapYL[y - 1, x])
155 rowLeft.append(mapXL[y - 1, x])
156 rowRight.append(mapYR[y - 1, x])
157 rowRight.append(mapXR[y - 1, x])
158 elif x == mapXL.shape[1]:
159 rowLeft.append(mapYL[y, x - 1])
160 rowLeft.append(mapXL[y, x - 1])
161 rowRight.append(mapYR[y, x - 1])
162 rowRight.append(mapXR[y, x - 1])
163 else:
164 rowLeft.append(mapYL[y, x])
165 rowLeft.append(mapXL[y, x])
166 rowRight.append(mapYR[y, x])
167 rowRight.append(mapXR[y, x])
168 if (mapXL.shape[1] % meshCellSize) % 2 != 0:
169 rowLeft.append(0)
170 rowLeft.append(0)
171 rowRight.append(0)
172 rowRight.append(0)
173
174 meshLeft.append(rowLeft)
175 meshRight.append(rowRight)
176
177 meshLeft = np.array(meshLeft)
178 meshRight = np.array(meshRight)
179
180 return meshLeft, meshRight
181
182
183def saveMeshFiles(meshLeft, meshRight, outputPath):
184 print("Saving mesh to:", outputPath)
185 meshLeft.tofile(outputPath + "/left_mesh.calib")
186 meshRight.tofile(outputPath + "/right_mesh.calib")
187
188
189def getDisparityFrame(frame, cvColorMap):
190 maxDisp = stereo.initialConfig.getMaxDisparity()
191 disp = (frame * (255.0 / maxDisp)).astype(np.uint8)
192 disp = cv2.applyColorMap(disp, cvColorMap)
193
194 return disp
195
196device = dai.Device()
197calibData = device.readCalibration()
198print("Creating Stereo Depth pipeline")
199pipeline = dai.Pipeline()
200
201camLeft = pipeline.create(dai.node.MonoCamera)
202camRight = pipeline.create(dai.node.MonoCamera)
203stereo = pipeline.create(dai.node.StereoDepth)
204xoutLeft = pipeline.create(dai.node.XLinkOut)
205xoutRight = pipeline.create(dai.node.XLinkOut)
206xoutDisparity = pipeline.create(dai.node.XLinkOut)
207xoutDepth = pipeline.create(dai.node.XLinkOut)
208xoutRectifLeft = pipeline.create(dai.node.XLinkOut)
209xoutRectifRight = pipeline.create(dai.node.XLinkOut)
210
211if args.swap_left_right:
212 camLeft.setCamera("right")
213 camRight.setCamera("left")
214else:
215 camLeft.setCamera("left")
216 camRight.setCamera("right")
217
218for monoCam in (camLeft, camRight): # Common config
219 monoCam.setResolution(resolution['res'])
220 # monoCam.setFps(20.0)
221
222stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
223stereo.initialConfig.setMedianFilter(median) # KERNEL_7x7 default
224stereo.setRectifyEdgeFillColor(0) # Black, to better see the cutout
225stereo.setLeftRightCheck(lrcheck)
226stereo.setExtendedDisparity(extended)
227stereo.setSubpixel(subpixel)
228if args.alpha is not None:
229 stereo.setAlphaScaling(args.alpha)
230 config = stereo.initialConfig.get()
231 config.postProcessing.brightnessFilter.minBrightness = 0
232 stereo.initialConfig.set(config)
233
234xoutLeft.setStreamName("left")
235xoutRight.setStreamName("right")
236xoutDisparity.setStreamName("disparity")
237xoutDepth.setStreamName("depth")
238xoutRectifLeft.setStreamName("rectifiedLeft")
239xoutRectifRight.setStreamName("rectifiedRight")
240
241camLeft.out.link(stereo.left)
242camRight.out.link(stereo.right)
243stereo.syncedLeft.link(xoutLeft.input)
244stereo.syncedRight.link(xoutRight.input)
245stereo.disparity.link(xoutDisparity.input)
246if depth:
247 stereo.depth.link(xoutDepth.input)
248if outRectified:
249 stereo.rectifiedLeft.link(xoutRectifLeft.input)
250 stereo.rectifiedRight.link(xoutRectifRight.input)
251
252streams = ["left", "right"]
253if outRectified:
254 streams.extend(["rectifiedLeft", "rectifiedRight"])
255streams.append("disparity")
256if depth:
257 streams.append("depth")
258
259cvColorMap = cv2.applyColorMap(np.arange(256, dtype=np.uint8), cv2.COLORMAP_JET)
260cvColorMap[0] = [0, 0, 0]
261print("Creating DepthAI device")
262with device:
263 device.startPipeline(pipeline)
264
265 # Create a receive queue for each stream
266 qList = [device.getOutputQueue(stream, 8, blocking=False) for stream in streams]
267
268 while True:
269 for q in qList:
270 name = q.getName()
271 frame = q.get().getCvFrame()
272 if name == "depth":
273 frame = frame.astype(np.uint16)
274 elif name == "disparity":
275 frame = getDisparityFrame(frame, cvColorMap)
276
277 cv2.imshow(name, frame)
278 if cv2.waitKey(1) == ord("q"):
279 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.