RGB-ToF Align
Demo
This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import numpy as np
4import cv2
5import depthai as dai
6import time
7from datetime import timedelta
8
9# This example is intended to run unchanged on an OAK-D-SR-PoE camera
10FPS = 30.0
11
12RGB_SOCKET = dai.CameraBoardSocket.CAM_C
13TOF_SOCKET = dai.CameraBoardSocket.CAM_A
14ALIGN_SOCKET = RGB_SOCKET
15
16class FPSCounter:
17 def __init__(self):
18 self.frameTimes = []
19
20 def tick(self):
21 now = time.time()
22 self.frameTimes.append(now)
23 self.frameTimes = self.frameTimes[-100:]
24
25 def getFps(self):
26 if len(self.frameTimes) <= 1:
27 return 0
28 # Calculate the FPS
29 return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])
30
31
32ISP_SCALE = 2
33
34device = dai.Device()
35
36calibrationHandler = device.readCalibration()
37rgbDistortion = calibrationHandler.getDistortionCoefficients(RGB_SOCKET)
38distortionModel = calibrationHandler.getDistortionModel(RGB_SOCKET)
39if distortionModel != dai.CameraModel.Perspective:
40 raise RuntimeError("Unsupported distortion model for RGB camera. This example supports only Perspective model.")
41
42pipeline = dai.Pipeline()
43
44# Define sources and outputs
45camRgb = pipeline.create(dai.node.ColorCamera)
46tof = pipeline.create(dai.node.ToF)
47camTof = pipeline.create(dai.node.Camera)
48sync = pipeline.create(dai.node.Sync)
49align = pipeline.create(dai.node.ImageAlign)
50out = pipeline.create(dai.node.XLinkOut)
51
52# ToF settings
53camTof.setFps(FPS)
54camTof.setImageOrientation(dai.CameraImageOrientation.ROTATE_180_DEG)
55camTof.setBoardSocket(TOF_SOCKET)
56
57# rgb settings
58camRgb.setBoardSocket(RGB_SOCKET)
59camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_800_P)
60camRgb.setFps(FPS)
61camRgb.setIspScale(1, ISP_SCALE)
62
63out.setStreamName("out")
64
65sync.setSyncThreshold(timedelta(seconds=0.5 / FPS))
66
67# Linking
68camRgb.isp.link(sync.inputs["rgb"])
69camTof.raw.link(tof.input)
70tof.depth.link(align.input)
71align.outputAligned.link(sync.inputs["depth_aligned"])
72sync.inputs["rgb"].setBlocking(False)
73camRgb.isp.link(align.inputAlignTo)
74sync.out.link(out.input)
75
76def colorizeDepth(frameDepth):
77 invalidMask = frameDepth == 0
78 # Log the depth, minDepth and maxDepth
79 try:
80 minDepth = np.percentile(frameDepth[frameDepth != 0], 3)
81 maxDepth = np.percentile(frameDepth[frameDepth != 0], 95)
82 logDepth = np.log(frameDepth, where=frameDepth != 0)
83 logMinDepth = np.log(minDepth)
84 logMaxDepth = np.log(maxDepth)
85 np.nan_to_num(logDepth, copy=False, nan=logMinDepth)
86 # Clip the values to be in the 0-255 range
87 logDepth = np.clip(logDepth, logMinDepth, logMaxDepth)
88
89 # Interpolate only valid logDepth values, setting the rest based on the mask
90 depthFrameColor = np.interp(logDepth, (logMinDepth, logMaxDepth), (0, 255))
91 depthFrameColor = np.nan_to_num(depthFrameColor)
92 depthFrameColor = depthFrameColor.astype(np.uint8)
93 depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_JET)
94 # Set invalid depth pixels to black
95 depthFrameColor[invalidMask] = 0
96 except IndexError:
97 # Frame is likely empty
98 depthFrameColor = np.zeros((frameDepth.shape[0], frameDepth.shape[1], 3), dtype=np.uint8)
99 except Exception as e:
100 raise e
101 return depthFrameColor
102
103
104rgbWeight = 0.4
105depthWeight = 0.6
106
107
108def updateBlendWeights(percentRgb):
109 """
110 Update the rgb and depth weights used to blend depth/rgb image
111
112 @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
113 """
114 global depthWeight
115 global rgbWeight
116 rgbWeight = float(percentRgb) / 100.0
117 depthWeight = 1.0 - rgbWeight
118
119
120
121# Connect to device and start pipeline
122with device:
123 device.startPipeline(pipeline)
124 queue = device.getOutputQueue("out", 8, False)
125
126 # Configure windows; trackbar adjusts blending ratio of rgb/depth
127 rgbDepthWindowName = "rgb-depth"
128
129 cv2.namedWindow(rgbDepthWindowName)
130 cv2.createTrackbar(
131 "RGB Weight %",
132 rgbDepthWindowName,
133 int(rgbWeight * 100),
134 100,
135 updateBlendWeights,
136 )
137 fpsCounter = FPSCounter()
138 while True:
139 messageGroup = queue.get()
140 fpsCounter.tick()
141 assert isinstance(messageGroup, dai.MessageGroup)
142 frameRgb = messageGroup["rgb"]
143 assert isinstance(frameRgb, dai.ImgFrame)
144 frameDepth = messageGroup["depth_aligned"]
145 assert isinstance(frameDepth, dai.ImgFrame)
146
147 sizeRgb = frameRgb.getData().size
148 sizeDepth = frameDepth.getData().size
149 # Blend when both received
150 if frameDepth is not None:
151 cvFrame = frameRgb.getCvFrame()
152 rgbIntrinsics = calibrationHandler.getCameraIntrinsics(RGB_SOCKET, int(cvFrame.shape[1]), int(cvFrame.shape[0]))
153 cvFrameUndistorted = cv2.undistort(
154 cvFrame,
155 np.array(rgbIntrinsics),
156 np.array(rgbDistortion),
157 )
158 # Colorize the aligned depth
159 alignedDepthColorized = colorizeDepth(frameDepth.getFrame())
160 # Resize depth to match the rgb frame
161 cv2.putText(
162 alignedDepthColorized,
163 f"FPS: {fpsCounter.getFps():.2f}",
164 (10, 30),
165 cv2.FONT_HERSHEY_SIMPLEX,
166 1,
167 (255, 255, 255),
168 2,
169 )
170 cv2.imshow("depth", alignedDepthColorized)
171
172 blended = cv2.addWeighted(
173 cvFrameUndistorted, rgbWeight, alignedDepthColorized, depthWeight, 0
174 )
175 cv2.imshow(rgbDepthWindowName, blended)
176
177 key = cv2.waitKey(1)
178 if key == ord("q"):
179 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.