Interactive Warp Mesh
r to restart the pipeline and apply the changes.User-defined arguments:--mesh_dims- Mesh dimensions (default:4x4).--resolution- Resolution of the input image (default:512x512). Width must be divisible by 16.--random- To generate random mesh points (disabled by default).
Demo

Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2import cv2
3import depthai as dai
4import numpy as np
5import argparse
6import re
7import sys
8from random import randint
9
10parser = argparse.ArgumentParser()
11parser.add_argument("-m", "--mesh_dims", type=str, default="4x4", help="mesh dimensions widthxheight (default=%(default)s)")
12parser.add_argument("-r", "--resolution", type=str, default="512x512", help="preview resolution (default=%(default)s)")
13parser.add_argument("-rnd", "--random", action="store_true", help="Generate random initial mesh")
14args = parser.parse_args()
15
16# mesh dimensions
17match = re.search(r'.*?(\d+)x(\d+).*', args.mesh_dims)
18if not match:
19 raise Exception(f"Mesh dimensions format incorrect '{args.resolution}'!")
20mesh_w = int(match.group(1))
21mesh_h = int(match.group(2))
22
23# Preview resolution
24match = re.search(r'.*?(\d+)x(\d+).*', args.resolution)
25if not match:
26 raise Exception(f"Resolution format incorrect '{args.resolution}'!")
27preview_w = int(match.group(1))
28preview_h = int(match.group(2))
29if preview_w % 16 != 0:
30 raise Exception(f"Preview width must be a multiple of 16!")
31
32# Create an initial mesh (optionally random) of dimension mesh_w x mesh_h
33first_point_x = int(preview_w / 10)
34between_points_x = int(4 * preview_w / (5 * (mesh_w - 1)))
35first_point_y = int(preview_h / 10)
36between_points_y = int(4 * preview_h / (5 * (mesh_h - 1)))
37if args.random:
38 max_rnd_x = int(between_points_x / 4)
39 max_rnd_y = int(between_points_y / 4)
40mesh = []
41for i in range(mesh_h):
42 for j in range(mesh_w):
43 x = first_point_x + j * between_points_x
44 y = first_point_y + i * between_points_y
45 if args.random:
46 rnd_x = randint(-max_rnd_x, max_rnd_x)
47 if x + rnd_x > 0 and x + rnd_x < preview_w:
48 x += rnd_x
49 rnd_y = randint(-max_rnd_y, max_rnd_y)
50 if y + rnd_y > 0 and y + rnd_y < preview_h:
51 y += rnd_y
52 mesh.append((x, y))
53
54def create_pipeline(mesh):
55 print(mesh)
56 # Create pipeline
57 pipeline = dai.Pipeline()
58
59 camRgb = pipeline.create(dai.node.ColorCamera)
60 camRgb.setPreviewSize(preview_w, preview_h)
61 camRgb.setInterleaved(False)
62 width = camRgb.getPreviewWidth()
63 height = camRgb.getPreviewHeight()
64
65 # Output source
66 xout_source = pipeline.create(dai.node.XLinkOut)
67 xout_source.setStreamName('source')
68 camRgb.preview.link(xout_source.input)
69 # Warp source frame
70 warp = pipeline.create(dai.node.Warp)
71 warp.setWarpMesh(mesh, mesh_w, mesh_h)
72 warp.setOutputSize(width, height)
73 warp.setMaxOutputFrameSize(width * height * 3)
74 camRgb.preview.link(warp.inputImage)
75
76 warp.setHwIds([1])
77 warp.setInterpolation(dai.Interpolation.NEAREST_NEIGHBOR)
78 # Output warped
79 xout_warped = pipeline.create(dai.node.XLinkOut)
80 xout_warped.setStreamName('warped')
81 warp.out.link(xout_warped.input)
82 return pipeline
83
84point_selected = None
85
86def mouse_callback(event, x, y, flags, param):
87 global mesh, point_selected, mesh_changed
88 if event == cv2.EVENT_LBUTTONDOWN:
89 if point_selected is None:
90 # Which point is selected ?
91 min_dist = 100
92
93 for i in range(len(mesh)):
94 dist = np.linalg.norm((x - mesh[i][0], y - mesh[i][1]))
95 if dist < 20 and dist < min_dist:
96 min_dist = dist
97 point_selected = i
98 if point_selected is not None:
99 mesh[point_selected] = (x, y)
100 mesh_changed = True
101
102 elif event == cv2.EVENT_LBUTTONUP:
103 point_selected = None
104 elif event == cv2.EVENT_MOUSEMOVE:
105 if point_selected is not None:
106 mesh[point_selected] = (x, y)
107 mesh_changed = True
108
109
110cv2.namedWindow("Source")
111cv2.setMouseCallback("Source", mouse_callback)
112
113running = True
114
115print("Use your mouse to modify the mesh by clicking/moving points of the mesh in the Source window")
116print("Then press 'r' key to restart the device/pipeline")
117while running:
118 pipeline = create_pipeline(mesh)
119 # Connect to device and start pipeline
120 with dai.Device(pipeline) as device:
121 print("Starting device")
122 # Output queue will be used to get the rgb frames from the output defined above
123 q_source = device.getOutputQueue(name="source", maxSize=4, blocking=False)
124 q_warped = device.getOutputQueue(name="warped", maxSize=4, blocking=False)
125
126 restart_device = False
127 mesh_changed = False
128 while not restart_device:
129 in0 = q_source.get()
130 if in0 is not None:
131 source = in0.getCvFrame()
132 color = (0, 0,255) if mesh_changed else (0,255,0)
133 for i in range(len(mesh)):
134 cv2.circle(source, (mesh[i][0], mesh[i][1]), 4, color, -1)
135 if i % mesh_w != mesh_w -1:
136 cv2.line(source, (mesh[i][0], mesh[i][1]), (mesh[i+1][0], mesh[i+1][1]), color, 2)
137 if i + mesh_w < len(mesh):
138 cv2.line(source, (mesh[i][0], mesh[i][1]), (mesh[i+mesh_w][0], mesh[i+mesh_w][1]), color, 2)
139 cv2.imshow("Source", source)
140
141 in1 = q_warped.get()
142 if in1 is not None:
143 cv2.imshow("Warped", in1.getCvFrame())
144
145 key = cv2.waitKey(1)
146 if key == ord('r'): # Restart the device if mesh has changed
147 if mesh_changed:
148 print("Restart requested...")
149 mesh_changed = False
150 restart_device = True
151 elif key == 27 or key == ord('q'): # Exit
152 running = False
153 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.