# RGB-D

RGBD refers to the type of image data that includes both color (RGB) and depth (D) information.

### Applications of RGB-D

### Colorized Pointcloud

Create on-device pointclouds

[Colorized Pointcloud](https://docs.luxonis.com/software-v3/depthai/examples/pointcloud_visualization.md)

### Spatial AI

Combine depth with neural networks

[Spatial AI](https://docs.luxonis.com/software-v3/depthai/perception/spatial-ai.md)

## Aligning RGB and Depth Images

Core element of RGB-D pipeline is alignment. The idea is to align each pixel in the depth image with the corresponding pixel in
the color image. This is necessary because the depth image perspective is different from the color image perspective due to the
different camera positions.

The alignment can be done using reprojection. By default, the depth is aligned to the `rectified_left` image during the
stereo-matching process. We can project this image to 3D space (using acquired depth information) and then reproject it back to
the color image plane using color camera intrinsics.

## Alignment using DepthAI

DepthAI provides a few ways to achieve alignment of RGB and depth images which all offer the same functionality, but have their
own benefits and drawbacks.

### StereoDepth and GPUStereo - for stereo cameras

The [StereoDepth](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/stereo_depth.md) node offers alignment
capabilities out of the box. The node takes in a pair of stereo images (`left` and `right`) and outputs a depth map. By default,
the depth image is aligned with the `rectified_left` image, but can be changed using the `setDepthAlign()` method.

```python
stereo.setDepthAlign(dai.CameraBoardSocket.RGB) # Provided that the RGB camera is connected to RGB/CAM_A port
```

On RVC4, [GPUStereo](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/gpu_stereo.md) is another stereo depth
option. It generates disparity and depth from a synchronized stereo pair; when you need that depth reprojected into the RGB camera
plane, pair it with [ImageAlign](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/image_align.md).

### Examples

* [RGB Depth Alignment](https://docs.luxonis.com/software-v3/depthai/examples/rgb_depth_aligned.md)

### ImageAlign - general alignment

The ImageAlign node is a more general-purpose node that can be used to align any two images. The node takes in two images (`input`
and `inputAlignTo`) and outputs the aligned image. For RGB-D, this node allows us to align the [Time-of-Flight (ToF)
depth](https://docs.luxonis.com/hardware/platform/features/depth.md) to RGB.

### Examples

* [ToF Minimal example](https://docs.luxonis.com/software-v3/depthai/examples/tof/tof_minimal.md)
 * [ToF Align example](https://docs.luxonis.com/software-v3/depthai/examples/tof/tof_align.md)
 * [RGB-Stereo alignment](https://github.com/luxonis/depthai-python/blob/main/examples/ImageAlign/depth_align.py)

> **Efficiency**
> Use [StereoDepth](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/stereo_depth.md) when you want built-in stereo depth alignment, as it avoids a separate [ImageAlign](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/image_align.md) reprojection step. On RVC4, [GPUStereo](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/gpu_stereo.md) remains a valid stereo source for RGB-D pipelines when paired with ImageAlign.

### RGB-D on Wide FOV cameras

When using WFOV cameras, the alignment can be tricky due to the large distortion in the images caused by the lens. By default, the
depth image is undistorted during the rectification-undistortion process, but the color image is not. This can lead to
misalignment between the two images. To solve this, the color image needs to be undistorted as well.

Using [Camera](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/camera.md) node. The node can be used to
undistort the color image using the intrinsic parameters of the camera. When requesting an undistorted output, use `alphaScaling`
to control how much of the original field of view is retained.

#### Python

```python
cam = pipeline.create(dai.node.Camera)
cam.setBoardSocket(dai.CameraBoardSocket.RGB)
cam.setMeshSource(dai.CameraProperties.WarpMeshSource.CALIBRATION)
```

#### C++

```cpp
auto cam = pipeline.create<dai::node::Camera>();
cam->setBoardSocket(dai::CameraBoardSocket::RGB);
cam->setMeshSource(dai::CameraProperties::WarpMeshSource::CALIBRATION);
```

The undistortion can be done manually using the intrinsic parameters of the camera and OpenCV.

```python
alpha = 0.0
stereo.setAlphaScaling(alpha)

rgb_w = camRgb.getResolutionWidth()
rgb_h = camRgb.getResolutionHeight()
rgbIntrinsics = np.array(calibData.getCameraIntrinsics(rgbCamSocket, rgb_w, rgb_h))
rgb_d = np.array(calibData.getDistortionCoefficients(rgbCamSocket))
rgb_new_cam_matrix, _ = cv2.getOptimalNewCameraMatrix(rgbIntrinsics, rgb_d, (rgb_w, rgb_h), alpha)
map_x, map_y = cv2.initUndistortRectifyMap(rgbIntrinsics, rgb_d, None, rgb_new_cam_matrix, (rgb_w, rgb_h), cv2.CV_32FC1)

frameRgb = cv2.remap(frameRgb, map_x, map_y, cv2.INTER_LINEAR)
```

### Full code

Example using OpenCV undistortion

[Full
code](https://gist.githubusercontent.com/Erol444/bf0fa3debde7e4479477b03e1a98867e/raw/7541837302af9c7b304a50102eb64ce8c938c8fa/rgb-depth-align-alpha1.py)

When undistorting an image captured by a wide FOV camera, the warping will cause some parts of the image to be cut off. This
results in the loss of FOV which is the primary selling point of WFOV cameras. DepthAI exposes `alphaScaling` to control the
balance between cropping and retaining the full field of view. In manual OpenCV undistortion, the equivalent value is passed as
the `alpha` argument to `getOptimalNewCameraMatrix()` [[guide](https://docs.opencv.org/4.x/dc/dbb/tutorial_py_calibration.html)].

### Setting alphaScaling

* `alphaScaling = 0` - Crops more aggressively, minimizing unused border pixels.

 * `alphaScaling = 1` - Retains as much of the original field of view as possible.

#### StereoDepth undistortion

```python
stereo.setAlphaScaling(alphaScaling)
```

#### Camera undistortion

```python
rgbOut = camRgb.requestOutput(
    size=(1280, 800),
    enableUndistortion=True,
    alphaScaling=alpha,
)
```

#### OpenCV undistortion

```python
rgb_new_cam_matrix, _ = cv2.getOptimalNewCameraMatrix(rgbIntrinsics, rgb_d, (rgb_w, rgb_h), alpha)
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.