# OAK Viewer

OAK Viewer is a GUI application that allows you to easily evaluate the camera by visualizing its output in real-time.

## Download

> If you are updating OAK Viewer via
> [oakctl](https://docs.luxonis.com/software-v3/oak-apps/oakctl.md)
> , you need to use version 0.15.0+ to get the latest OAK Viewer.

#### Linux

> Debian packages are available for Ubuntu 24.04 / 22.04, supporting x86_64 (AMD64) architecture.

OAK Viewer 3.2.1 for [Ubuntu 24.04 / 22.04 (x86)](https://oak-viewer-releases.luxonis.com/data/3.2.1/debian_x86_64/viewer.deb)

#### macOS

> Viewer is available for macOS 12 and later, supporting both ARM (Apple Silicon) and x86_64 (Intel) architectures.

OAK Viewer 3.2.1 for [macOS 12+ (ARM)](https://oak-viewer-releases.luxonis.com/data/3.2.1/macos_arm_64/Viewer.zip) | [macOS 12+
(x86)](https://oak-viewer-releases.luxonis.com/data/3.2.1/macos_x86_64/Viewer.zip)

#### Windows

> Please note that you can get warning from Microsoft Defender. Viewer is available for Windows 10/11, supporting the x86_64
(AMD64) architecture.

OAK Viewer 3.2.1 for [Windows 10/11 (x86)](https://oak-viewer-releases.luxonis.com/data/3.2.1/windows_x86_64/Viewer.msi)

## Features

### Local Viewer and OAK4 Default App

> Please note that all features of Viewer work only in Chrome. The local version includes a bundled Chrome browser. However, the
web version can be opened in any browser, albeit with some limitations. All browsers should support RAW streams. Encoded streams
and features based on them are supported only in Chrome because they require the full set of the
> [WebCodecs API](https://developer.mozilla.org/en-US/docs/Web/API/VideoDecoder)
> , which currently only Chrome provides with high quality and performance.

It is possible to run the Viewer as a local application or as a default app that can be installed during device setup. Both
versions provide similar features. The main difference is that the default app on OAK4 works only with the device itself. On the
other hand, the local version includes a device selector in the header that displays all OAK cameras the Viewer can detect,
including devices available via Ethernet and USB. The Viewer uses DepthAI V3 for connections, so any RVC2 or RVC4 device is
supported.

The local version uses WebSocket for communication between the frontend and backend, and therefore it is limited only by the speed
of the local network. The default app supports two modes. The first mode involves a direct connection to the device, typically
using https://device-IP:9000. The exact URL can be found in the application logs. A self-signed certificate is required for the
encoded streams to function properly. If multiple applications are running, the second port 9001 is used. It is recommended to
verify the exact URL in the application logs.

The second option to open the Viewer as a default app is through remote access. Internally, WebRTC is used, and therefore the
theoretical bandwidth throughput supported is around 400 Mbps locally. It can be lower when the connection is over the internet,
depending on actual connectivity. In this case, the URL will look like this: https://viewer.luxonis.app/1.2.1/?t=xxxx. The
specific URL can be found in the application logs, or the UI can be opened remotely via the Hub, where the correct URL is
available.

> Please note that this URL is valid only for 15 minutes and is then regenerated. It is not necessary to reopen the UI, as it will
automatically refresh, but it is not possible to bookmark this URL.

### Pipelines

You can choose from four predefined pipelines. Each pipeline uses its own DepthAI pipeline.

 * Vision 3D: Focused on output from the main camera and point clouds.
 * Vision AI: Focused on outputs from selected neural network (NN) model and their annotations.
 * Dynamic Calibration: You can
   [recalibrate](https://docs.luxonis.com/software-v3/depthai/depthai-components/host_nodes/dynamic_calibration.md) your device in
   this pipeline. All OAK Series 2 full stereo lineup (excluding FFC) and OAK Series 4 full stereo lineup are supported. [Learn
   more.](https://discuss.luxonis.com/blog/6346-dynamic-calibration-keeping-stereo-depth-accurate)
 * Advanced: Allows in‑depth configuration of all features and access to calibration data.

### Streams and Pipeline Graph

There are two main tabs available in the Viewer. The first one is Streams. It displays a predefined set of streams that the device
can provide. These streams depend on the supported features, such as the main RGB camera, left/right cameras (if available), depth
stream, temperature, etc. Additionally, there is a stream from the selected NN model. These models are loaded from the Luxonis
Models ZOO. If a YOLO model is selected, annotations can be displayed on the RGB camera stream, and so on. Among the streams,
there is also the depth and point cloud, which are computed on the frontend based on depth and RGB data to be bandwidth-efficient.
All these features offer simple configuration options.

> **Custom models cannot be uploaded in OAK Viewer**
> OAK Viewer supports only a selected subset of Luxonis Models Zoo models. User can cannot upload custom models or run models
outside that subset. See the
> [Use custom models on HubAI](https://docs.luxonis.com/cloud/tutorials/use-custom-models-on-hub-ai.md)
> tutorial.

The second tab is Pipeline Graph. This tab shows the active pipeline that the Viewer backend has created in DepthAI V3. It
provides a visual representation of all nodes, their parameters, and connections.

### Streams features in Advanced Pipeline

The following actions are available on the Streams screen:

 * Configuration: Allows configuration of sensors, stereo depth, and advanced settings.
 * Neural Network: Displays a list of NN models from the Luxonis ZOO that can be quickly tested and configured.
 * Streams: Shows a list of all streams available on the device based on the current configuration.
 * Point Cloud: Displays a real-time point cloud based on depth data and colored by the RGB camera.
 * Panel Layout: Provides a quick way to set the layout of visible panels.

### Stream panel

Every stream panel has a unique name, resolution, and several performance metrics. It includes the following FPS metrics:

 * Camera: The FPS requested based on the configuration.
 * Network: The FPS delivered over the network.
 * Decoding: The FPS decoded on the client side.
 * Rendering: The FPS rendered on the client side.

Throughput is calculated as the sum of all the frames actually delivered to the client in the browser over the network from the
Viewer backend. It doesn’t include traffic between DepthAI and the device. Other buttons provide options to control which
annotations are visible, panel position, and fullscreen mode.

## Troubleshooting device discovery

> **Device visible in oakctl, missing in OAK Viewer**
> `oakctl list`
> and OAK Viewer can disagree on some networks.
> `oakctl`
> discovery uses mDNS, while DepthAI discovery used by OAK Viewer depends on local network broadcast behavior.

 1. Update to the latest versions:
    * Run oakctl self-update on the host.
    * Run oakctl device update for the camera.
 2. Verify the host and camera are on the same subnet and that broadcast traffic is not blocked on your network.
 3. Check firewall rules on the host:
    * Allow 11491/udp for discovery.
    * Allow 11490/tcp for XLink connection.
 4. Disable VPN temporarily and test again.
 5. If the host has multiple interfaces (for example Wi-Fi and Ethernet), set routing so the camera subnet is reached through the
    correct interface.

## Release Notes

### Version 3.2.1 (June 8, 2026)

 * Backported DepthAI version due to Windows and Mac issues.
 * Reverted Point Cloud Alignment fix due to Windows and MacOS issues.

### Version 3.2.0 (June 8, 2026)

 * Fixed Windows and MacOS start device issues.

### Version 3.0.2 (June 5, 2026)

 * Improved performance across the board.
 * Improved point cloud precision & responsiveness.
 * Improved error state handling, including cases where the app is already running or the device is offline.
 * Fixed device disconnect handling.
 * Added detection of insufficient device power.
 * Several bug fixes and UI/UX improvements.

### Version 2.5.2 (June 2, 2026)

 * Improvements to stability and bugfixing.

### Version 2.5.1 (May 27, 2026)

 * Fix crashes when running with hardware acceleration enabled on macOS and Windows.
 * Fix oakctl dependencies on Windows.
 * Improve error handling during OS update.
 * Improve error handling for cameras without a color sensor.

### Version 2.4.11 (May 25, 2026)

 * RVC4 USB support
 * Initial TOF support (RVC2 only)
 * Expanded device support
 * Stability improvements
 * Neural Assisted Stereo (RVC4 only)

### Version 1.6.3 (December 18, 2025)

 * Includes oakctl 0.17.0, with more robust handling of device setup and adoption to Hub.
 * Includes DAI 3.2.1 and DAI Nodes 0.3.6.
 * Improvements to OTA update flows.
 * Improved stream and annotation rendering performance.
 * Error toasts are now properly displayed when configuration changes fail.
 * Moved the distance slider to the top-right corner.
 * Added a link to USB camera troubleshooting documentation.

### Version 1.5.53 (December 8, 2025)

 * Full support for OAK 4 device setup and adoption to Luxonis Hub, including migration to a different team when the device is
   already in Hub.
 * Fixed video encoder issues on Windows, resolving green stripe artifacts.
 * Fixed issues with loading information about connected devices.
 * Fixed connection issues when multiple devices are present.
 * Improved UI responsiveness across different resolutions and corrected the positioning of info toasts.
 * Corrected Flood Light and Dot Projector badges for OAK 4 D.
 * Improved Neural Depth configuration.
 * Includes Visualizer 2.68.8 (Improved responsiveness, Better NV12 decoding, Ability to change the point cloud camera).
 * Fixed the toast shown when another application is already running on OAK 4.