# Optimizing FPS & Latency

These tables show what performance you can expect from USB 3.2 Gen 1 (5 Gbps) connection with an RVC2 OAK camera. XLink chunking
was disabled for these tests (`pipeline.setXLinkChunkSize(0)`). For an example code, see [Benchmark
Camera](https://docs.luxonis.com/software-v3/depthai/examples/benchmark/benchmark_camera.md).

> **Note**
> To enable 10Gbps USB3 mode (when using a USB 3.2 Gen 2 compliant cable), create the [Device](https://docs.luxonis.com/software-v3/depthai/depthai-components/device.md) with `maxUsbSpeed` and pass it to the pipeline:

```python
with dai.Device(maxUsbSpeed=dai.UsbSpeed.SUPER_PLUS) as device:
    with dai.Pipeline(device) as pipeline:
        pipeline.start()
```

| What | Resolution | FPS | FPS set | Latency [ms] | Bandwidth | Histogram |
| --- | --- | --- | --- | --- | --- | --- |
| Color (NV12) | 1080P | 60 | 60 | 33 | 1.5 Gbps |
[link](https://user-images.githubusercontent.com/18037362/162675407-77882498-5bf1-4af8-b779-9b9e8321af57.png) |
| Color (NV12) | 4K | 28.5 | 30 | 150 | 2.8 Gbps |
[link](https://user-images.githubusercontent.com/18037362/162675403-f3c5a4c3-1f7d-4acc-a5d5-f5aecff5a66a.png) |
| Color (NV12) | 4K | 26 | 26 | 83 (Std: 3.6) | 2.6 Gbps | / |
| Mono | 720P/800P | 120 | 120 | 24.5 | 885/983 Mbps |
[link](https://user-images.githubusercontent.com/18037362/162675400-b19f1e2c-bee0-4482-a861-39481bf2e35e.png) |
| Mono | 400P | 120 | 120 | 7.5 | 246 Mbps |
[link](https://user-images.githubusercontent.com/18037362/162675393-e3fb08fb-0f17-49d0-85d0-31ae7b5af0f9.png) |

Below are the same tests, but also with OAK PoE camera, which uses Gigabit ethernet link. The camera was connected directly to the
computer, without any switches or routers in between. Power was supplied via M8 connector.

 * [oak_bandwidth_test.py](https://github.com/luxonis/oak-examples/tree/master/random-scripts#oak-bandwidth-test) results: 797
   mbps downlink, 264 mbps uplink.
 * [oak_latency_test.py](https://github.com/luxonis/oak-examples/tree/master/random-scripts#oak-latency-test) results: Average:
   5.2 ms, Std: 6.2.

These two scripts use the DepthAI v2 API, so they do not run with DepthAI v3.

| What | Resolution | FPS | FPS set | PoE Latency [ms] | USB Latency [ms] | Bandwidth |
| --- | --- | --- | --- | --- | --- | --- |
| Color (NV12) | 1080P | 25 | 25 | 51 | 33 Std: 0.8 | 622 Mbps |
| Color (NV12) | 4K | 8 | 8 | 148 | 80 Std: 1.2 | 796 Mbps |
| Color (NV12) | 4K | 8.5 | 10 | 530 | 80 Std: 1.3 | 995 Mbps |
| Mono | 400P | 90 | 90 | 12 Std: 5.0 | 8 Std: 0.47 | 184 Mbps |
| Mono | 400P | 110 | 110 | 16 Std: 9.4 | 8 Std: 0.45 | 225 Mbps |

We set lower FPS for the POE measurements due to bandwidth constraints. For example, 4K 8 FPS had 150ms latency, while 4K 10FPS
had 530ms latency, as link was saturated.

 * Latency is measured time between frame timestamp (`imgFrame.getTimestamp()`) and host timestamp when the frame is received
   (`dai.Clock.now()`).
 * Histogram shows how much Time-to-Host varies frame to frame. Y axis represents number of frame that occurred at that time while
   the X axis represents microseconds.
 * Bandwidth is calculated bandwidth required to stream specified frames at specified FPS.

## Encoded frames

| What | Resolution | FPS | FPS set | Time-to-Host [ms] | Histogram |
| --- | --- | --- | --- | --- | --- |
| Color video H.265 | 4K | 28.5 | 30 | 210 |
[link](https://user-images.githubusercontent.com/18037362/162675386-a59a58d1-1d5c-4c82-89d8-12882926425b.png) |
| Color video MJPEG | 4K | 30 | 30 | 71 |
[link](https://user-images.githubusercontent.com/18037362/162675384-64842bd6-f5e7-4b40-adf4-39b9c25d1c89.png) |
| Color video H.265 | 1080P | 60 | 60 | 42 |
[link](https://user-images.githubusercontent.com/18037362/162675356-c7c86730-63cd-4de8-bad6-4e1484b29ca5.png) |
| Color video MJPEG | 1080P | 60 | 60 | 31 |
[link](https://user-images.githubusercontent.com/18037362/162675371-62aadb93-20f0-4838-9aab-727fb1bfe6f4.png) |
| Mono H.265 | 800P | 60 | 60 | 23.5 |
[link](https://user-images.githubusercontent.com/18037362/162675318-92a8541b-424c-49b1-8ec4-6d9e0170410a.png) |
| Mono MJPEG | 800P | 60 | 60 | 22.5 |
[link](https://user-images.githubusercontent.com/18037362/162675328-20afbe8f-4587-4263-8981-919e5a8811c7.png) |
| Mono H.265 | 400P | 120 | 120 | 7.5 |
[link](https://user-images.githubusercontent.com/18037362/162675345-dfb4d04a-5d3a-4f84-81e9-dfc091bc00b5.png) |
| Mono MJPEG | 400P | 120 | 120 | 7.5 |
[link](https://user-images.githubusercontent.com/18037362/162675335-2e5a9581-972a-448c-b650-6b6d076a04b8.png) |

## PoE latency

On PoE, the latency can vary quite a bit due to a number of factors:

 * Network itself. Eg. if you are in a large network with many nodes, the latency will be higher compared to using a direct
   connection.
 * There's a bottleneck in bandwidth:
    * Perhaps some network link is 10mbps/100mbps instead of full 1gbps (due to switch/network card..). You can test this with
      [PoE Test script](https://github.com/luxonis/oak-examples/tree/master/random-scripts#poe-test-script) (`speed` should be
      1000).
    * Network/computer is saturated with other traffic. You can test the actual bandwidth with [OAK bandwidth
      test](https://github.com/luxonis/oak-examples/tree/master/random-scripts#oak-bandwidth-test) script (DepthAI v2). With
      direct link I got ~800mbps downlink and ~210mbps uplink.
 * Computer's Network Interface Card settings, [documentation
   here](https://docs.luxonis.com/hardware/platform/deploy/poe-deployment-guide.md)
 * 100% OAK Leon CSS (CPU) usage. The Leon CSS core handles the POE communication ([see docs
   here](https://docs.luxonis.com/hardware/platform/rvc/rvc2.md)), and if the CPU is 100% used, it will not be able to handle the
   communication as fast as it should. Workaround: See [CPU
   usage](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages/system_information.md) docs.
 * Another potential way to improve PoE latency would be to fine-tune network settings, like MTU, TCP window size, etc. (see
   [here](https://docs.luxonis.com/hardware/platform/deploy/poe-deployment-guide.md) for more info)

## Bandwidth

With large, unencoded frames, one can quickly saturate the bandwidth even at 30FPS, especially on PoE devices (1gbps link):

```bash
4K NV12/YUV420 frames: 3840 * 2160 * 1.5 * 30fps * 8bits = 3 gbps
1080P NV12/YUV420 frames: 1920 * 1080 * 1.5 * 30fps * 8bits = 747 mbps
720P NV12/YUV420 frames: 1280 * 720 * 1.5 * 30fps * 8bits = 331 mbps

1080P RGB frames: 1920 * 1080 * 3 * 30fps * 8bits = 1.5 gbps

800P depth frames: 1280 * 800 * 2 * 30fps * 8bits = 492 mbps
400P depth frames: 640 * 400 * 2 * 30fps * 8bits = 123 mbps

800P mono frames: 1280 * 800 * 1 * 30fps * 8bits = 246 mbps
400P mono frames: 640 * 400 * 1 * 30fps * 8bits = 62 mbps
```

The third value in the formula is byte/pixel, which is 1.5 for NV12/YUV420, 3 for RGB, and 2 for depth frames, and 1 for mono
(grayscale) frames. For disparity frames, it's either 1 (normal) or 2 (subpixel mode) on RVC2, and 2 on RVC4.

A few options to reduce bandwidth:

 * Encode frames (H.264, H.265, MJPEG) on-device using
   [VideoEncoder](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/video_encoder.md)
 * Reduce FPS/resolution/number of streams

## Measuring operation times

If user sets depthai level to `trace` (see [DepthAI debugging
level](https://docs.luxonis.com/software-v3/depthai/depthai-components/device.md)), depthai will log operation times for each
node/process, as shown below.

```bash
[NeuralNetwork(5)] [trace] NeuralNetwork inference took '90.23677' ms.
[StereoDepth(3)] [trace] Warp node took '1.094078' ms.
[system] [trace] EV:0,S:0,IDS:22,IDD:46,TSS:3,TSN:728092267
[system] [trace] EV:0,S:1,IDS:22,IDD:46,TSS:3,TSN:728145970
[DetectionParser(6)] [trace] DetectionParser took 91ms, getting input 86ms, processing 4ms,  sending output 0ms
[SpatialLocationCalculator(7)] [trace] SpatialLocationCalculator took 20ms, getting input 15ms, processing 4ms,  sending output 0ms
[StereoDepth(3)] [trace] Stereo took '13.878461' ms.
[StereoDepth(3)] [trace] 'Disparity to depth' pipeline took '1.274076' ms.
[StereoDepth(3)] [trace] Stereo post processing (total) took '1.344238' ms.
[StereoDepth(3)] [trace] Stereo rectification took '2.866409' ms.
[Camera(0)] [trace] Color ISP took '3.735966' ms.
[Camera(1)] [trace] Mono ISP took '1.383502' ms.
```

## Reducing latency when running NN

In the examples above we were only streaming frames, without doing anything else on the OAK camera. This section will focus on how
to reduce latency when also running NN model on the OAK.

### Increasing NN resources

One option to reduce latency is to increase the NN resources. This can be done by changing the number of allocated NCEs and SHAVES
(see HW accelerator [docs here](https://docs.luxonis.com/hardware/platform/rvc/rvc2.md)). NCEs and SHAVEs are RVC2 hardware
blocks, so this section applies to RVC2 devices. [Compile
Tool](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/offline/openvino.md) can compile a model for
more SHAVE cores. To allocate more NCEs, you can use API below:

```python
import depthai as dai

pipeline = dai.Pipeline()
# nn = pipeline.create(dai.node.NeuralNetwork)
nn = pipeline.create(dai.node.DetectionNetwork)
nn.setNumInferenceThreads(1) # By default, 2 threads if the model uses at most half of the free SHAVEs, else 1
nn.setNumNCEPerInferenceThread(2) # By default, 1 NCE per thread with 2 threads, 2 NCEs with 1 thread
```

Models usually run at max FPS when using 2 threads (1 NCE/Thread), and compiling model for `AVAILABLE_SHAVES / 2`.

Example of FPS & latency comparison for YoloV7-tiny:

| NN resources | Camera FPS | Latency | NN FPS |
| --- | --- | --- | --- |
| 6 SHAVEs, 2x Threads (1NCE/Thread) | 15 | 155 ms | 15 |
| 6 SHAVEs, 2x Threads (1NCE/Thread) | 14 | 149 ms | 14 |
| 6 SHAVEs, 2x Threads (1NCE/Thread) | 13 | 146 ms | 13 |
| 6 SHAVEs, 2x Threads (1NCE/Thread) | 10 | 141 ms | 10 |
| 13 SHAVEs, 1x Thread (2NCE/Thread) | 30 | 145 ms | 11.6 |
| 13 SHAVEs, 1x Thread (2NCE/Thread) | 12 | 128 ms | 12 |
| 13 SHAVEs, 1x Thread (2NCE/Thread) | 10 | 118 ms | 10 |

### Lowering camera FPS to match NN FPS

Lowering FPS to not exceed NN capabilities typically provides the best latency performance, since the NN is able to start the
inference as soon as a new frame is available.

For example, with 15 FPS we get a total of about 70 ms latency, measured from capture time (end of exposure and MIPI readout
start).

This time includes the following:

 * MIPI readout
 * ISP processing
 * Resizing the frame to the NN input size
 * NN processing
 * Streaming to host
 * And finally, eventual extra latency until it reaches the app

Note: if the FPS is increased slightly more, towards 19..21 FPS, an extra latency of about 10ms appears, that we believe is
related to firmware. We are actively looking for improvements for lower latencies.

### NN input queue size and blocking behavior

If the app has `detNetwork.input.setBlocking(False)`, but the queue size doesn't change, the following adjustment may help improve
latency performance:

By adding `detNetwork.input.setMaxSize(1)`, while setting back the camera FPS to 40, we get about 80.. 105ms latency. One of the
causes of being non-deterministic is that the camera is producing at a different rate (25ms frame-time), vs. when NN has finished
and can accept a new frame to process.