# Feature Tracker

Example shows capabilities of [FeatureTracker](https://docs.luxonis.com/software/depthai/examples/feature_tracker.md). It detects
features and tracks them between consecutive frames using optical flow by assigning unique ID to matching features. [Feature
Detector](https://docs.luxonis.com/software/depthai/examples/feature_detector.md) example only detects features.

## Demo

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
from collections import deque

class FeatureTrackerDrawer:

    lineColor = (200, 0, 200)
    pointColor = (0, 0, 255)
    circleRadius = 2
    maxTrackedFeaturesPathLength = 30
    # for how many frames the feature is tracked
    trackedFeaturesPathLength = 10

    trackedIDs = None
    trackedFeaturesPath = None

    def onTrackBar(self, val):
        FeatureTrackerDrawer.trackedFeaturesPathLength = val
        pass

    def trackFeaturePath(self, features):

        newTrackedIDs = set()
        for currentFeature in features:
            currentID = currentFeature.id
            newTrackedIDs.add(currentID)

            if currentID not in self.trackedFeaturesPath:
                self.trackedFeaturesPath[currentID] = deque()

            path = self.trackedFeaturesPath[currentID]

            path.append(currentFeature.position)
            while(len(path) > max(1, FeatureTrackerDrawer.trackedFeaturesPathLength)):
                path.popleft()

            self.trackedFeaturesPath[currentID] = path

        featuresToRemove = set()
        for oldId in self.trackedIDs:
            if oldId not in newTrackedIDs:
                featuresToRemove.add(oldId)

        for id in featuresToRemove:
            self.trackedFeaturesPath.pop(id)

        self.trackedIDs = newTrackedIDs

    def drawFeatures(self, img):

        cv2.setTrackbarPos(self.trackbarName, self.windowName, FeatureTrackerDrawer.trackedFeaturesPathLength)

        for featurePath in self.trackedFeaturesPath.values():
            path = featurePath

            for j in range(len(path) - 1):
                src = (int(path[j].x), int(path[j].y))
                dst = (int(path[j + 1].x), int(path[j + 1].y))
                cv2.line(img, src, dst, self.lineColor, 1, cv2.LINE_AA, 0)
            j = len(path) - 1
            cv2.circle(img, (int(path[j].x), int(path[j].y)), self.circleRadius, self.pointColor, -1, cv2.LINE_AA, 0)

    def __init__(self, trackbarName, windowName):
        self.trackbarName = trackbarName
        self.windowName = windowName
        cv2.namedWindow(windowName)
        cv2.createTrackbar(trackbarName, windowName, FeatureTrackerDrawer.trackedFeaturesPathLength, FeatureTrackerDrawer.maxTrackedFeaturesPathLength, self.onTrackBar)
        self.trackedIDs = set()
        self.trackedFeaturesPath = dict()

# Create pipeline
pipeline = dai.Pipeline()

# Define sources and outputs
monoLeft = pipeline.create(dai.node.MonoCamera)
monoRight = pipeline.create(dai.node.MonoCamera)
featureTrackerLeft = pipeline.create(dai.node.FeatureTracker)
featureTrackerRight = pipeline.create(dai.node.FeatureTracker)

xoutPassthroughFrameLeft = pipeline.create(dai.node.XLinkOut)
xoutTrackedFeaturesLeft = pipeline.create(dai.node.XLinkOut)
xoutPassthroughFrameRight = pipeline.create(dai.node.XLinkOut)
xoutTrackedFeaturesRight = pipeline.create(dai.node.XLinkOut)
xinTrackedFeaturesConfig = pipeline.create(dai.node.XLinkIn)

xoutPassthroughFrameLeft.setStreamName("passthroughFrameLeft")
xoutTrackedFeaturesLeft.setStreamName("trackedFeaturesLeft")
xoutPassthroughFrameRight.setStreamName("passthroughFrameRight")
xoutTrackedFeaturesRight.setStreamName("trackedFeaturesRight")
xinTrackedFeaturesConfig.setStreamName("trackedFeaturesConfig")

# Properties
monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
monoLeft.setCamera("left")
monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
monoRight.setCamera("right")

# Linking
monoLeft.out.link(featureTrackerLeft.inputImage)
featureTrackerLeft.passthroughInputImage.link(xoutPassthroughFrameLeft.input)
featureTrackerLeft.outputFeatures.link(xoutTrackedFeaturesLeft.input)
xinTrackedFeaturesConfig.out.link(featureTrackerLeft.inputConfig)

monoRight.out.link(featureTrackerRight.inputImage)
featureTrackerRight.passthroughInputImage.link(xoutPassthroughFrameRight.input)
featureTrackerRight.outputFeatures.link(xoutTrackedFeaturesRight.input)
xinTrackedFeaturesConfig.out.link(featureTrackerRight.inputConfig)

# By default the least mount of resources are allocated
# increasing it improves performance
numShaves = 2
numMemorySlices = 2
featureTrackerLeft.setHardwareResources(numShaves, numMemorySlices)
featureTrackerRight.setHardwareResources(numShaves, numMemorySlices)

featureTrackerConfig = featureTrackerRight.initialConfig.get()
print("Press 's' to switch between Lucas-Kanade optical flow and hardware accelerated motion estimation!")

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queues used to receive the results
    passthroughImageLeftQueue = device.getOutputQueue("passthroughFrameLeft", 8, False)
    outputFeaturesLeftQueue = device.getOutputQueue("trackedFeaturesLeft", 8, False)
    passthroughImageRightQueue = device.getOutputQueue("passthroughFrameRight", 8, False)
    outputFeaturesRightQueue = device.getOutputQueue("trackedFeaturesRight", 8, False)

    inputFeatureTrackerConfigQueue = device.getInputQueue("trackedFeaturesConfig")

    leftWindowName = "left"
    leftFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", leftWindowName)

    rightWindowName = "right"
    rightFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", rightWindowName)

    while True:
        inPassthroughFrameLeft = passthroughImageLeftQueue.get()
        passthroughFrameLeft = inPassthroughFrameLeft.getFrame()
        leftFrame = cv2.cvtColor(passthroughFrameLeft, cv2.COLOR_GRAY2BGR)

        inPassthroughFrameRight = passthroughImageRightQueue.get()
        passthroughFrameRight = inPassthroughFrameRight.getFrame()
        rightFrame = cv2.cvtColor(passthroughFrameRight, cv2.COLOR_GRAY2BGR)

        trackedFeaturesLeft = outputFeaturesLeftQueue.get().trackedFeatures
        leftFeatureDrawer.trackFeaturePath(trackedFeaturesLeft)
        leftFeatureDrawer.drawFeatures(leftFrame)

        trackedFeaturesRight = outputFeaturesRightQueue.get().trackedFeatures
        rightFeatureDrawer.trackFeaturePath(trackedFeaturesRight)
        rightFeatureDrawer.drawFeatures(rightFrame)

        # Show the frame
        cv2.imshow(leftWindowName, leftFrame)
        cv2.imshow(rightWindowName, rightFrame)

        key = cv2.waitKey(1)
        if key == ord('q'):
            break
        elif key == ord('s'):
            if featureTrackerConfig.motionEstimator.type == dai.FeatureTrackerConfig.MotionEstimator.Type.LUCAS_KANADE_OPTICAL_FLOW:
                featureTrackerConfig.motionEstimator.type = dai.FeatureTrackerConfig.MotionEstimator.Type.HW_MOTION_ESTIMATION
                print("Switching to hardware accelerated motion estimation")
            else:
                featureTrackerConfig.motionEstimator.type = dai.FeatureTrackerConfig.MotionEstimator.Type.LUCAS_KANADE_OPTICAL_FLOW
                print("Switching to Lucas-Kanade optical flow")

            cfg = dai.FeatureTrackerConfig()
            cfg.set(featureTrackerConfig)
            inputFeatureTrackerConfigQueue.send(cfg)
```

#### C++

```cpp
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"
#include "deque"
#include "unordered_map"
#include "unordered_set"

static const auto lineColor = cv::Scalar(200, 0, 200);
static const auto pointColor = cv::Scalar(0, 0, 255);

class FeatureTrackerDrawer {
   private:
    static const int circleRadius = 2;
    static const int maxTrackedFeaturesPathLength = 30;
    // for how many frames the feature is tracked
    static int trackedFeaturesPathLength;

    using featureIdType = decltype(dai::TrackedFeature::id);

    std::unordered_set<featureIdType> trackedIDs;
    std::unordered_map<featureIdType, std::deque<dai::Point2f>> trackedFeaturesPath;

    std::string trackbarName;
    std::string windowName;

   public:
    void trackFeaturePath(std::vector<dai::TrackedFeature>& features) {
        std::unordered_set<featureIdType> newTrackedIDs;
        for(auto& currentFeature : features) {
            auto currentID = currentFeature.id;
            newTrackedIDs.insert(currentID);

            if(!trackedFeaturesPath.count(currentID)) {
                trackedFeaturesPath.insert({currentID, std::deque<dai::Point2f>()});
            }
            std::deque<dai::Point2f>& path = trackedFeaturesPath.at(currentID);

            path.push_back(currentFeature.position);
            while(path.size() > std::max<unsigned int>(1, trackedFeaturesPathLength)) {
                path.pop_front();
            }
        }

        std::unordered_set<featureIdType> featuresToRemove;
        for(auto& oldId : trackedIDs) {
            if(!newTrackedIDs.count(oldId)) {
                featuresToRemove.insert(oldId);
            }
        }

        for(auto& id : featuresToRemove) {
            trackedFeaturesPath.erase(id);
        }

        trackedIDs = newTrackedIDs;
    }

    void drawFeatures(cv::Mat& img) {
        cv::setTrackbarPos(trackbarName.c_str(), windowName.c_str(), trackedFeaturesPathLength);

        for(auto& featurePath : trackedFeaturesPath) {
            std::deque<dai::Point2f>& path = featurePath.second;
            unsigned int j = 0;
            for(j = 0; j < path.size() - 1; j++) {
                auto src = cv::Point(path[j].x, path[j].y);
                auto dst = cv::Point(path[j + 1].x, path[j + 1].y);
                cv::line(img, src, dst, lineColor, 1, cv::LINE_AA, 0);
            }

            cv::circle(img, cv::Point(path[j].x, path[j].y), circleRadius, pointColor, -1, cv::LINE_AA, 0);
        }
    }

    FeatureTrackerDrawer(std::string trackbarName, std::string windowName) : trackbarName(trackbarName), windowName(windowName) {
        cv::namedWindow(windowName.c_str());
        cv::createTrackbar(trackbarName.c_str(), windowName.c_str(), &trackedFeaturesPathLength, maxTrackedFeaturesPathLength, nullptr);
    }
};

int FeatureTrackerDrawer::trackedFeaturesPathLength = 10;

int main() {
    using namespace std;

    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto monoLeft = pipeline.create<dai::node::MonoCamera>();
    auto monoRight = pipeline.create<dai::node::MonoCamera>();
    auto featureTrackerLeft = pipeline.create<dai::node::FeatureTracker>();
    auto featureTrackerRight = pipeline.create<dai::node::FeatureTracker>();

    auto xoutPassthroughFrameLeft = pipeline.create<dai::node::XLinkOut>();
    auto xoutTrackedFeaturesLeft = pipeline.create<dai::node::XLinkOut>();
    auto xoutPassthroughFrameRight = pipeline.create<dai::node::XLinkOut>();
    auto xoutTrackedFeaturesRight = pipeline.create<dai::node::XLinkOut>();
    auto xinTrackedFeaturesConfig = pipeline.create<dai::node::XLinkIn>();

    xoutPassthroughFrameLeft->setStreamName("passthroughFrameLeft");
    xoutTrackedFeaturesLeft->setStreamName("trackedFeaturesLeft");
    xoutPassthroughFrameRight->setStreamName("passthroughFrameRight");
    xoutTrackedFeaturesRight->setStreamName("trackedFeaturesRight");
    xinTrackedFeaturesConfig->setStreamName("trackedFeaturesConfig");

    // Properties
    monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoLeft->setCamera("left");
    monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_720_P);
    monoRight->setCamera("right");

    // Linking
    monoLeft->out.link(featureTrackerLeft->inputImage);
    featureTrackerLeft->passthroughInputImage.link(xoutPassthroughFrameLeft->input);
    featureTrackerLeft->outputFeatures.link(xoutTrackedFeaturesLeft->input);
    xinTrackedFeaturesConfig->out.link(featureTrackerLeft->inputConfig);

    monoRight->out.link(featureTrackerRight->inputImage);
    featureTrackerRight->passthroughInputImage.link(xoutPassthroughFrameRight->input);
    featureTrackerRight->outputFeatures.link(xoutTrackedFeaturesRight->input);
    xinTrackedFeaturesConfig->out.link(featureTrackerRight->inputConfig);

    // By default the least mount of resources are allocated
    // increasing it improves performance when optical flow is enabled
    auto numShaves = 2;
    auto numMemorySlices = 2;
    featureTrackerLeft->setHardwareResources(numShaves, numMemorySlices);
    featureTrackerRight->setHardwareResources(numShaves, numMemorySlices);

    auto featureTrackerConfig = featureTrackerRight->initialConfig.get();

    printf("Press 's' to switch between Lucas-Kanade optical flow and hardware accelerated motion estimation! \n");

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queues used to receive the results
    auto passthroughImageLeftQueue = device.getOutputQueue("passthroughFrameLeft", 8, false);
    auto outputFeaturesLeftQueue = device.getOutputQueue("trackedFeaturesLeft", 8, false);
    auto passthroughImageRightQueue = device.getOutputQueue("passthroughFrameRight", 8, false);
    auto outputFeaturesRightQueue = device.getOutputQueue("trackedFeaturesRight", 8, false);

    auto inputFeatureTrackerConfigQueue = device.getInputQueue("trackedFeaturesConfig");

    const auto leftWindowName = "left";
    auto leftFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", leftWindowName);

    const auto rightWindowName = "right";
    auto rightFeatureDrawer = FeatureTrackerDrawer("Feature tracking duration (frames)", rightWindowName);

    while(true) {
        auto inPassthroughFrameLeft = passthroughImageLeftQueue->get<dai::ImgFrame>();
        cv::Mat passthroughFrameLeft = inPassthroughFrameLeft->getFrame();
        cv::Mat leftFrame;
        cv::cvtColor(passthroughFrameLeft, leftFrame, cv::COLOR_GRAY2BGR);

        auto inPassthroughFrameRight = passthroughImageRightQueue->get<dai::ImgFrame>();
        cv::Mat passthroughFrameRight = inPassthroughFrameRight->getFrame();
        cv::Mat rightFrame;
        cv::cvtColor(passthroughFrameRight, rightFrame, cv::COLOR_GRAY2BGR);

        auto trackedFeaturesLeft = outputFeaturesLeftQueue->get<dai::TrackedFeatures>()->trackedFeatures;
        leftFeatureDrawer.trackFeaturePath(trackedFeaturesLeft);
        leftFeatureDrawer.drawFeatures(leftFrame);

        auto trackedFeaturesRight = outputFeaturesRightQueue->get<dai::TrackedFeatures>()->trackedFeatures;
        rightFeatureDrawer.trackFeaturePath(trackedFeaturesRight);
        rightFeatureDrawer.drawFeatures(rightFrame);

        // Show the frame
        cv::imshow(leftWindowName, leftFrame);
        cv::imshow(rightWindowName, rightFrame);

        int key = cv::waitKey(1);
        if(key == 'q') {
            break;
        } else if(key == 's') {
            if(featureTrackerConfig.motionEstimator.type == dai::FeatureTrackerConfig::MotionEstimator::Type::LUCAS_KANADE_OPTICAL_FLOW) {
                featureTrackerConfig.motionEstimator.type = dai::FeatureTrackerConfig::MotionEstimator::Type::HW_MOTION_ESTIMATION;
                printf("Switching to hardware accelerated motion estimation \n");
            } else {
                featureTrackerConfig.motionEstimator.type = dai::FeatureTrackerConfig::MotionEstimator::Type::LUCAS_KANADE_OPTICAL_FLOW;
                printf("Switching to Lucas-Kanade optical flow \n");
            }
            auto cfg = dai::FeatureTrackerConfig();
            cfg.set(featureTrackerConfig);
            inputFeatureTrackerConfigQueue->send(cfg);
        }
    }
    return 0;
}
```

## Pipeline

### examples/feature_tracker.pipeline.json

```json
{"pipeline": {"connections": [{"node1Id": 5, "node1Output": "out", "node1OutputGroup": "", "node2Id": 2, "node2Input": "inputConfig", "node2InputGroup": ""}, {"node1Id": 2, "node1Output": "outputFeatures", "node1OutputGroup": "", "node2Id": 8, "node2Input": "in", "node2InputGroup": ""}, {"node1Id": 1, "node1Output": "out", "node1OutputGroup": "", "node2Id": 2, "node2Input": "inputImage", "node2InputGroup": ""}, {"node1Id": 0, "node1Output": "0", "node1OutputGroup": "dynamicOutputs", "node2Id": 6, "node2Input": "in", "node2InputGroup": ""}, {"node1Id": 0, "node1Output": "0", "node1OutputGroup": "dynamicOutputs", "node2Id": 1, "node2Input": "inputImage", "node2InputGroup": ""}], "globalProperties": {"calibData": null, "cameraTuningBlobSize": null, "cameraTuningBlobUri": "", "leonCssFrequencyHz": 700000000.0, "leonMssFrequencyHz": 700000000.0, "pipelineName": null, "pipelineVersion": null, "sippBufferSize": 18432, "sippDmaBufferSize": 16384, "xlinkChunkSize": -1}, "nodes": [[8, {"alias": "", "id": 8, "ioInfo": [[["", "in"], {"blocking": true, "group": "", "id": 13, "name": "in", "queueSize": 3, "type": 3, "waitForMessage": false}]], "logLevel": 3, "name": "XLinkOut", "parentId": -1, "properties": {"maxFpsLimit": -1.0, "metadataOnly": false, "streamName": "__x_2_outputFeatures"}}], [6, {"alias": "", "id": 6, "ioInfo": [[["", "in"], {"blocking": true, "group": "", "id": 12, "name": "in", "queueSize": 3, "type": 3, "waitForMessage": false}]], "logLevel": 3, "name": "XLinkOut", "parentId": -1, "properties": {"maxFpsLimit": -1.0, "metadataOnly": false, "streamName": "__x_0_0"}}], [5, {"alias": "", "id": 5, "ioInfo": [[["", "out"], {"blocking": false, "group": "", "id": 11, "name": "out", "queueSize": 8, "type": 0, "waitForMessage": false}]], "logLevel": 3, "name": "XLinkIn", "parentId": -1, "properties": {"maxDataSize": 5242880, "numFrames": 8, "streamName": "__x_2__inputConfig"}}], [2, {"alias": "", "id": 2, "ioInfo": [[["", "passthroughInputImage"], {"blocking": false, "group": "", "id": 10, "name": "passthroughInputImage", "queueSize": 8, "type": 0, "waitForMessage": false}], [["", "outputFeatures"], {"blocking": false, "group": "", "id": 9, "name": "outputFeatures", "queueSize": 8, "type": 0, "waitForMessage": false}], [["", "inputImage"], {"blocking": false, "group": "", "id": 8, "name": "inputImage", "queueSize": 4, "type": 3, "waitForMessage": true}], [["", "inputConfig"], {"blocking": false, "group": "", "id": 7, "name": "inputConfig", "queueSize": 4, "type": 3, "waitForMessage": false}]], "logLevel": 3, "name": "FeatureTracker", "parentId": -1, "properties": {"initialConfig": {"cornerDetector": {"cellGridDimension": 4, "enableSobel": true, "enableSorting": true, "numMaxFeatures": 256, "numTargetFeatures": 256, "thresholds": {"decreaseFactor": 0.8999999761581421, "increaseFactor": 1.100000023841858, "initialValue": 20000.0, "max": 0.0, "min": 0.0}, "type": 0}, "featureMaintainer": {"enable": true, "lostFeatureErrorThreshold": 50000.0, "minimumDistanceBetweenFeatures": 50.0, "trackedFeatureThreshold": 200000.0}, "motionEstimator": {"enable": true, "opticalFlow": {"epsilon": 0.009999999776482582, "maxIterations": 9, "pyramidLevels": 0, "searchWindowHeight": 5, "searchWindowWidth": 5}, "type": 0}}, "numMemorySlices": 2, "numShaves": 2}}], [1, {"alias": "", "id": 1, "ioInfo": [[["", "out"], {"blocking": false, "group": "", "id": 6, "name": "out", "queueSize": 8, "type": 0, "waitForMessage": false}], [["", "inputImage"], {"blocking": true, "group": "", "id": 5, "name": "inputImage", "queueSize": 3, "type": 3, "waitForMessage": false}], [["", "inputConfig"], {"blocking": true, "group": "", "id": 4, "name": "inputConfig", "queueSize": 3, "type": 3, "waitForMessage": false}]], "logLevel": 3, "name": "ImageManip", "parentId": -1, "properties": {"backend": 0, "initialConfig": {"base": {"background": 0, "backgroundB": 0, "backgroundG": 0, "backgroundR": 0, "center": true, "colormap": 0, "operations": [], "outputHeight": 0, "outputWidth": 0, "resizeMode": 0, "undistort": false}, "outputFrameType": 30, "reusePreviousImage": false, "skipCurrentImage": false}, "numFramesPool": 4, "outputFrameSize": 1048576, "performanceMode": 0}}], [0, {"alias": "", "id": 0, "ioInfo": [[["dynamicOutputs", "0"], {"blocking": false, "group": "dynamicOutputs", "id": 3, "name": "0", "queueSize": 8, "type": 0, "waitForMessage": false}], [["", "raw"], {"blocking": false, "group": "", "id": 2, "name": "raw", "queueSize": 8, "type": 0, "waitForMessage": false}], [["", "mockIsp"], {"blocking": true, "group": "", "id": 1, "name": "mockIsp", "queueSize": 8, "type": 3, "waitForMessage": false}], [["", "inputControl"], {"blocking": true, "group": "", "id": 0, "name": "inputControl", "queueSize": 3, "type": 3, "waitForMessage": false}]], "logLevel": 3, "name": "Camera", "parentId": -1, "properties": {"boardSocket": 0, "cameraName": "", "fps": -1.0, "imageOrientation": -1, "initialControl": {"aeLockMode": false, "aeMaxExposureTimeUs": 0, "aeRegion": {"height": 0, "priority": 0, "width": 0, "x": 0, "y": 0}, "afRegion": {"height": 0, "priority": 0, "width": 0, "x": 0, "y": 0}, "antiBandingMode": 0, "autoFocusMode": 3, "awbLockMode": false, "awbMode": 0, "brightness": 0, "captureIntent": 0, "chromaDenoise": 0, "cmdMask": 0, "contrast": 0, "controlMode": 0, "effectMode": 0, "enableHdr": false, "expCompensation": 0, "expManual": {"exposureTimeUs": 0, "frameDurationUs": 0, "sensitivityIso": 0}, "frameSyncMode": 0, "lensPosAutoInfinity": 0, "lensPosAutoMacro": 0, "lensPosition": 0, "lensPositionRaw": 0.0, "lowPowerNumFramesBurst": 0, "lowPowerNumFramesDiscard": 0, "lumaDenoise": 0, "miscControls": [], "saturation": 0, "sceneMode": 0, "sharpness": 0, "strobeConfig": {"activeLevel": 0, "enable": 0, "gpioNumber": 0}, "strobeTimings": {"durationUs": 0, "exposureBeginOffsetUs": 0, "exposureEndOffsetUs": 0}, "wbColorTemp": 0}, "isp3aFps": 0, "mockIspHeight": -1, "mockIspWidth": -1, "numFramesPoolIsp": 3, "numFramesPoolPreview": 4, "numFramesPoolRaw": 3, "numFramesPoolStill": 4, "numFramesPoolVideo": 4, "outputRequests": [{"enableUndistortion": null, "fps": {"value": null}, "resizeMode": 0, "size": {"value": {"index": 0, "value": [640, 640]}}, "type": 22}], "resolutionHeight": -1, "resolutionWidth": -1}}]]}}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.