# IMU and Video Sync

This example demonstrates the use of the DepthAI Sync node to synchronize IMU (Inertial Measurement Unit) data with video frames
from a color camera. It highlights the capability to process and display the latest rotation vector from the IMU alongside the
video stream in real-time.

### Similar samples:

 * [Depth and Video Sync](https://docs.luxonis.com/software/depthai/examples/depth_video_sync.md)
 * [Multiple Scripts Sync](https://docs.luxonis.com/software/depthai/examples/scripts_sync.md)

## Demo

```bash
~/depthai-python/examples/Sync $ python3 imu_video_synced.py
IMU type: BNO086, firmware version: 3.9.7

Device timestamp imu: 0:00:05.379914
Device timestamp video:0:00:05.385096
Quaternion: i: -0.0549 j: -0.0335 k: 0.0018 real: 0.9979

Device timestamp imu: 0:00:05.410274
Device timestamp video:0:00:05.418425
Quaternion: i: -0.0549 j: -0.0334 k: 0.0018 real: 0.9979

Device timestamp imu: 0:00:05.445439
Device timestamp video:0:00:05.451753
Quaternion: i: -0.0548 j: -0.0334 k: 0.0018 real: 0.9979

Device timestamp imu: 0:00:05.475084
Device timestamp video:0:00:05.485082
Quaternion: i: -0.0547 j: -0.0334 k: 0.0018 real: 0.9979

Device timestamp imu: 0:00:05.510046
Device timestamp video:0:00:05.518411
Quaternion: i: -0.0546 j: -0.0334 k: 0.0018 real: 0.9979
```

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
import depthai as dai
import numpy as np
import cv2
from datetime import timedelta

device = dai.Device()

imuType = device.getConnectedIMU()
imuFirmwareVersion = device.getIMUFirmwareVersion()
print(f"IMU type: {imuType}, firmware version: {imuFirmwareVersion}")

if imuType != "BNO086":
    print("Rotation vector output is supported only by BNO086!")
    exit(0)

pipeline = dai.Pipeline()

color = pipeline.create(dai.node.ColorCamera)
imu = pipeline.create(dai.node.IMU)
sync = pipeline.create(dai.node.Sync)
xoutImu = pipeline.create(dai.node.XLinkOut)
xoutImu.setStreamName("imu")

xoutGrp = pipeline.create(dai.node.XLinkOut)
xoutGrp.setStreamName("xout")

color.setCamera("color")

imu.enableIMUSensor(dai.IMUSensor.ROTATION_VECTOR, 120)
imu.setBatchReportThreshold(1)
imu.setMaxBatchReports(10)

sync.setSyncThreshold(timedelta(milliseconds=10))
sync.setSyncAttempts(-1)

color.video.link(sync.inputs["video"])
imu.out.link(sync.inputs["imu"])

sync.out.link(xoutGrp.input)

with device:
    device.startPipeline(pipeline)
    groupQueue = device.getOutputQueue("xout", 3, True)
    while True:
        groupMessage = groupQueue.get()
        imuMessage = groupMessage["imu"]
        colorMessage = groupMessage["video"]
        print()
        print("Device timestamp imu: " + str(imuMessage.getTimestampDevice()))
        print("Device timestamp video:" + str(colorMessage.getTimestampDevice()))
        latestRotationVector = imuMessage.packets[-1].rotationVector
        imuF = "{:.4f}"
        print(f"Quaternion: i: {imuF.format(latestRotationVector.i)} j: {imuF.format(latestRotationVector.j)} "
        f"k: {imuF.format(latestRotationVector.k)} real: {imuF.format(latestRotationVector.real)}")
        print()
        cv2.imshow("video", colorMessage.getCvFrame())
        if cv2.waitKey(1) == ord("q"):
            break
```

#### C++

```cpp
#include <iostream>
#include <opencv2/opencv.hpp>

#include "depthai/depthai.hpp"

int main() {
    dai::Device device;

    auto imuType = device.getConnectedIMU();
    auto imuFirmwareVersion = device.getIMUFirmwareVersion();
    std::cout << "IMU type: " << imuType << ", firmware version: " << imuFirmwareVersion << std::endl;

    if(imuType != "BNO086") {
        std::cout << "Rotation vector output is supported only by BNO086!" << std::endl;
        return 1;
    }

    dai::Pipeline pipeline;

    auto colorCamera = pipeline.create<dai::node::ColorCamera>();
    auto imu = pipeline.create<dai::node::IMU>();
    auto sync = pipeline.create<dai::node::Sync>();
    auto xoutGroup = pipeline.create<dai::node::XLinkOut>();

    xoutGroup->setStreamName("xout");

    colorCamera->setCamera("color");

    imu->enableIMUSensor(dai::IMUSensor::ROTATION_VECTOR, 120);
    imu->setBatchReportThreshold(1);
    imu->setMaxBatchReports(10);

    sync->setSyncThreshold(std::chrono::milliseconds(10));
    sync->setSyncAttempts(-1);  // Infinite attempts

    colorCamera->video.link(sync->inputs["video"]);
    imu->out.link(sync->inputs["imu"]);

    sync->out.link(xoutGroup->input);

    device.startPipeline(pipeline);

    auto groupQueue = device.getOutputQueue("xout", 3, false);

    while(true) {
        auto groupMessage = groupQueue->get<dai::MessageGroup>();
        auto imuData = groupMessage->get<dai::IMUData>("imu");
        auto colorData = groupMessage->get<dai::ImgFrame>("video");
        auto timeDifference = imuData->getTimestampDevice() - colorData->getTimestampDevice();
        auto timeDifferenceUs = std::chrono::duration_cast<std::chrono::microseconds>(timeDifference).count();

        std::cout << "Time difference between messages is: " << std::abs(timeDifferenceUs / 1000.0) << " ms" << std::endl;

        for(auto& packet : imuData->packets) {
            auto& rv = packet.rotationVector;

            printf(
                "Quaternion: i: %.3f j: %.3f k: %.3f real: %.3f\n"
                "Accuracy (rad): %.3f \n",
                rv.i,
                rv.j,
                rv.k,
                rv.real,
                rv.rotationVectorAccuracy);
        }

        cv::imshow("Color", colorData->getCvFrame());
        if(cv::waitKey(1) == 'q') {
            break;
        }
    }

    return 0;
}
```

### How it Works

 * Initialize the DepthAI device.
 * Check the connected IMU type and firmware version.
 * Create a pipeline and add a ColorCamera and IMU node.
 * Set up the Sync node to synchronize the IMU data with the video frames.
 * Link the output of the ColorCamera and IMU nodes to the Sync node.
 * Start the pipeline and continuously receive synchronized data.
 * Display the video frames and print the IMU rotation vector data, including quaternion values.

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.