# Multiple devices

For many applications it's useful to have multiple OAK cameras running at the same time, as more cameras can perceive more (of the
world around them). Examples here would include:

 * [Box measurement](https://github.com/luxonis/oak-examples/tree/master/gen2-box_measurement) app, multiple cameras from multiple
   different perspectives could provide better dimension estimation
 * [People counter/tracker](https://github.com/luxonis/oak-examples/tree/master/gen2-people-tracker#gen2-people-tracker) app,
   multiple cameras could count/track people across a large area (eg. shopping mall)
 * Attaching multiple cameras on front/back/left/right side of your robot for full 360° vision, so your robot can perceive the
   whole area around it regardless of how it's positioned.

This example shows how you can use multiple OAK cameras on a single host. The demo will find all devices connected to the host
computer and display an RGB preview from each of the camera.

An demo application that does object detection from multiple cameras can be [found
here](https://github.com/luxonis/oak-examples/tree/master/gen2-multiple-devices).

## Demo

```bash
Connected to  18443010F105060F00
        >>> MXID: 18443010F105060F00
        >>> Num of cameras: 3
        >>> USB speed: UsbSpeed.SUPER
        >>> Board name: DM9098
        >>> Product name: OAK-D S2 FF
    Connected to  1844301011F4C51200
        >>> MXID: 1844301011F4C51200
        >>> Num of cameras: 3
        >>> USB speed: UsbSpeed.UNKNOWN
        >>> Board name: NG9097
        >>> Product name: OAK-D Pro PoE AF
```

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
import contextlib

def createPipeline():
    # Start defining a pipeline
    pipeline = dai.Pipeline()
    # Define a source - color camera
    camRgb = pipeline.create(dai.node.ColorCamera)

    camRgb.setPreviewSize(300, 300)
    camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
    camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
    camRgb.setInterleaved(False)

    # Create output
    xoutRgb = pipeline.create(dai.node.XLinkOut)
    xoutRgb.setStreamName("rgb")
    camRgb.preview.link(xoutRgb.input)

    return pipeline

with contextlib.ExitStack() as stack:
    deviceInfos = dai.Device.getAllAvailableDevices()
    usbSpeed = dai.UsbSpeed.SUPER
    openVinoVersion = dai.OpenVINO.Version.VERSION_2021_4

    qRgbMap = []
    devices = []

    for deviceInfo in deviceInfos:
        deviceInfo: dai.DeviceInfo
        device: dai.Device = stack.enter_context(dai.Device(openVinoVersion, deviceInfo, usbSpeed))
        devices.append(device)
        print("===Connected to ", deviceInfo.getMxId())
        mxId = device.getMxId()
        cameras = device.getConnectedCameras()
        usbSpeed = device.getUsbSpeed()
        eepromData = device.readCalibration2().getEepromData()
        print("   >>> MXID:", mxId)
        print("   >>> Num of cameras:", len(cameras))
        print("   >>> USB speed:", usbSpeed)
        if eepromData.boardName != "":
            print("   >>> Board name:", eepromData.boardName)
        if eepromData.productName != "":
            print("   >>> Product name:", eepromData.productName)

        pipeline = createPipeline()
        device.startPipeline(pipeline)

        # Output queue will be used to get the rgb frames from the output defined above
        q_rgb = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
        stream_name = "rgb-" + mxId + "-" + eepromData.productName
        qRgbMap.append((q_rgb, stream_name))

    while True:
        for q_rgb, stream_name in qRgbMap:
            if q_rgb.has():
                cv2.imshow(stream_name, q_rgb.get().getCvFrame())

        if cv2.waitKey(1) == ord('q'):
            break
```

#### C++

```cpp
#include <chrono>
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

std::shared_ptr<dai::Pipeline> createPipeline() {
    // Start defining a pipeline
    auto pipeline = std::make_shared<dai::Pipeline>();
    // Define a source - color camera
    auto camRgb = pipeline->create<dai::node::ColorCamera>();

    camRgb->setPreviewSize(300, 300);
    camRgb->setBoardSocket(dai::CameraBoardSocket::CAM_A);
    camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_1080_P);
    camRgb->setInterleaved(false);

    // Create output
    auto xoutRgb = pipeline->create<dai::node::XLinkOut>();
    xoutRgb->setStreamName("rgb");
    camRgb->preview.link(xoutRgb->input);

    return pipeline;
}

int main(int argc, char** argv) {
    auto deviceInfoVec = dai::Device::getAllAvailableDevices();
    const auto usbSpeed = dai::UsbSpeed::SUPER;
    auto openVinoVersion = dai::OpenVINO::Version::VERSION_2021_4;

    std::map<std::string, std::shared_ptr<dai::DataOutputQueue>> qRgbMap;
    std::vector<std::shared_ptr<dai::Device>> devices;

    for(auto& deviceInfo : deviceInfoVec) {
        auto device = std::make_shared<dai::Device>(openVinoVersion, deviceInfo, usbSpeed);
        devices.push_back(device);
        std::cout << "===Connected to " << deviceInfo.getMxId() << std::endl;
        auto mxId = device->getMxId();
        auto cameras = device->getConnectedCameras();
        auto usbSpeed = device->getUsbSpeed();
        auto eepromData = device->readCalibration2().getEepromData();
        std::cout << "   >>> MXID:" << mxId << std::endl;
        std::cout << "   >>> Num of cameras:" << cameras.size() << std::endl;
        std::cout << "   >>> USB speed:" << usbSpeed << std::endl;
        if(eepromData.boardName != "") {
            std::cout << "   >>> Board name:" << eepromData.boardName << std::endl;
        }
        if(eepromData.productName != "") {
            std::cout << "   >>> Product name:" << eepromData.productName << std::endl;
        }
        auto pipeline = createPipeline();
        device->startPipeline(*pipeline);

        auto qRgb = device->getOutputQueue("rgb", 4, false);
        std::string streamName = "rgb-" + eepromData.productName + mxId;
        qRgbMap.insert({streamName, qRgb});
    }
    while(true) {
        for(auto& element : qRgbMap) {
            auto qRgb = element.second;
            auto streamName = element.first;
            auto inRgb = qRgb->tryGet<dai::ImgFrame>();
            if(inRgb != nullptr) {
                cv::imshow(streamName, inRgb->getCvFrame());
            }
        }

        int key = cv::waitKey(1);
        if(key == 'q' || key == 'Q') {
            return 0;
        }
    }
    return 0;
}
```

## Pipeline

### examples/multiple_devices.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "preview",
        "node1OutputGroup": "",
        "node2Id": 1,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "inputConfig"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 1,
                "name": "inputConfig",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 6,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "still"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 7,
                "name": "still",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "video"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 3,
                "name": "video",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "isp"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 4,
                "name": "isp",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "preview"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 5,
                "name": "preview",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 8,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "ColorCamera",
          "properties": {
            "boardSocket": 0,
            "cameraName": "",
            "colorOrder": 0,
            "fp16": false,
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "interleaved": false,
            "isp3aFps": 0,
            "ispScale": {
              "horizDenominator": 0,
              "horizNumerator": 0,
              "vertDenominator": 0,
              "vertNumerator": 0
            },
            "numFramesPoolIsp": 3,
            "numFramesPoolPreview": 4,
            "numFramesPoolRaw": 3,
            "numFramesPoolStill": 4,
            "numFramesPoolVideo": 4,
            "previewHeight": 300,
            "previewKeepAspectRatio": true,
            "previewWidth": 300,
            "rawPacked": null,
            "resolution": 0,
            "sensorCropX": -1.0,
            "sensorCropY": -1.0,
            "stillHeight": -1,
            "stillWidth": -1,
            "videoHeight": -1,
            "videoWidth": -1
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 9,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "rgb"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.