# RGB Camera Control

This example shows how to control the [ColorCamera](https://docs.luxonis.com/software/depthai-components/nodes/color_camera.md),
such as exposure, sensitivity, white balance, luma/chroma denoise, device-side crop, camera triggers, etc.

An output is a full frame along with cropped frame (video) which can be moved with WASD keys.

List of all controls:

```bash
Uses 'WASD' controls to move the crop window, 'C' to capture a still image, 'T' to
  trigger autofocus, 'IOKL,.NM' for manual exposure/focus/white-balance:
Control:  key[dec/inc]  min..max
exposure time: I   O  1..33000 [us]
sensitivity iso:   K   L100..1600
focus: ,   .  0..255 [far..near]
white balance: N   M   1000..12000 (light color temperature K)

  To go back to auto controls:
'E' - autoexposure
'F' - autofocus (continuous)
'B' - auto white-balance

  Other controls:
'1' - AWB lock (true / false)
'2' - AE lock (true / false)
'3' - Select control: AWB mode
'4' - Select control: AE compensation
'5' - Select control: anti-banding/flicker mode
'6' - Select control: effect mode
'7' - Select control: brightness
'8' - Select control: contrast
'9' - Select control: saturation
'0' - Select control: sharpness
'[' - Select control: luma denoise
']' - Select control: chroma denoise

  For the 'Select control: ...' options, use these keys to modify the value:
'-' or '_' to decrease
'+' or '=' to increase
```

### Similar samples:

 * [Mono Camera Control](https://docs.luxonis.com/software/depthai/examples/mono_camera_control.md)
 * [Depth Crop Control](https://docs.luxonis.com/software/depthai/examples/depth_crop_control.md)

## Demo

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

"""
This example shows usage of Camera Control message as well as ColorCamera configInput to change crop x and y
Uses 'WASD' controls to move the crop window, 'C' to capture a still image, 'T' to trigger autofocus, 'IOKL,.NM'
for manual exposure/focus/white-balance:
  Control:      key[dec/inc]  min..max
  exposure time:     I   O      1..33000 [us]
  sensitivity iso:   K   L    100..1600
  focus:             ,   .      0..255 [far..near]
  white balance:     N   M   1000..12000 (light color temperature K)

To go back to auto controls:
  'E' - autoexposure
  'F' - autofocus (continuous)
  'B' - auto white-balance

Other controls:
    '1' - AWB lock (true / false)
    '2' - AE lock (true / false)
    '3' - Select control: AWB mode
    '4' - Select control: AE compensation
    '5' - Select control: anti-banding/flicker mode
    '6' - Select control: effect mode
    '7' - Select control: brightness
    '8' - Select control: contrast
    '9' - Select control: saturation
    '0' - Select control: sharpness
    '[' - Select control: luma denoise
    ']' - Select control: chroma denoise

For the 'Select control: ...' options, use these keys to modify the value:
  '-' or '_' to decrease
  '+' or '=' to increase

'/' to toggle showing camera settings: exposure, ISO, lens position, color temperature
"""

import depthai as dai
import cv2
from itertools import cycle

# Step size ('W','A','S','D' controls)
STEP_SIZE = 8
# Manual exposure/focus/white-balance set step
EXP_STEP = 500  # us
ISO_STEP = 50
LENS_STEP = 3
WB_STEP = 200

def clamp(num, v0, v1):
    return max(v0, min(num, v1))

# Create pipeline
pipeline = dai.Pipeline()

# Define sources and outputs
camRgb = pipeline.create(dai.node.ColorCamera)
camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
camRgb.setIspScale(2,3) # 1080P -> 720P
stillEncoder = pipeline.create(dai.node.VideoEncoder)

controlIn = pipeline.create(dai.node.XLinkIn)
configIn = pipeline.create(dai.node.XLinkIn)
ispOut = pipeline.create(dai.node.XLinkOut)
videoOut = pipeline.create(dai.node.XLinkOut)
stillMjpegOut = pipeline.create(dai.node.XLinkOut)

controlIn.setStreamName('control')
configIn.setStreamName('config')
ispOut.setStreamName('isp')
videoOut.setStreamName('video')
stillMjpegOut.setStreamName('still')

# Properties
camRgb.setVideoSize(640,360)
stillEncoder.setDefaultProfilePreset(1, dai.VideoEncoderProperties.Profile.MJPEG)

# Linking
camRgb.isp.link(ispOut.input)
camRgb.still.link(stillEncoder.input)
camRgb.video.link(videoOut.input)
controlIn.out.link(camRgb.inputControl)
configIn.out.link(camRgb.inputConfig)
stillEncoder.bitstream.link(stillMjpegOut.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Get data queues
    controlQueue = device.getInputQueue('control')
    configQueue = device.getInputQueue('config')
    ispQueue = device.getOutputQueue('isp')
    videoQueue = device.getOutputQueue('video')
    stillQueue = device.getOutputQueue('still')

    # Max cropX & cropY
    maxCropX = (camRgb.getIspWidth() - camRgb.getVideoWidth()) / camRgb.getIspWidth()
    maxCropY = (camRgb.getIspHeight() - camRgb.getVideoHeight()) / camRgb.getIspHeight()
    print(maxCropX, maxCropY, camRgb.getIspWidth(), camRgb.getVideoHeight())

    # Default crop
    cropX = 0
    cropY = 0
    sendCamConfig = True

    # Defaults and limits for manual focus/exposure controls
    lensPos = 150
    expTime = 20000
    sensIso = 800    
    wbManual = 4000
    ae_comp = 0
    ae_lock = False
    awb_lock = False
    saturation = 0
    contrast = 0
    brightness = 0
    sharpness = 0
    luma_denoise = 0
    chroma_denoise = 0
    control = 'none'
    show = False

    awb_mode = cycle([item for name, item in vars(dai.CameraControl.AutoWhiteBalanceMode).items() if name.isupper()])
    anti_banding_mode = cycle([item for name, item in vars(dai.CameraControl.AntiBandingMode).items() if name.isupper()])
    effect_mode = cycle([item for name, item in vars(dai.CameraControl.EffectMode).items() if name.isupper()])

    while True:
        vidFrames = videoQueue.tryGetAll()
        for vidFrame in vidFrames:
            cv2.imshow('video', vidFrame.getCvFrame())

        ispFrames = ispQueue.tryGetAll()
        for ispFrame in ispFrames:
            if show:
                txt = f"[{ispFrame.getSequenceNum()}] "
                txt += f"Exposure: {ispFrame.getExposureTime().total_seconds()*1000:.3f} ms, "
                txt += f"ISO: {ispFrame.getSensitivity()}, "
                txt += f"Lens position: {ispFrame.getLensPosition()}, "
                txt += f"Color temp: {ispFrame.getColorTemperature()} K"
                print(txt)
            cv2.imshow('isp', ispFrame.getCvFrame())

            # Send new cfg to camera
            if sendCamConfig:
                cfg = dai.ImageManipConfig()
                cfg.setCropRect(cropX, cropY, 0, 0)
                configQueue.send(cfg)
                print('Sending new crop - x: ', cropX, ' y: ', cropY)
                sendCamConfig = False

        stillFrames = stillQueue.tryGetAll()
        for stillFrame in stillFrames:
            # Decode JPEG
            frame = cv2.imdecode(stillFrame.getData(), cv2.IMREAD_UNCHANGED)
            # Display
            cv2.imshow('still', frame)

        # Update screen (1ms pooling rate)
        key = cv2.waitKey(1)
        if key == ord('q'):
            break
        elif key == ord('/'):
            show = not show
            if not show: print("Printing camera settings: OFF")
        elif key == ord('c'):
            ctrl = dai.CameraControl()
            ctrl.setCaptureStill(True)
            controlQueue.send(ctrl)
        elif key == ord('t'):
            print("Autofocus trigger (and disable continuous)")
            ctrl = dai.CameraControl()
            ctrl.setAutoFocusMode(dai.CameraControl.AutoFocusMode.AUTO)
            ctrl.setAutoFocusTrigger()
            controlQueue.send(ctrl)
        elif key == ord('f'):
            print("Autofocus enable, continuous")
            ctrl = dai.CameraControl()
            ctrl.setAutoFocusMode(dai.CameraControl.AutoFocusMode.CONTINUOUS_VIDEO)
            controlQueue.send(ctrl)
        elif key == ord('e'):
            print("Autoexposure enable")
            ctrl = dai.CameraControl()
            ctrl.setAutoExposureEnable()
            controlQueue.send(ctrl)
        elif key == ord('b'):
            print("Auto white-balance enable")
            ctrl = dai.CameraControl()
            ctrl.setAutoWhiteBalanceMode(dai.CameraControl.AutoWhiteBalanceMode.AUTO)
            controlQueue.send(ctrl)
        elif key in [ord(','), ord('.')]:
            if key == ord(','): lensPos -= LENS_STEP
            if key == ord('.'): lensPos += LENS_STEP
            lensPos = clamp(lensPos, 0, 255)
            print("Setting manual focus, lens position: ", lensPos)
            ctrl = dai.CameraControl()
            ctrl.setManualFocus(lensPos)
            controlQueue.send(ctrl)
        elif key in [ord('i'), ord('o'), ord('k'), ord('l')]:
            if key == ord('i'): expTime -= EXP_STEP
            if key == ord('o'): expTime += EXP_STEP
            if key == ord('k'): sensIso -= ISO_STEP
            if key == ord('l'): sensIso += ISO_STEP
            expTime = clamp(expTime, 1, 33000)
            sensIso = clamp(sensIso, 100, 1600)
            print("Setting manual exposure, time: ", expTime, "iso: ", sensIso)
            ctrl = dai.CameraControl()
            ctrl.setManualExposure(expTime, sensIso)
            controlQueue.send(ctrl)
        elif key in [ord('n'), ord('m')]:
            if key == ord('n'): wbManual -= WB_STEP
            if key == ord('m'): wbManual += WB_STEP
            wbManual = clamp(wbManual, 1000, 12000)
            print("Setting manual white balance, temperature: ", wbManual, "K")
            ctrl = dai.CameraControl()
            ctrl.setManualWhiteBalance(wbManual)
            controlQueue.send(ctrl)
        elif key in [ord('w'), ord('a'), ord('s'), ord('d')]:
            if key == ord('a'):
                cropX = cropX - (maxCropX / camRgb.getResolutionWidth()) * STEP_SIZE
                if cropX < 0: cropX = 0
            elif key == ord('d'):
                cropX = cropX + (maxCropX / camRgb.getResolutionWidth()) * STEP_SIZE
                if cropX > maxCropX: cropX = maxCropX
            elif key == ord('w'):
                cropY = cropY - (maxCropY / camRgb.getResolutionHeight()) * STEP_SIZE
                if cropY < 0: cropY = 0
            elif key == ord('s'):
                cropY = cropY + (maxCropY / camRgb.getResolutionHeight()) * STEP_SIZE
                if cropY > maxCropY: cropY = maxCropY
            sendCamConfig = True
        elif key == ord('1'):
            awb_lock = not awb_lock
            print("Auto white balance lock:", awb_lock)
            ctrl = dai.CameraControl()
            ctrl.setAutoWhiteBalanceLock(awb_lock)
            controlQueue.send(ctrl)
        elif key == ord('2'):
            ae_lock = not ae_lock
            print("Auto exposure lock:", ae_lock)
            ctrl = dai.CameraControl()
            ctrl.setAutoExposureLock(ae_lock)
            controlQueue.send(ctrl)
        elif key >= 0 and chr(key) in '34567890[]':
            if   key == ord('3'): control = 'awb_mode'
            elif key == ord('4'): control = 'ae_comp'
            elif key == ord('5'): control = 'anti_banding_mode'
            elif key == ord('6'): control = 'effect_mode'
            elif key == ord('7'): control = 'brightness'
            elif key == ord('8'): control = 'contrast'
            elif key == ord('9'): control = 'saturation'
            elif key == ord('0'): control = 'sharpness'
            elif key == ord('['): control = 'luma_denoise'
            elif key == ord(']'): control = 'chroma_denoise'
            print("Selected control:", control)
        elif key in [ord('-'), ord('_'), ord('+'), ord('=')]:
            change = 0
            if key in [ord('-'), ord('_')]: change = -1
            if key in [ord('+'), ord('=')]: change = 1
            ctrl = dai.CameraControl()
            if control == 'none':
                print("Please select a control first using keys 3..9 0 [ ]")
            elif control == 'ae_comp':
                ae_comp = clamp(ae_comp + change, -9, 9)
                print("Auto exposure compensation:", ae_comp)
                ctrl.setAutoExposureCompensation(ae_comp)
            elif control == 'anti_banding_mode':
                abm = next(anti_banding_mode)
                print("Anti-banding mode:", abm)
                ctrl.setAntiBandingMode(abm)
            elif control == 'awb_mode':
                awb = next(awb_mode)
                print("Auto white balance mode:", awb)
                ctrl.setAutoWhiteBalanceMode(awb)
            elif control == 'effect_mode':
                eff = next(effect_mode)
                print("Effect mode:", eff)
                ctrl.setEffectMode(eff)
            elif control == 'brightness':
                brightness = clamp(brightness + change, -10, 10)
                print("Brightness:", brightness)
                ctrl.setBrightness(brightness)
            elif control == 'contrast':
                contrast = clamp(contrast + change, -10, 10)
                print("Contrast:", contrast)
                ctrl.setContrast(contrast)
            elif control == 'saturation':
                saturation = clamp(saturation + change, -10, 10)
                print("Saturation:", saturation)
                ctrl.setSaturation(saturation)
            elif control == 'sharpness':
                sharpness = clamp(sharpness + change, 0, 4)
                print("Sharpness:", sharpness)
                ctrl.setSharpness(sharpness)
            elif control == 'luma_denoise':
                luma_denoise = clamp(luma_denoise + change, 0, 4)
                print("Luma denoise:", luma_denoise)
                ctrl.setLumaDenoise(luma_denoise)
            elif control == 'chroma_denoise':
                chroma_denoise = clamp(chroma_denoise + change, 0, 4)
                print("Chroma denoise:", chroma_denoise)
                ctrl.setChromaDenoise(chroma_denoise)
            controlQueue.send(ctrl)
```

#### C++

```cpp
/**
 * This example shows usage of Camera Control message as well as ColorCamera configInput to change crop x and y
 * Uses 'WASD' controls to move the crop window, 'C' to capture a still image, 'T' to trigger autofocus, 'IOKL,.[]'
 * for manual exposure/focus/white-balance:
 *   Control:      key[dec/inc]  min..max
 *   exposure time:     I   O      1..33000 [us]
 *   sensitivity iso:   K   L    100..1600
 *   focus:             ,   .      0..255 [far..near]
 *   white balance:     [   ]   1000..12000 (light color temperature K)
 * To go back to auto controls:
 *   'E' - autoexposure
 *   'F' - autofocus (continuous)
 *   'B' - auto white-balance
 */
#include <iostream>

#include "utility.hpp"

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

// Step size ('W','A','S','D' controls)
static constexpr int STEP_SIZE = 8;

// Manual exposure/focus set step
static constexpr int EXP_STEP = 500;  // us
static constexpr int ISO_STEP = 50;
static constexpr int LENS_STEP = 3;
static constexpr int WB_STEP = 200;

static int clamp(int num, int v0, int v1) {
    return std::max(v0, std::min(num, v1));
}

int main() {
    // Create pipeline
    dai::Pipeline pipeline;

    // Define sources and outputs
    auto camRgb = pipeline.create<dai::node::ColorCamera>();
    auto videoEncoder = pipeline.create<dai::node::VideoEncoder>();
    auto stillEncoder = pipeline.create<dai::node::VideoEncoder>();

    auto controlIn = pipeline.create<dai::node::XLinkIn>();
    auto configIn = pipeline.create<dai::node::XLinkIn>();
    auto videoMjpegOut = pipeline.create<dai::node::XLinkOut>();
    auto stillMjpegOut = pipeline.create<dai::node::XLinkOut>();
    auto previewOut = pipeline.create<dai::node::XLinkOut>();

    controlIn->setStreamName("control");
    configIn->setStreamName("config");
    videoMjpegOut->setStreamName("video");
    stillMjpegOut->setStreamName("still");
    previewOut->setStreamName("preview");

    // Properties
    camRgb->setVideoSize(640, 360);
    camRgb->setPreviewSize(300, 300);
    videoEncoder->setDefaultProfilePreset(camRgb->getFps(), dai::VideoEncoderProperties::Profile::MJPEG);
    stillEncoder->setDefaultProfilePreset(1, dai::VideoEncoderProperties::Profile::MJPEG);

    // Linking
    camRgb->video.link(videoEncoder->input);
    camRgb->still.link(stillEncoder->input);
    camRgb->preview.link(previewOut->input);
    controlIn->out.link(camRgb->inputControl);
    configIn->out.link(camRgb->inputConfig);
    videoEncoder->bitstream.link(videoMjpegOut->input);
    stillEncoder->bitstream.link(stillMjpegOut->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Get data queues
    auto controlQueue = device.getInputQueue("control");
    auto configQueue = device.getInputQueue("config");
    auto previewQueue = device.getOutputQueue("preview");
    auto videoQueue = device.getOutputQueue("video");
    auto stillQueue = device.getOutputQueue("still");

    // Max cropX & cropY
    float maxCropX = (camRgb->getResolutionWidth() - camRgb->getVideoWidth()) / (float)camRgb->getResolutionWidth();
    float maxCropY = (camRgb->getResolutionHeight() - camRgb->getVideoHeight()) / (float)camRgb->getResolutionHeight();

    // Default crop
    float cropX = 0;
    float cropY = 0;
    bool sendCamConfig = true;

    // Defaults and limits for manual focus/exposure controls
    int lensPos = 150;
    int lensMin = 0;
    int lensMax = 255;

    int expTime = 20000;
    int expMin = 1;
    int expMax = 33000;

    int sensIso = 800;
    int sensMin = 100;
    int sensMax = 1600;

    int wbManual = 4000;
    int wbMin = 1000;
    int wbMax = 12000;

    while(true) {
        auto previewFrames = previewQueue->tryGetAll<dai::ImgFrame>();
        for(const auto& previewFrame : previewFrames) {
            cv::Mat frame(previewFrame->getHeight(), previewFrame->getWidth(), CV_8UC3, previewFrame->getData().data());
            cv::imshow("preview", frame);
        }

        auto videoFrames = videoQueue->tryGetAll<dai::ImgFrame>();
        for(const auto& videoFrame : videoFrames) {
            // Decode JPEG
            auto frame = cv::imdecode(videoFrame->getData(), cv::IMREAD_UNCHANGED);
            // Display
            cv::imshow("video", frame);

            // Send new cfg to camera
            if(sendCamConfig) {
                dai::ImageManipConfig cfg;
                cfg.setCropRect(cropX, cropY, 0, 0);
                configQueue->send(cfg);
                printf("Sending new crop - x: %f, y: %f\n", cropX, cropY);
                sendCamConfig = false;
            }
        }

        auto stillFrames = stillQueue->tryGetAll<dai::ImgFrame>();
        for(const auto& stillFrame : stillFrames) {
            // Decode JPEG
            auto frame = cv::imdecode(stillFrame->getData(), cv::IMREAD_UNCHANGED);
            // Display
            cv::imshow("still", frame);
        }

        // Update screen (1ms pooling rate)
        int key = cv::waitKey(1);
        if(key == 'q') {
            break;
        } else if(key == 'c') {
            dai::CameraControl ctrl;
            ctrl.setCaptureStill(true);
            controlQueue->send(ctrl);
        } else if(key == 't') {
            printf("Autofocus trigger (and disable continuous)\n");
            dai::CameraControl ctrl;
            ctrl.setAutoFocusMode(dai::CameraControl::AutoFocusMode::AUTO);
            ctrl.setAutoFocusTrigger();
            controlQueue->send(ctrl);
        } else if(key == 'f') {
            printf("Autofocus enable, continuous\n");
            dai::CameraControl ctrl;
            ctrl.setAutoFocusMode(dai::CameraControl::AutoFocusMode::CONTINUOUS_VIDEO);
            controlQueue->send(ctrl);
        } else if(key == 'e') {
            printf("Autoexposure enable\n");
            dai::CameraControl ctrl;
            ctrl.setAutoExposureEnable();
            controlQueue->send(ctrl);
        } else if(key == 'b') {
            printf("Auto white-balance enable\n");
            dai::CameraControl ctrl;
            ctrl.setAutoWhiteBalanceMode(dai::CameraControl::AutoWhiteBalanceMode::AUTO);
            controlQueue->send(ctrl);
        } else if(key == ',' || key == '.') {
            if(key == ',') lensPos -= LENS_STEP;
            if(key == '.') lensPos += LENS_STEP;
            lensPos = clamp(lensPos, lensMin, lensMax);
            printf("Setting manual focus, lens position: %d\n", lensPos);
            dai::CameraControl ctrl;
            ctrl.setManualFocus(lensPos);
            controlQueue->send(ctrl);
        } else if(key == 'i' || key == 'o' || key == 'k' || key == 'l') {
            if(key == 'i') expTime -= EXP_STEP;
            if(key == 'o') expTime += EXP_STEP;
            if(key == 'k') sensIso -= ISO_STEP;
            if(key == 'l') sensIso += ISO_STEP;
            expTime = clamp(expTime, expMin, expMax);
            sensIso = clamp(sensIso, sensMin, sensMax);
            printf("Setting manual exposure, time: %d, iso: %d\n", expTime, sensIso);
            dai::CameraControl ctrl;
            ctrl.setManualExposure(expTime, sensIso);
            controlQueue->send(ctrl);
        } else if(key == '[' || key == ']') {
            if(key == '[') wbManual -= WB_STEP;
            if(key == ']') wbManual += WB_STEP;
            wbManual = clamp(wbManual, wbMin, wbMax);
            printf("Setting manual white balance, temperature: %d K\n", wbManual);
            dai::CameraControl ctrl;
            ctrl.setManualWhiteBalance(wbManual);
            controlQueue->send(ctrl);
        } else if(key == 'w' || key == 'a' || key == 's' || key == 'd') {
            if(key == 'a') {
                cropX -= (maxCropX / camRgb->getResolutionWidth()) * STEP_SIZE;
                if(cropX < 0) cropX = maxCropX;
            } else if(key == 'd') {
                cropX += (maxCropX / camRgb->getResolutionWidth()) * STEP_SIZE;
                if(cropX > maxCropX) cropX = 0.0f;
            } else if(key == 'w') {
                cropY -= (maxCropY / camRgb->getResolutionHeight()) * STEP_SIZE;
                if(cropY < 0) cropY = maxCropY;
            } else if(key == 's') {
                cropY += (maxCropY / camRgb->getResolutionHeight()) * STEP_SIZE;
                if(cropY > maxCropY) cropY = 0.0f;
            }
            sendCamConfig = true;
        }
    }
    return 0;
}
```

## Pipeline

### examples/rgb_camera_control.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "isp",
        "node1OutputGroup": "",
        "node2Id": 4,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 0,
        "node1Output": "still",
        "node1OutputGroup": "",
        "node2Id": 1,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 0,
        "node1Output": "video",
        "node1OutputGroup": "",
        "node2Id": 5,
        "node2Input": "in",
        "node2InputGroup": ""
      },
      {
        "node1Id": 2,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 0,
        "node2Input": "inputControl",
        "node2InputGroup": ""
      },
      {
        "node1Id": 3,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 0,
        "node2Input": "inputConfig",
        "node2InputGroup": ""
      },
      {
        "node1Id": 1,
        "node1Output": "bitstream",
        "node1OutputGroup": "",
        "node2Id": 6,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "inputConfig"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 1,
                "name": "inputConfig",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 6,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "still"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 7,
                "name": "still",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "video"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 3,
                "name": "video",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "isp"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 4,
                "name": "isp",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "preview"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 5,
                "name": "preview",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 8,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "ColorCamera",
          "properties": {
            "boardSocket": -1,
            "cameraName": "",
            "colorOrder": 0,
            "fp16": false,
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "interleaved": true,
            "isp3aFps": 0,
            "ispScale": {
              "horizDenominator": 3,
              "horizNumerator": 2,
              "vertDenominator": 3,
              "vertNumerator": 2
            },
            "numFramesPoolIsp": 3,
            "numFramesPoolPreview": 4,
            "numFramesPoolRaw": 3,
            "numFramesPoolStill": 4,
            "numFramesPoolVideo": 4,
            "previewHeight": 300,
            "previewKeepAspectRatio": true,
            "previewWidth": 300,
            "rawPacked": null,
            "resolution": 0,
            "sensorCropX": -1.0,
            "sensorCropY": -1.0,
            "stillHeight": -1,
            "stillWidth": -1,
            "videoHeight": 360,
            "videoWidth": 640
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 9,
                "name": "in",
                "queueSize": 4,
                "type": 3,
                "waitForMessage": true
              }
            ],
            [
              [
                "",
                "bitstream"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 10,
                "name": "bitstream",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 11,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "VideoEncoder",
          "properties": {
            "bitrate": 0,
            "frameRate": 1.0,
            "keyframeFrequency": 30,
            "lossless": false,
            "maxBitrate": 0,
            "numBFrames": 0,
            "numFramesPool": 0,
            "outputFrameSize": 0,
            "profile": 4,
            "quality": 95,
            "rateCtrlMode": 0
          }
        }
      ],
      [
        2,
        {
          "id": 2,
          "ioInfo": [
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 12,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "XLinkIn",
          "properties": {
            "maxDataSize": 5242880,
            "numFrames": 8,
            "streamName": "control"
          }
        }
      ],
      [
        3,
        {
          "id": 3,
          "ioInfo": [
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 13,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "XLinkIn",
          "properties": {
            "maxDataSize": 5242880,
            "numFrames": 8,
            "streamName": "config"
          }
        }
      ],
      [
        4,
        {
          "id": 4,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 14,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "isp"
          }
        }
      ],
      [
        5,
        {
          "id": 5,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 15,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "video"
          }
        }
      ],
      [
        6,
        {
          "id": 6,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 16,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "still"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.