# Script HTTP client

> This example can only run on
> [OAK POE devices](https://docs.luxonis.com/hardware.md#poe-designs)
> . You need
> **bootloader**
> on/above version
> **0.0.15**
> . You can flash bootloader by running
> `python3 examples/bootloader/flash_bootloader.py`
> .

This example will send an [HTTP request](https://en.wikipedia.org/wiki/Hypertext_Transfer_Protocol) to the http://api.ipify.org
and print your public IP.

## Demo

```bash
~/depthai-python/examples/Script$ python3 script_http_client.py
Sending http GET request...
200 OK
Public IP: b'123.123.123.123'
```

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3
import depthai as dai

# Start defining a pipeline
pipeline = dai.Pipeline()

# Script node
script = pipeline.create(dai.node.Script)
script.setProcessor(dai.ProcessorType.LEON_CSS)
script.setScript("""
    import http.client
    import time

    node.warn('Sending http GET request...')
    h1 = http.client.HTTPConnection('api.ipify.org', 80)
    h1.request("GET", "/")
    r1 = h1.getresponse()
    node.warn(f'{r1.status} {r1.reason}')
    data1 = r1.read()
    node.warn(f'Public IP: {data1}')

    node.io['end'].send(Buffer(32))
""")

xout = pipeline.create(dai.node.XLinkOut)
xout.setStreamName('end')
script.outputs['end'].link(xout.input)

# Connect to device with pipeline
with dai.Device(pipeline) as device:
    device.getOutputQueue("end").get() # Wait for the "end" msg
```

#### C++

```cpp
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

int main() {
    using namespace std;

    // Start defining a pipeline
    dai::Pipeline pipeline;

    // Script node
    auto script = pipeline.create<dai::node::Script>();
    script->setProcessor(dai::ProcessorType::LEON_CSS);
    script->setScript(R"(
    import http.client
    import time

    node.warn('Sending http GET request...')
    h1 = http.client.HTTPConnection('api.ipify.org', 80)
    h1.request("GET", "/")
    r1 = h1.getresponse()
    node.warn(f'{r1.status} {r1.reason}')
    data1 = r1.read()
    node.warn(f'Public IP: {data1}')

    node.io['end'].send(Buffer(32))
    )");

    // XLinkOut
    auto xout = pipeline.create<dai::node::XLinkOut>();
    xout->setStreamName("end");
    script->outputs["end"].link(xout->input);

    // Connect to device with pipeline
    dai::Device device(pipeline);
    device.getOutputQueue("end")->get<dai::Buffer>();
    return 0;
}
```

## Pipeline

### examples/script_http_client.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "end",
        "node1OutputGroup": "io",
        "node2Id": 1,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "io",
                "end"
              ],
              {
                "blocking": false,
                "group": "io",
                "id": 1,
                "name": "end",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "Script",
          "properties": {
            "processor": 0,
            "scriptName": "<script>",
            "scriptUri": "asset:__script"
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "end"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.