# System information

This example shows how to get system information (memory usage, cpu usage and temperature) from the board.

## Demo

Example script output

```bash
Ddr used / total - 0.13 / 414.80 MiB
  Cmx used / total - 2.24 / 2.50 MiB
  LeonCss heap used / total - 4.17 / 46.41 MiB
  LeonMss heap used / total - 2.87 / 27.58 MiB
  Chip temperature - average: 38.59, css: 39.81, mss: 37.71, upa: 38.65, dss: 38.18
  Cpu usage - Leon CSS: 7.08%, Leon MSS: 1.48 %
  ----------------------------------------
  Ddr used / total - 0.13 / 414.80 MiB
  Cmx used / total - 2.24 / 2.50 MiB
  LeonCss heap used / total - 4.17 / 46.41 MiB
  LeonMss heap used / total - 2.87 / 27.58 MiB
  Chip temperature - average: 38.59, css: 39.58, mss: 37.94, upa: 38.18, dss: 38.65
  Cpu usage - Leon CSS: 1.55%, Leon MSS: 0.30 %
  ----------------------------------------
  Ddr used / total - 0.13 / 414.80 MiB
  Cmx used / total - 2.24 / 2.50 MiB
  LeonCss heap used / total - 4.17 / 46.41 MiB
  LeonMss heap used / total - 2.87 / 27.58 MiB
  Chip temperature - average: 38.94, css: 40.04, mss: 38.18, upa: 39.35, dss: 38.18
  Cpu usage - Leon CSS: 0.56%, Leon MSS: 0.06 %
  ----------------------------------------
  Ddr used / total - 0.13 / 414.80 MiB
  Cmx used / total - 2.24 / 2.50 MiB
  LeonCss heap used / total - 4.17 / 46.41 MiB
  LeonMss heap used / total - 2.87 / 27.58 MiB
  Chip temperature - average: 39.46, css: 40.28, mss: 38.88, upa: 39.81, dss: 38.88
  Cpu usage - Leon CSS: 0.51%, Leon MSS: 0.06 %
  ----------------------------------------
```

 * upa represents the temperature of the SHAVE block
 * dss represents the temperature of the DDR subsystem

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai

def printSystemInformation(info):
    m = 1024 * 1024 # MiB
    print(f"Ddr used / total - {info.ddrMemoryUsage.used / m:.2f} / {info.ddrMemoryUsage.total / m:.2f} MiB")
    print(f"Cmx used / total - {info.cmxMemoryUsage.used / m:.2f} / {info.cmxMemoryUsage.total / m:.2f} MiB")
    print(f"LeonCss heap used / total - {info.leonCssMemoryUsage.used / m:.2f} / {info.leonCssMemoryUsage.total / m:.2f} MiB")
    print(f"LeonMss heap used / total - {info.leonMssMemoryUsage.used / m:.2f} / {info.leonMssMemoryUsage.total / m:.2f} MiB")
    t = info.chipTemperature
    print(f"Chip temperature - average: {t.average:.2f}, css: {t.css:.2f}, mss: {t.mss:.2f}, upa: {t.upa:.2f}, dss: {t.dss:.2f}")
    print(f"Cpu usage - Leon CSS: {info.leonCssCpuUsage.average * 100:.2f}%, Leon MSS: {info.leonMssCpuUsage.average * 100:.2f} %")
    print("----------------------------------------")

# Create pipeline
pipeline = dai.Pipeline()

# Define source and output
sysLog = pipeline.create(dai.node.SystemLogger)
linkOut = pipeline.create(dai.node.XLinkOut)

linkOut.setStreamName("sysinfo")

# Properties
sysLog.setRate(1)  # 1 Hz

# Linking
sysLog.out.link(linkOut.input)

# Connect to device and start pipeline
with dai.Device(pipeline) as device:

    # Output queue will be used to get the system info
    qSysInfo = device.getOutputQueue(name="sysinfo", maxSize=4, blocking=False)

    while True:
        sysInfo = qSysInfo.get()  # Blocking call, will wait until a new data has arrived
        printSystemInformation(sysInfo)
```

#### C++

```cpp
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"
void printSystemInformation(dai::SystemInformation info) {
    printf("Ddr used / total - %.2f / %.2f MiB\n", info.ddrMemoryUsage.used / (1024.0f * 1024.0f), info.ddrMemoryUsage.total / (1024.0f * 1024.0f));
    printf("Cmx used / total - %.2f / %.2f MiB\n", info.cmxMemoryUsage.used / (1024.0f * 1024.0f), info.cmxMemoryUsage.total / (1024.0f * 1024.0f));
    printf("LeonCss heap used / total - %.2f / %.2f MiB\n",
           info.leonCssMemoryUsage.used / (1024.0f * 1024.0f),
           info.leonCssMemoryUsage.total / (1024.0f * 1024.0f));
    printf("LeonMss heap used / total - %.2f / %.2f MiB\n",
           info.leonMssMemoryUsage.used / (1024.0f * 1024.0f),
           info.leonMssMemoryUsage.total / (1024.0f * 1024.0f));
    const auto& t = info.chipTemperature;
    printf("Chip temperature - average: %.2f, css: %.2f, mss: %.2f, upa: %.2f, dss: %.2f\n", t.average, t.css, t.mss, t.upa, t.dss);
    printf("Cpu usage - Leon CSS: %.2f %%, Leon MSS: %.2f %%\n", info.leonCssCpuUsage.average * 100, info.leonMssCpuUsage.average * 100);
    printf("----------------------------------------\n");
}

int main() {
    // Create pipeline
    dai::Pipeline pipeline;

    // Define source and output
    auto sysLog = pipeline.create<dai::node::SystemLogger>();
    auto xout = pipeline.create<dai::node::XLinkOut>();

    xout->setStreamName("sysinfo");

    // Properties
    sysLog->setRate(1.0f);  // 1 hz updates

    // Linking
    sysLog->out.link(xout->input);

    // Connect to device and start pipeline
    dai::Device device(pipeline);

    // Output queue will be used to get the system info
    auto qSysInfo = device.getOutputQueue("sysinfo", 4, false);

    while(true) {
        auto sysInfo = qSysInfo->get<dai::SystemInformation>();
        printSystemInformation(*sysInfo);
    }
    return 0;
}
```

## Pipeline

### examples/system_information.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "out",
        "node1OutputGroup": "",
        "node2Id": 1,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "out"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 1,
                "name": "out",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "SystemLogger",
          "properties": {
            "rateHz": 1.0
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "XLinkOut",
          "properties": {
            "maxFpsLimit": -1.0,
            "metadataOnly": false,
            "streamName": "sysinfo"
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.