# UVC & Color Camera

This example demonstrates how to use the RGB camera on your OAK device as a UVC webcam. The
[UVC](https://docs.luxonis.com/software/depthai-components/nodes/uvc.md) node allows you to use your OAK device as a regular
webcam in applications like OpenCV's cv2.VideoCapture(), native camera apps, and more.

### Similar samples:

 * [UVC & Disparity](https://docs.luxonis.com/software/depthai/examples/uvc_disparity.md)
 * [UVC & Mono Camera](https://docs.luxonis.com/software/depthai/examples/uvc_mono.md)

## Setup

Please run the [install script](https://github.com/luxonis/depthai-python/blob/main/examples/install_requirements.py) to download
all required dependencies. Please note that this script must be ran from git context, so you have to download the
[depthai-python](https://github.com/luxonis/depthai-python) repository first and then run the script

```bash
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
```

For additional information, please follow the [installation guide](https://docs.luxonis.com/software/depthai/manual-install.md).

## Code used for testing

```python
import cv2

# Initialize the VideoCapture object to use the default camera (camera index 0 is webcam)
cap = cv2.VideoCapture(1)

# Check if the camera opened successfully
if not cap.isOpened():
    print("Error: Could not open camera.")
    exit()

# Loop to continuously get frames from the camera
while True:
    ret, frame = cap.read()

    if not ret:
        print("Error: Could not read frame.")
        break

    cv2.imshow('Video Feed', frame)

    if cv2.waitKey(1) & 0xFF == ord('q'):
        break

cap.release()
cv2.destroyAllWindows()
```

## Source code

#### Python

```python
#!/usr/bin/env python3

import time
import argparse

parser = argparse.ArgumentParser()
parser.add_argument('-fb', '--flash-bootloader', default=False, action="store_true")
parser.add_argument('-f',  '--flash-app',        default=False, action="store_true")
parser.add_argument('-l',  '--load-and-exit',    default=False, action="store_true")
args = parser.parse_args()

if args.load_and_exit:
    import os
    # Disabling device watchdog, so it doesn't need the host to ping periodically.
    # Note: this is done before importing `depthai`
    os.environ["DEPTHAI_WATCHDOG"] = "0"

import depthai as dai

def getPipeline():
    enable_4k = False  # Will downscale 4K -> 1080p

    pipeline = dai.Pipeline()

    # Define a source - color camera
    cam_rgb = pipeline.createColorCamera()
    cam_rgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
    cam_rgb.setInterleaved(False)
    #cam_rgb.initialControl.setManualFocus(130)

    if enable_4k:
        cam_rgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_4_K)
        cam_rgb.setIspScale(1, 2)
    else:
        cam_rgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)

    # Create an UVC (USB Video Class) output node
    uvc = pipeline.createUVC()
    cam_rgb.video.link(uvc.input)

    # Note: if the pipeline is sent later to device (using startPipeline()),
    # it is important to pass the device config separately when creating the device
    config = dai.Device.Config()
    # config.board.uvc = dai.BoardConfig.UVC()  # enable default 1920x1080 NV12
    config.board.uvc = dai.BoardConfig.UVC(1920, 1080)
    config.board.uvc.frameType = dai.ImgFrame.Type.NV12
    # config.board.uvc.cameraName = "My Custom Cam"
    pipeline.setBoardConfig(config.board)

    return pipeline

# Will flash the bootloader if no pipeline is provided as argument
def flash(pipeline=None):
    (f, bl) = dai.DeviceBootloader.getFirstAvailableDevice()
    bootloader = dai.DeviceBootloader(bl, True)

    # Create a progress callback lambda
    progress = lambda p : print(f'Flashing progress: {p*100:.1f}%')

    startTime = time.monotonic()
    if pipeline is None:
        print("Flashing bootloader...")
        bootloader.flashBootloader(progress)
    else:
        print("Flashing application pipeline...")
        bootloader.flash(progress, pipeline)

    elapsedTime = round(time.monotonic() - startTime, 2)
    print("Done in", elapsedTime, "seconds")

if args.flash_bootloader or args.flash_app:
    if args.flash_bootloader: flash()
    if args.flash_app: flash(getPipeline())
    print("Flashing successful. Please power-cycle the device")
    quit()

if args.load_and_exit:
    device = dai.Device(getPipeline())
    print("\nDevice started. Attempting to force-terminate this process...")
    print("Open an UVC viewer to check the camera stream.")
    print("To reconnect with depthai, a device power-cycle may be required in some cases")
    # We do not want the device to be closed, so terminate the process uncleanly.
    # (TODO add depthai API to be able to cleanly exit without closing device)
    import signal
    os.kill(os.getpid(), signal.SIGTERM)

# Standard UVC load with depthai
with dai.Device(getPipeline()) as device:
    print("\nDevice started, please keep this process running")
    print("and open an UVC viewer to check the camera stream.")
    print("\nTo close: Ctrl+C")

    # Doing nothing here, just keeping the host feeding the watchdog
    while True:
        try:
            time.sleep(0.1)
        except KeyboardInterrupt:
            break
```

## Pipeline

### examples/uvc_rgb.pipeline.json

```json
{
  "pipeline": {
    "connections": [
      {
        "node1Id": 0,
        "node1Output": "video",
        "node1OutputGroup": "",
        "node2Id": 1,
        "node2Input": "in",
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
      "xlinkChunkSize": -1
    },
    "nodes": [
      [
        0,
        {
          "id": 0,
          "ioInfo": [
            [
              [
                "",
                "inputConfig"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 1,
                "name": "inputConfig",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "raw"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 6,
                "name": "raw",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "still"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 7,
                "name": "still",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "inputControl"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 2,
                "name": "inputControl",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "video"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 3,
                "name": "video",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "isp"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 4,
                "name": "isp",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "preview"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 5,
                "name": "preview",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ],
            [
              [
                "",
                "frameEvent"
              ],
              {
                "blocking": false,
                "group": "",
                "id": 8,
                "name": "frameEvent",
                "queueSize": 8,
                "type": 0,
                "waitForMessage": false
              }
            ]
          ],
          "name": "ColorCamera",
          "properties": {
            "boardSocket": 0,
            "cameraName": "",
            "colorOrder": 0,
            "fp16": false,
            "fps": 30.0,
            "imageOrientation": -1,
            "initialControl": {
              "aeLockMode": false,
              "aeMaxExposureTimeUs": 0,
              "aeRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "afRegion": {
                "height": 0,
                "priority": 0,
                "width": 0,
                "x": 0,
                "y": 0
              },
              "antiBandingMode": 0,
              "autoFocusMode": 3,
              "awbLockMode": false,
              "awbMode": 0,
              "brightness": 0,
              "captureIntent": 0,
              "chromaDenoise": 0,
              "cmdMask": 0,
              "contrast": 0,
              "controlMode": 0,
              "effectMode": 0,
              "expCompensation": 0,
              "expManual": {
                "exposureTimeUs": 0,
                "frameDurationUs": 0,
                "sensitivityIso": 0
              },
              "frameSyncMode": 0,
              "lensPosAutoInfinity": 0,
              "lensPosAutoMacro": 0,
              "lensPosition": 0,
              "lensPositionRaw": 0.0,
              "lowPowerNumFramesBurst": 0,
              "lowPowerNumFramesDiscard": 0,
              "lumaDenoise": 0,
              "saturation": 0,
              "sceneMode": 0,
              "sharpness": 0,
              "strobeConfig": {
                "activeLevel": 0,
                "enable": 0,
                "gpioNumber": 0
              },
              "strobeTimings": {
                "durationUs": 0,
                "exposureBeginOffsetUs": 0,
                "exposureEndOffsetUs": 0
              },
              "wbColorTemp": 0
            },
            "interleaved": false,
            "isp3aFps": 0,
            "ispScale": {
              "horizDenominator": 0,
              "horizNumerator": 0,
              "vertDenominator": 0,
              "vertNumerator": 0
            },
            "numFramesPoolIsp": 3,
            "numFramesPoolPreview": 4,
            "numFramesPoolRaw": 3,
            "numFramesPoolStill": 4,
            "numFramesPoolVideo": 4,
            "previewHeight": 300,
            "previewKeepAspectRatio": true,
            "previewWidth": 300,
            "rawPacked": null,
            "resolution": 0,
            "sensorCropX": -1.0,
            "sensorCropY": -1.0,
            "stillHeight": -1,
            "stillWidth": -1,
            "videoHeight": -1,
            "videoWidth": -1
          }
        }
      ],
      [
        1,
        {
          "id": 1,
          "ioInfo": [
            [
              [
                "",
                "in"
              ],
              {
                "blocking": true,
                "group": "",
                "id": 9,
                "name": "in",
                "queueSize": 8,
                "type": 3,
                "waitForMessage": true
              }
            ]
          ],
          "name": "UVC",
          "properties": {
            "gpioInit": [],
            "gpioStreamOff": [],
            "gpioStreamOn": []
          }
        }
      ]
    ]
  }
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.