Platform

ON THIS PAGE

  • IP rating
  • PoE cameras
  • Internal testing
  • USB cameras
  • USB IP certification

IP rating

IP code tells you whether a device is dustproof and/or waterproof. Only our OAK PoE devices have an IP rating, current version of USB devices do not have an IP rating.

PoE cameras

Series 1 PoE devices (OAK-D PoE and OAK-1 PoE), OAK-D SR PoE, and OAK Thermal are shipped with an IP67 rated enclosure. It means that the device is protected from total dust ingress and that it's protected from water immersion between 15 centimeters and 1 meter in depth.OAK-D S2 PoE (and all its variants, so -W, -Pro, and -Pro-W) have IP65 rated enclosure.PoE enclosures have gaskets which makes them waterproof/dustproof:

Internal testing

Here's our testing setup for the enclosures used in our R&D process. The drum, filled with water, has a height of 1 meter. We conducted extended testing on these two enclosures.

USB cameras

In 2024 we started shipping an USB with screw-locking mechanism (shop link) along with several of our cameras; OAK-D-W, OAK-D Pro, and OAK-D Pro W.This cable is water-proof, and provides IP66 protection to the cameras. If you wish to have OAK-D-S2 with IP66 protection, you can order this cable separately, as by default it ships with a standard USB cable (non-waterproof).

USB IP certification

For testing and certification we are using a 3rd party certified laboratory. The certificate for the Series 2 USB cameras is available here.The photos and video below were captured during the water resistance certification process.