# RAE ROS

Note The RAE project is under active development so you can expect changes in the API and improvements in the performance in near
future. Please report problems on Github issues as it's important for the development efforts.

## Setting up procedure

#### SSH

 1. Connect via USB cable or wifi `rae-<ID>`, password `wifiwifi@` (See [RAE getting started
    documentation](https://docs.luxonis.com/hardware/rae/get-started.md)).
 2. To use SHH without typing password each time - `ssh-copy-id root@192.168.11.1`. Also a easier solution for USB devices, can
    append to `~/.ssh/config` the following, entering just with `ssh ku`:

```plaintext
Host ku 192.168.197.55
  HostName 192.168.197.55
  User root
  StrictHostKeyChecking no
  UserKnownHostsFile /dev/null
```

 1. Currently date resets after each startup to set current - ssh root@192.168.11.1 sudo date -s @`( date -u +"%s" )`
 2. If you want to run ROS packages while bypassing Luxonis Hub it would be advised to stop RH agent before starting docker
    containers, otherwise you can easily run into conflicts as they would be competing for same hardware resources - `robothub-ctl
    stop`. Keep in mind that since `wpa_supplicant` is a subprocess of the RH agent, the WiFi connection will get killed along
    with the agent. To resolve this we recommend you manually setup the WiFi connection as done in [this
    guide](https://docs.luxonis.com/hardware/rae/get-started.md).

#### Generating docker image

You can download prebuilt images form [dockerhub](https://hub.docker.com/r/luxonis/rae-ros-robot/tags), in which case you can skip
first 2 steps in guide below. We recommend using image tagged as humble as all other images are generally experimental images. You
can download docker image with:

`docker pull luxonis/rae-ros-robot:humble`

Downloading prebuilt images is recommended if you are not planning to considerably change source code.

 1. Clone repository `git clone git@github.com:luxonis/rae-ros.git`
 2. Build docker image `cd rae && docker buildx build --platform arm64 --build-arg USE_RVIZ=0 --build-arg SIM=0 --build-arg
    ROS_DISTRO=humble --build-arg CORE_NUM=10 -f Dockerfile --squash -t <docker-image-name>:<tag> --load .` You need to install
    necessary tools along buildx `sudo docker run --rm --privileged multiarch/qemu-user-static --reset -p yes`
 3. Upload docker image to robot. Connect robot to your PC via USB so you can transfer image quicker. Note that currently space on
    the robot is limited, so you need to have 7-8 GB of free space in `/data` directory - `docker save <docker-image-name>:<tag> |
    ssh -C root@192.168.197.55 docker load`
 4. SSH into robot and run docker image or just skip all first 3 steps and run the second: * `docker run -it
    --restart=unless-stopped -v /dev/:/dev/ -v /sys/:/sys/ --privileged --net=host <docker-image-name>:<tag>`
     * `docker run -it -v /dev/:/dev/ -v /sys/:/sys/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix -v
       /dev/bus/usb:/dev/bus/usb --device-cgroup-rule='c 189:* rmw' --network host <docker-image-name>:<tag>`
 5. Search for docker container name with `docker ps`
 6. Attach to the shell - `docker attach <container_name>`, or if you want to create separate session `docker exec -it
    <container_name> zsh`
 7. To launch robot hardware - `ros2 launch rae_bringup robot.launch.py`. This launches: * Motor drivers and differential
    controller
     * Camera driver, currently set up to provide Depth and streams from left & right camera. Note here that you have to calibrate
       cameras (see steps below). Currently a default calibration file is loaded. It's located in `rae_camera/config/cal.json`. To
       use one on the device or from other path, change `i_external_calibration_path` parameter in `rae_camera/config/camera.yaml`
     * Depth image -> LaserScan conversion node used for SLAM
 8. Launching whole stack - `ros2 launch rae_bringup bringup.launch.py`. It has following arguments used for enabling parts of the
    stack: * `enable_slam_toolbox` (true)
     * `enable_rosbridge` (false)
     * `enable_rtabmap` (false)
     * `enable_nav` (false) Example launch with an argument - `ros2 launch rae_bringup bringup.launch.py enable_nav:=false`

#### Developing on docker

You can rebuild RAE_hw related packages directly on the robot if you limit colcon (for example run: `MAKEFLAGS="-j1 -l1" colcon
build --symlink-install --packages-select rae_hw`). For related camera stuff you can build locally on PC due to hardware
limitation of RAE. For quickly rebuild broken images is recommended to use docker.

You can also test/develop/build on PC with connected RAE for rapid prototyping. This is recommended for rebuilding camera related
stuff and testing, also need to comment from `rae_camera.launch.py` the following:

```python
RegisterEventHandler(
            OnProcessStart(
                target_action=perception,
                on_start=[
                    TimerAction(
                        period=15.0,
                        actions=[reset_pwm, LogInfo(msg='Resetting PWM.'),],
                    )
                ]
            )
        ),
```

 1. Open rae-ros workspace in vscode
 2. Create `.devcontainer` directory in the workspace
 3. In it, create `devcontainer.json`
 4. You'll need to add Remote containers extension to VScode if you didn't already
 5. After that, a window should pop out that will ask if you want to reopen the directory in container, select yes If nothing pops
    up, CTRL+SHIFT+P , select option Rebuild and reopen

```json
// See https://aka.ms/vscode-remote/devcontainer.json for format details.
{
	"dockerFile": "../src/rae-ros/Dockerfile",
	"build": {
		"args": {
			"USE_RVIZ": "1",
			"SIM": "1",
			"CORE_NUM": "10",
			"--ssh": "default=$HOME/.ssh/id_rsa.pub ."
		}
	},
	"remoteUser": "root",
	"runArgs": [
		"--device=/dev/ttyUSB0",
		"--privileged",
		"--network=host",
		"--cap-add=SYS_PTRACE",
		"--security-opt=seccomp:unconfined",
		"--security-opt=apparmor:unconfined",
		"--volume=/dev:/dev",
		"--volume=/tmp/.X11-unix:/tmp/.X11-unix",
        "--volume=${env:HOME}/.ssh:/${HOME}/.ssh",
		// "--gpus=all"
	],
	"containerEnv": {
		"DISPLAY": "${localEnv:DISPLAY}",
		"QT_X11_NO_MITSHM": "1",
		// "LIBGL_ALWAYS_SOFTWARE": "1" // Needed for software rendering of opengl
	},
	// Set *default* container specific settings.json values on container create.
	"settings": {
		"terminal.integrated.profiles.linux": {
			"zsh": {
				"path": "zsh"
			},
			"bash": {
				"path": "bash"
			}
		},
		"terminal.integrated.defaultProfile.linux": "zsh"
	},
	"extensions": [
		"dotjoshjohnson.xml",
		"ms-azuretools.vscode-docker",
		"ms-iot.vscode-ros",
		"ms-python.python",
		"ms-vscode.cpptools",
		"redhat.vscode-yaml",
		"smilerobotics.urdf",
		"streetsidesoftware.code-spell-checker",
		"twxs.cmake",
		"yzhang.markdown-all-in-one",
		"augustocdias.tasks-shell-input",
		"eamodio.gitlens"
	]
}
```

Note: For displaying RViz in docker you need to run on PC: `xhost +local:docker`.

#### Calibration

Every shipped RAE has already been factory calibrated, so this step is rarely needed. Besides the section below, [Calibration
documentation](https://docs.luxonis.com/hardware/platform/depth/manual-calibration.md) is also a good source of information.

With PC connected to RAE via SSH (RH agent use depthai_gate):

```bash
robothub-ctl stop
```

On your PC:

```bash
git clone --branch rvc3_calibration https://github.com/luxonis/depthai.git
cd depthai/
python3 install_requirements.py
# To calibrate RAE's front cameras - for back cameras we would change the board name to "RAE-D-E"
python3 calibrate.py -s <size>  -brd RAE-A-B-C -cd 1 -c 3
```

Some tips:

 1. Try to fill stereo pairs matrices (color camera preview can be out of FOV, but not the Stereo pairs)
 2. Put charuco on a flat surface (bigger board it will be better)
 3. When you take a frame is a better practice to freeze board (motion are not ok)

## Configuration:

#### Feature Tracker

Each sensor node (and rectified streams from Stereo node) has the option to add FeatureTracker node, which publishes
`depthai_ros_msgs/msg/TrackedFeatures` messages. To enable features on, for example rgb node, set `rgb: i_enable_feature_tracker:
true`. To enable publishing on rectified streams, set for example `stereo: i_left_rect_enable_feature_tracker`

#### Setting Camera and IMU parameters

You can set params for camera and IMU in file: `rae_camera/config/camera.yaml`. For all available settings refer to
[depthai-ros](https://github.com/luxonis/depthai-ros)

#### Robot Localization

Config file for robot localization package can be found: `rae_hw/config/ekf.yaml` . For more information refer to [this
link](http://wiki.ros.org/robot_localization)

#### Sensors and sockets

Socket 1 - OV9782 Socket 0 - IMX214 Socket 2 - OV9782 Socket 3 - OV9782 Socket 4 - OV9782

## Peripherals:

 * LCD node - accepts BGR8 image (best if already resized to 160x80px) on /lcd Image topic
 * LED node - Subscribes to /led topic, message type is LEDControl (refer to rae_msgs/msg/LEDControl)
 * Mic node - Publishes audio_msgs/msg/Audio (from gst_bridge package) on /audio_in, configuration is S32_LE, 48kHz, 2 channel
   interleaved
 * Speakers node - Subsides to audio_out to same type as Mic node, configuration is S16_LE, 41kHz, 2 channel interleaved

#### Testing motors

In `rae_hw/test` you can find three scripts that will help you verify that the motors are running correctly. If you want to change
arguments, you need to provide all of them.

 1. To find out if encoder is working accurately, execute `ros2 run rae_hw test_encoders` and rotate the wheel by 360 degrees.
    After rotation, encoder readout should be ~2PI. If not, adjust encoder tick per rev parameter. Script arguments - `[encRatioL
    encRatioR]`. Full arg version `ros2 run rae_hw test_encoders 756 756`
 2. Finding out max speed - `ros2 run rae_hw test_max_speed`. Script arguments `[duration encRatioL encRatioR]`. Full arg version
    `ros2 run rae_hw test_max_speed 1.0 756 756`
 3. Motor verification - `ros2 run rae_hw test_motors`. Script arguments `[duration speedL speedR encRatioL encRatioR maxVelL
    maxVelR]`. Full arg version `ros2 run rae_hw test_motors 5.0 16.0 16.0 756 756 32 32`

Motor configuration parameters are provided in `rae_description/urdf/rae_ros2_control.urdf.xacro` file. Pin numbers shouldn't
change between devices, but if that's the case you can edit that file to set new ones.

 * PWM pins (speed control):

```xml
<param name="pwmL">2</param>
<param name="pwmR">1</param>
```

 * Phase pins (direction control)

```xml
<param name="phL">41</param>
<param name="phR">45</param>
```

 * Encoder pins - each motor has A and B pins for encoders.

```xml
<param name="enLA">42</param>
<param name="enLB">43</param>
<param name="enRA">46</param>
<param name="enRB">47</param>
```

 * How many encoder tics are there per revolution - this might vary from setup to setup. To verify that, run the controller and
   rotate a wheel manually. You can see current positions/velocities by listening on `/joint_states` topic - `ros2 topic echo
   /joint_states`.

```xml
<param name="encTicsPerRevL">756</param>
<param name="encTicsPerRevR">756</param>
```

 * Max motor speed in rads/s

```xml
<param name="maxVelL">32</param>
<param name="maxVelR">32</param>
```

 * Both wheels have parameters for PID control set in that file, those values could need some tuning:

```xml
<param name="closed_loopR">1</param>
<param name="PID_P_R">0.2</param>
<param name="PID_I_R">0.1</param>
<param name="PID_D_R">0.0005</param>
```

Parameters for differential driver controller are present in `rae_hw/config/controller.yaml`. `wheel_separation` and
`wheel_radius` parameters might also need tuning depending on the setup.

Implementation of motor control is found in rae_hw package. You can set the motor to be ready to receive twist commands on
/cmd_vel topic by running:

`ros2 launch rae_hw control.launch.py`

You can then control the robot via keyboard teleop from your pc via (assuming you are connected to same network robot is in):

 1. `sudo apt-get install ros-humble-teleop-twist-keyboard`
 2. `ros2 run  teleop_twist_keyboard teleop_twist_keyboard`

If keyboard is too limiting for your tests you could also use ros-humble-teleop-twist-joy and connect a joystick.

#### LED node

Under rae_msgs package you can find custom messages that let you control LED lights around the robot. Under those messages there
are 3 control types:

 1. Control all (set control_type to 0) gives all LEDs the same color
 2. Control single (control_type to 1) lets you control just a single LED light by setting single_led_n variable
 3. Custom control (control_type to 2) where you send a list that defines every value of LED lights at once.

Useful example of how to work with LEDs can be found in rae_bringup/scripts/led_test.py where this for loop is populating LED
values (with custom control) for each individual LED:

```python
 for i in range(40):
            led_msg.single_led_n = 0
            led_msg.control_type = 2
            if i < 8:
                color = "white"
                led_msg.data[i]=(colors[color])
            if i >9 and i < 14 and angular_speed > 0.0 and blinking==True:
                color = "yellow"
                led_msg.data[i]=(colors[color])
            if i > 20 and i < 29 and linear_speed < 0.0:
                color = "red"
                led_msg.data[i]=(colors[color])
            if i> 34 and i < 39 and angular_speed < 0.0 and blinking==True:
                color = "yellow"
                led_msg.data[i]=(colors[color])
```

We can then send that message to a topic that LED node listens to - by default that is /leds . Easiest way to run LED node (and
all other peripheral node) is to run one of the following launch files:

```bash
ros2 launch rae_hw peripherals.launch.py
ros2 launch rae_hw control.launch.py
ros2 launch rae_bringup robot.launch.py
```

Where first file is running only peripherals, 2nd is running peripherals and motors, while 3rd is running both of those along with
cameras. It could be useful to create your own launch file that mimics peripherals launch file, so you can run your own examples
along with nodes.

#### LCD node

LCD node is listening to messages on /lcd topic and showing it on the screen in the. Useful demo for this node is in
rae_bringup/scripts/battery_status.py where we subscribe to battery status topic and based on that create image of battery status
on LCD screen. This node expects ROS (sensor_msg/Image) image, so you will generally have to transform opencv image to ROS image:

`img_msg = self.bridge.cv2_to_imgmsg(img_cv, encoding="bgr8")`

#### Microphone and speakers

Microphone node expects audio messages and example of how to use that data (along with some other peripherals) can be found in
rae_bringup/scripts/audio_spectrum.py . For fair amount of use cases, you will need to decode incoming data as shown in example
below.

```python
 if msg.encoding == "S32LE":
            audio_data = np.frombuffer(msg.data, dtype=np.int32)
        elif msg.encoding == "S16LE":
            audio_data = np.frombuffer(msg.data, dtype=np.int16)
        if msg.layout == Audio.LAYOUT_INTERLEAVED:
            # Deinterleave channels
            audio_data = audio_data.reshape((msg.frames, msg.channels))
```

GST-ROS bridge You can use gst-bridge for testing, for example to play audio on a ros topic:

 * `gst-launch-1.0 --gst-plugin-path=install/gst_bridge/lib/gst_bridge/ filesrc location=sample.mp3 ! decodebin ! audioconvert !
   rosaudiosink ros-topic="/audio_out"`
 * `gst-launch-1.0 --gst-plugin-path=install/gst_bridge/lib/gst_bridge/ rosaudiosrc ros-topic="audio_out" ! audioconvert ! wavenc
   ! filesink location=mic1.wav`
 * `gst-launch-1.0 --gst-plugin-path=install/gst_bridge/lib/gst_bridge/ rosimagesrc ros-topic="/rae/right_front/image_raw" !
   videoconvert ! videoscale ! video/x-raw,width=160,height=80 ! fbdevsink`
 * `gst-launch-1.0 alsasrc device="hw:0,1" ! audio/x-raw,rate=48000,format=S32LE ! audioconvert ! spectrascope ! videoconvert !
   video/x-raw,width=160,height=80 ! fbdevsink`

Speakers operate similarly, in that they output audio messages. In bringup package in scripts folder sound_test.py offers a decent
example of how you can create audio messages. We will shortly create more demos for speakers and microphone.

#### USB ports

To use top USB port to for example connect it to some external device, you need to disable communication side USB.

To do that, execute

```bash
gpioset gpiochip0 44=1
echo host > /sys/kernel/debug/usb/34000000.dwc3/mode
```

This will be reverted after reboot. To revert it manually, execute

```bash
gpioset gpiochip0 44=0
echo device > /sys/kernel/debug/usb/34000000.dwc3/mode
```