Demuxing Synchronized Script Outputs
Similar samples
Demo
Command Line
1~/depthai-python/examples/Sync $ python3 demux_message_group.py
2Start
3Buffer 1 timestamp: 0:00:03.581073
4Buffer 2 timestamp: 0:00:03.591084
5----------
6Buffer 1 timestamp: 0:00:04.583100
7Buffer 2 timestamp: 0:00:04.497079
8----------
9Buffer 1 timestamp: 0:00:06.587174
10Buffer 2 timestamp: 0:00:06.611154
11----------
12Buffer 1 timestamp: 0:00:07.589147
13Buffer 2 timestamp: 0:00:07.517125
14----------
15Buffer 1 timestamp: 0:00:09.593076
16Buffer 2 timestamp: 0:00:09.631089
17----------
18Buffer 1 timestamp: 0:00:10.595106
19Buffer 2 timestamp: 0:00:10.537082Source code
Python
C++
Python
PythonGitHub
1import depthai as dai
2import time
3from datetime import timedelta
4
5pipeline = dai.Pipeline()
6
7script1 = pipeline.create(dai.node.Script)
8script1.setScript("""
9from time import sleep
10
11while True:
12 sleep(1)
13 b = Buffer(512)
14 b.setData(bytes(4 * [i for i in range(0, 128)]))
15 b.setTimestamp(Clock.now())
16 node.io['out'].send(b)
17""")
18
19script2 = pipeline.create(dai.node.Script)
20script2.setScript("""
21from time import sleep
22
23while True:
24 sleep(0.3)
25 b = Buffer(512)
26 b.setData(bytes(4 * [i for i in range(128, 256)]))
27 b.setTimestamp(Clock.now())
28 node.io['out'].send(b)
29""")
30
31sync = pipeline.create(dai.node.Sync)
32sync.setSyncThreshold(timedelta(milliseconds=100))
33
34demux = pipeline.create(dai.node.MessageDemux)
35
36xout1 = pipeline.create(dai.node.XLinkOut)
37xout1.setStreamName("xout1")
38xout2 = pipeline.create(dai.node.XLinkOut)
39xout2.setStreamName("xout2")
40
41script1.outputs["out"].link(sync.inputs["s1"])
42script2.outputs["out"].link(sync.inputs["s2"])
43sync.out.link(demux.input)
44demux.outputs["s1"].link(xout1.input)
45demux.outputs["s2"].link(xout2.input)
46
47with dai.Device(pipeline) as device:
48 print("Start")
49 q1 = device.getOutputQueue("xout1", maxSize=10, blocking=True)
50 q2 = device.getOutputQueue("xout2", maxSize=10, blocking=True)
51 while True:
52 bufS1 = q1.get()
53 bufS2 = q2.get()
54 print(f"Buffer 1 timestamp: {bufS1.getTimestamp()}")
55 print(f"Buffer 2 timestamp: {bufS2.getTimestamp()}")
56 print("----------")
57 time.sleep(0.2)How it Works
- Initialize a DepthAI pipeline.
- Create two Script nodes, with each script generating and sending data buffers at different intervals.
- Set up a Sync node with a synchronization threshold.
- Integrate a MessageDemux node to separate the synchronized data streams.
- Link the outputs of the Script nodes to the Sync node, and then from the Sync node to the MessageDemux node.
- Start the pipeline and continuously receive demultiplexed data from the MessageDemux node.
- Print the timestamps of the demultiplexed data for comparison.
Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.