Latency measurement
.getTimestamp() function in combination with dai.Clock.now() to measure the latency since image was captured (more accurately since it was processed by ISP and timestamp was attached to it) until the frame was received on the host computer.If you would like to learn more about low-latency, see the documentation page here.Demo
isp 1080P output (YUV420 encoded frame) from ColorCamera running at 60FPS. We get about 33ms, which is what was measured in optimizing latency docs page as well.Command Line
1UsbSpeed.SUPER
2Latency: 33.49 ms, Average latency: 33.49 ms, Std: 0.00
3Latency: 34.92 ms, Average latency: 34.21 ms, Std: 0.71
4Latency: 33.23 ms, Average latency: 33.88 ms, Std: 0.74
5Latency: 33.70 ms, Average latency: 33.84 ms, Std: 0.65
6Latency: 33.94 ms, Average latency: 33.86 ms, Std: 0.58
7Latency: 34.18 ms, Average latency: 33.91 ms, Std: 0.54Source code
Python
C++
Python
PythonGitHub
1import depthai as dai
2import numpy as np
3# Create pipeline
4pipeline = dai.Pipeline()
5# This might improve reducing the latency on some systems
6pipeline.setXLinkChunkSize(0)
7
8# Define source and output
9camRgb = pipeline.create(dai.node.ColorCamera)
10camRgb.setFps(60)
11camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
12
13xout = pipeline.create(dai.node.XLinkOut)
14xout.setStreamName("out")
15camRgb.isp.link(xout.input)
16
17# Connect to device and start pipeline
18with dai.Device(pipeline) as device:
19 print(device.getUsbSpeed())
20 q = device.getOutputQueue(name="out")
21 diffs = np.array([])
22 while True:
23 imgFrame = q.get()
24 # Latency in miliseconds
25 latencyMs = (dai.Clock.now() - imgFrame.getTimestamp()).total_seconds() * 1000
26 diffs = np.append(diffs, latencyMs)
27 print('Latency: {:.2f} ms, Average latency: {:.2f} ms, Std: {:.2f}'.format(latencyMs, np.average(diffs), np.std(diffs)))
28
29 # Not relevant for this example
30 # cv2.imshow('frame', imgFrame.getCvFrame())Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.