Mono Camera Control
wwill move the crop upawill move the crop leftswill move the crop downdwill move the crop rightewill trigger autoexposureiandowill decrease/increase the exposure timekandlwill decrease/increase the sensitivity iso
Similar samples:
Demo
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3"""
4This example shows usage of mono camera in crop mode with the possibility to move the crop.
5Uses 'WASD' controls to move the crop window, 'T' to trigger autofocus, 'IOKL,.' for manual exposure/focus:
6 Control: key[dec/inc] min..max
7 exposure time: I O 1..33000 [us]
8 sensitivity iso: K L 100..1600
9To go back to auto controls:
10 'E' - autoexposure
11"""
12
13import cv2
14import depthai as dai
15
16# Step size ('W','A','S','D' controls)
17stepSize = 0.02
18# Manual exposure/focus set step
19expStep = 500 # us
20isoStep = 50
21
22def clamp(num, v0, v1):
23 return max(v0, min(num, v1))
24
25sendCamConfig = False
26
27# Create pipeline
28pipeline = dai.Pipeline()
29
30# Define sources and outputs
31monoRight = pipeline.create(dai.node.MonoCamera)
32monoLeft = pipeline.create(dai.node.MonoCamera)
33manipRight = pipeline.create(dai.node.ImageManip)
34manipLeft = pipeline.create(dai.node.ImageManip)
35
36controlIn = pipeline.create(dai.node.XLinkIn)
37configIn = pipeline.create(dai.node.XLinkIn)
38manipOutRight = pipeline.create(dai.node.XLinkOut)
39manipOutLeft = pipeline.create(dai.node.XLinkOut)
40
41controlIn.setStreamName('control')
42configIn.setStreamName('config')
43manipOutRight.setStreamName("right")
44manipOutLeft.setStreamName("left")
45
46# Crop range
47topLeft = dai.Point2f(0.2, 0.2)
48bottomRight = dai.Point2f(0.8, 0.8)
49
50# Properties
51monoRight.setCamera("right")
52monoLeft.setCamera("left")
53monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
54monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_720_P)
55manipRight.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
56manipLeft.initialConfig.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
57manipRight.setMaxOutputFrameSize(monoRight.getResolutionHeight()*monoRight.getResolutionWidth()*3)
58
59# Linking
60monoRight.out.link(manipRight.inputImage)
61monoLeft.out.link(manipLeft.inputImage)
62controlIn.out.link(monoRight.inputControl)
63controlIn.out.link(monoLeft.inputControl)
64configIn.out.link(manipRight.inputConfig)
65configIn.out.link(manipLeft.inputConfig)
66manipRight.out.link(manipOutRight.input)
67manipLeft.out.link(manipOutLeft.input)
68
69# Connect to device and start pipeline
70with dai.Device(pipeline) as device:
71
72 # Output queues will be used to get the grayscale frames
73 qRight = device.getOutputQueue(manipOutRight.getStreamName(), maxSize=4, blocking=False)
74 qLeft = device.getOutputQueue(manipOutLeft.getStreamName(), maxSize=4, blocking=False)
75 configQueue = device.getInputQueue(configIn.getStreamName())
76 controlQueue = device.getInputQueue(controlIn.getStreamName())
77
78 # Defaults and limits for manual focus/exposure controls
79 expTime = 20000
80 expMin = 1
81 expMax = 33000
82
83 sensIso = 800
84 sensMin = 100
85 sensMax = 1600
86
87 while True:
88 inRight = qRight.get()
89 inLeft = qLeft.get()
90 cv2.imshow("right", inRight.getCvFrame())
91 cv2.imshow("left", inLeft.getCvFrame())
92
93 # Update screen (1ms pooling rate)
94 key = cv2.waitKey(1)
95 if key == ord('q'):
96 break
97 elif key == ord('e'):
98 print("Autoexposure enable")
99 ctrl = dai.CameraControl()
100 ctrl.setAutoExposureEnable()
101 controlQueue.send(ctrl)
102 elif key in [ord('i'), ord('o'), ord('k'), ord('l')]:
103 if key == ord('i'): expTime -= expStep
104 if key == ord('o'): expTime += expStep
105 if key == ord('k'): sensIso -= isoStep
106 if key == ord('l'): sensIso += isoStep
107 expTime = clamp(expTime, expMin, expMax)
108 sensIso = clamp(sensIso, sensMin, sensMax)
109 print("Setting manual exposure, time:", expTime, "iso:", sensIso)
110 ctrl = dai.CameraControl()
111 ctrl.setManualExposure(expTime, sensIso)
112 controlQueue.send(ctrl)
113 elif key == ord('w'):
114 if topLeft.y - stepSize >= 0:
115 topLeft.y -= stepSize
116 bottomRight.y -= stepSize
117 sendCamConfig = True
118 elif key == ord('a'):
119 if topLeft.x - stepSize >= 0:
120 topLeft.x -= stepSize
121 bottomRight.x -= stepSize
122 sendCamConfig = True
123 elif key == ord('s'):
124 if bottomRight.y + stepSize <= 1:
125 topLeft.y += stepSize
126 bottomRight.y += stepSize
127 sendCamConfig = True
128 elif key == ord('d'):
129 if bottomRight.x + stepSize <= 1:
130 topLeft.x += stepSize
131 bottomRight.x += stepSize
132 sendCamConfig = True
133
134 # Send new config to camera
135 if sendCamConfig:
136 cfg = dai.ImageManipConfig()
137 cfg.setCropRect(topLeft.x, topLeft.y, bottomRight.x, bottomRight.y)
138 configQueue.send(cfg)
139 sendCamConfig = FalsePipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.