ON THIS PAGE

  • PointCloud Control
  • Demo
  • Setup
  • Source code
  • Pipeline

PointCloud Control

This example demonstrates how to use PointCloudConfig message to dynamically update the transformation matrix of a point cloud and visualize the transformed point cloud using Open3D.The transformation matrix is updated to make it look like the point cloud is rotating about the Z-axis. This is achieved by first moving the point cloud along the Y axis:
Python
1# Move the point cloud along Y axis
2translate_y_matrix = np.array([
3    [1, 0, 0, 0],
4    [0, 1, 0, 500],
5    [0, 0, 1, 0],
6    [0, 0, 0, 1]
7])
Then, the point cloud is rotated about the Z axis:
Python
1# Rotate the point cloud about Z axis
2rotate_z_matrix = np.array([
3    [np.cos(angle), -np.sin(angle), 0, 0],
4    [np.sin(angle), np.cos(angle), 0, 0],
5    [0, 0, 1, 0],
6    [0, 0, 0, 1]
7])

Demo

Setup

Ensure DepthAI and Open3D are installed in your Python environment:
Command Line
1python3 -m pip install depthai open3d

Source code

The example initializes the DepthAI pipeline with color and mono cameras and a stereo depth node to generate depth information. It then creates a point cloud node, dynamically updates its transformation matrix based on a rotation value, and visualizes this transformed point cloud using Open3D. Each point's color corresponds to the color image captured by the RGB camera.
Python

Python

Python
GitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4import numpy as np
5import cv2
6import sys
7
8try:
9    import open3d as o3d
10except ImportError:
11    sys.exit(f"Critical dependency missing: Open3D. Please install it using the command: '{sys.executable} -m pip install open3d' and then rerun the script.")
12
13
14# Continue with the DepthAI and Open3D setup as before
15pipeline = dai.Pipeline()
16camRgb = pipeline.create(dai.node.ColorCamera)
17monoLeft = pipeline.create(dai.node.MonoCamera)
18monoRight = pipeline.create(dai.node.MonoCamera)
19depth = pipeline.create(dai.node.StereoDepth)
20pointcloud: dai.node.PointCloud = pipeline.create(dai.node.PointCloud)
21sync = pipeline.create(dai.node.Sync)
22xOut = pipeline.create(dai.node.XLinkOut)
23xOut.input.setBlocking(False)
24
25
26camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
27camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
28camRgb.setIspScale(1,3)
29
30monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
31monoLeft.setCamera("left")
32
33monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
34monoRight.setCamera("right")
35
36
37depth.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
38depth.initialConfig.setMedianFilter(dai.MedianFilter.KERNEL_7x7)
39depth.setLeftRightCheck(True)
40depth.setExtendedDisparity(False)
41depth.setSubpixel(True)
42depth.setDepthAlign(dai.CameraBoardSocket.CAM_A)
43config = depth.initialConfig.get()
44config.postProcessing.thresholdFilter.minRange = 200
45config.postProcessing.thresholdFilter.maxRange = 1000
46depth.initialConfig.set(config)
47
48monoLeft.out.link(depth.left)
49monoRight.out.link(depth.right)
50depth.depth.link(pointcloud.inputDepth)
51camRgb.isp.link(sync.inputs["rgb"])
52pointcloud.outputPointCloud.link(sync.inputs["pcl"])
53pointcloud.initialConfig.setSparse(False)
54sync.out.link(xOut.input)
55xOut.setStreamName("out")
56
57inConfig = pipeline.create(dai.node.XLinkIn)
58inConfig.setStreamName("config")
59inConfig.out.link(pointcloud.inputConfig)
60
61with dai.Device(pipeline) as device:
62
63    isRunning = True
64    def key_callback(vis, action, mods):
65        global isRunning
66        if action == 0:
67            isRunning = False
68
69    q = device.getOutputQueue(name="out", maxSize=4, blocking=False)
70    pclConfIn = device.getInputQueue(name="config", maxSize=4, blocking=False)
71
72    vis = o3d.visualization.Visualizer()
73    vis.create_window()
74    pcd = o3d.geometry.PointCloud()
75    coordinateFrame = o3d.geometry.TriangleMesh.create_coordinate_frame(size=1000, origin=[0,0,0])
76    vis.add_geometry(coordinateFrame)
77    vis.add_geometry(pcd)
78
79    first = True
80    rot = 0
81    while device.isPipelineRunning():
82        
83        inMessage = q.get()
84        inColor = inMessage["rgb"]
85        inPointCloud = inMessage["pcl"]
86        cvColorFrame = inColor.getCvFrame()
87        
88        cvRGBFrame = cv2.cvtColor(cvColorFrame, cv2.COLOR_BGR2RGB)
89
90        if inPointCloud:
91            points = inPointCloud.getPoints().astype(np.float64)
92            pcd.points = o3d.utility.Vector3dVector(points)
93            colors = (cvRGBFrame.reshape(-1, 3) / 255.0).astype(np.float64)
94            pcd.colors = o3d.utility.Vector3dVector(colors)
95            
96            vis.update_geometry(pcd)
97        vis.poll_events()
98        vis.update_renderer()
99
100        # Create a transformation matrix that rotates around all 3 axes at the same time
101        rotate_z_matrix = np.array([[np.cos(rot), -np.sin(rot), 0, 0],
102                                          [np.sin(rot), np.cos(rot), 0, 0],
103                                          [0, 0, 1, 0],
104                                          [0, 0, 0, 1]])
105        
106        translate_y_matrix = np.array([[1, 0, 0, 0],
107                                  [0, 1, 0, 500],
108                                  [0, 0, 1, 0],
109                                  [0, 0, 0, 1]])
110    
111        
112        # Combine the 3 transformation matrices into one
113        transformation_matrix = rotate_z_matrix @ translate_y_matrix
114        
115        rot += 0.05
116
117        pclConfig = dai.PointCloudConfig()
118        pclConfig.setTransformationMatrix(transformation_matrix)
119        pclConfig.setSparse(False)
120        pclConfIn.send(pclConfig)
121
122            
123    vis.destroy_window()
124    cv2.destroyAllWindows()

Pipeline

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.