ON THIS PAGE

  • PointCloud Visualization
  • Key Concepts
  • Demo
  • Setup
  • Source code

PointCloud Visualization

This example demonstrates how to visualize an on-device created point cloud using DepthAI and Open3D. It captures color and depth data from an OAK device, combines them to create a colored point cloud, and displays it in real-time. The FPS counter is included to monitor performance.

Key Concepts

  • Capturing synchronized color and depth frames using the DepthAI API.
  • Creating a point cloud with color data for visualization.
  • Real-time visualization of the point cloud using Open3D.
  • Implementing an FPS counter to monitor the application's performance.

Demo

Setup

If you are using Python, ensure you have DepthAI and Open3D installed in your Python environment:
Command Line
1python3 -m pip install depthai open3d
If Open3D is not already installed, the script will prompt you to install it.

Source code

The example initializes the DepthAI pipeline with color and mono cameras and a stereo depth node to generate depth information. It then creates a point cloud node and configures it for sparse point cloud generation. The script visualizes this point cloud using Open3D, with each point's color corresponding to the color image captured by the RGB camera.
Python
C++

Python

Python
GitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4from time import sleep
5import numpy as np
6import cv2
7import time
8import sys
9try:
10    import open3d as o3d
11except ImportError:
12    sys.exit("Critical dependency missing: Open3D. Please install it using the command: '{} -m pip install open3d' and then rerun the script.".format(sys.executable))
13
14FPS = 30
15class FPSCounter:
16    def __init__(self):
17        self.frameCount = 0
18        self.fps = 0
19        self.startTime = time.time()
20
21    def tick(self):
22        self.frameCount += 1
23        if self.frameCount % 10 == 0:
24            elapsedTime = time.time() - self.startTime
25            self.fps = self.frameCount / elapsedTime
26            self.frameCount = 0
27            self.startTime = time.time()
28        return self.fps
29
30pipeline = dai.Pipeline()
31camRgb = pipeline.create(dai.node.ColorCamera)
32monoLeft = pipeline.create(dai.node.MonoCamera)
33monoRight = pipeline.create(dai.node.MonoCamera)
34depth = pipeline.create(dai.node.StereoDepth)
35pointcloud = pipeline.create(dai.node.PointCloud)
36sync = pipeline.create(dai.node.Sync)
37xOut = pipeline.create(dai.node.XLinkOut)
38xOut.input.setBlocking(False)
39
40
41camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
42camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
43camRgb.setIspScale(1,3)
44camRgb.setFps(FPS)
45
46monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
47monoLeft.setCamera("left")
48monoLeft.setFps(FPS)
49monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
50monoRight.setCamera("right")
51monoRight.setFps(FPS)
52
53depth.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
54depth.initialConfig.setMedianFilter(dai.MedianFilter.KERNEL_7x7)
55depth.setLeftRightCheck(True)
56depth.setExtendedDisparity(False)
57depth.setSubpixel(True)
58depth.setDepthAlign(dai.CameraBoardSocket.CAM_A)
59
60monoLeft.out.link(depth.left)
61monoRight.out.link(depth.right)
62depth.depth.link(pointcloud.inputDepth)
63camRgb.isp.link(sync.inputs["rgb"])
64pointcloud.outputPointCloud.link(sync.inputs["pcl"])
65sync.out.link(xOut.input)
66xOut.setStreamName("out")
67
68
69
70
71with dai.Device(pipeline) as device:
72    isRunning = True
73    def key_callback(vis, action, mods):
74        global isRunning
75        if action == 0:
76            isRunning = False
77
78    q = device.getOutputQueue(name="out", maxSize=4, blocking=False)
79    vis = o3d.visualization.VisualizerWithKeyCallback()
80    vis.create_window()
81    vis.register_key_action_callback(81, key_callback)
82    pcd = o3d.geometry.PointCloud()
83    coordinateFrame = o3d.geometry.TriangleMesh.create_coordinate_frame(size=1000, origin=[0,0,0])
84    vis.add_geometry(coordinateFrame)
85
86    first = True
87    fpsCounter = FPSCounter()
88    while isRunning:
89        inMessage = q.get()
90        inColor = inMessage["rgb"]
91        inPointCloud = inMessage["pcl"]
92        cvColorFrame = inColor.getCvFrame()
93        # Convert the frame to RGB
94        cvRGBFrame = cv2.cvtColor(cvColorFrame, cv2.COLOR_BGR2RGB)
95        fps = fpsCounter.tick()
96        # Display the FPS on the frame
97        cv2.putText(cvColorFrame, f"FPS: {fps:.2f}", (10, 30), cv2.FONT_HERSHEY_SIMPLEX, 1, (0, 0, 255), 2)
98        cv2.imshow("color", cvColorFrame)
99        key = cv2.waitKey(1)
100        if key == ord('q'):
101            break
102        if inPointCloud:
103            t_before = time.time()
104            points = inPointCloud.getPoints().astype(np.float64)
105            pcd.points = o3d.utility.Vector3dVector(points)
106            colors = (cvRGBFrame.reshape(-1, 3) / 255.0).astype(np.float64)
107            pcd.colors = o3d.utility.Vector3dVector(colors)
108            if first:
109                vis.add_geometry(pcd)
110                first = False
111            else:
112                vis.update_geometry(pcd)
113        vis.poll_events()
114        vis.update_renderer()
115    vis.destroy_window()

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.