RGB Depth Alignment
You can also perform depth alignment with ImageAlign node (example), but we recommend using StereoDepth's alignment for better performance.
stereo.setOutputSize(width, height).To align depth with higher resolution color stream (eg. 12MP), you need to limit the resolution of the depth map. You can do that with stereo.setOutputSize(w,h). Code example here.Demo
This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import numpy as np
5import depthai as dai
6import argparse
7
8# Weights to use when blending depth/rgb image (should equal 1.0)
9rgbWeight = 0.4
10depthWeight = 0.6
11
12parser = argparse.ArgumentParser()
13parser.add_argument('-alpha', type=float, default=None, help="Alpha scaling parameter to increase float. [0,1] valid interval.")
14args = parser.parse_args()
15alpha = args.alpha
16
17def updateBlendWeights(percent_rgb):
18 """
19 Update the rgb and depth weights used to blend depth/rgb image
20
21 @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
22 """
23 global depthWeight
24 global rgbWeight
25 rgbWeight = float(percent_rgb)/100.0
26 depthWeight = 1.0 - rgbWeight
27
28
29fps = 30
30# The disparity is computed at this resolution, then upscaled to RGB resolution
31monoResolution = dai.MonoCameraProperties.SensorResolution.THE_720_P
32
33# Create pipeline
34pipeline = dai.Pipeline()
35device = dai.Device()
36queueNames = []
37
38# Define sources and outputs
39camRgb = pipeline.create(dai.node.Camera)
40left = pipeline.create(dai.node.MonoCamera)
41right = pipeline.create(dai.node.MonoCamera)
42stereo = pipeline.create(dai.node.StereoDepth)
43
44rgbOut = pipeline.create(dai.node.XLinkOut)
45disparityOut = pipeline.create(dai.node.XLinkOut)
46
47rgbOut.setStreamName("rgb")
48queueNames.append("rgb")
49disparityOut.setStreamName("disp")
50queueNames.append("disp")
51
52#Properties
53rgbCamSocket = dai.CameraBoardSocket.CAM_A
54
55camRgb.setBoardSocket(rgbCamSocket)
56camRgb.setSize(1280, 720)
57camRgb.setFps(fps)
58
59# For now, RGB needs fixed focus to properly align with depth.
60# This value was used during calibration
61try:
62 calibData = device.readCalibration2()
63 lensPosition = calibData.getLensPosition(rgbCamSocket)
64 if lensPosition:
65 camRgb.initialControl.setManualFocus(lensPosition)
66except:
67 raise
68left.setResolution(monoResolution)
69left.setCamera("left")
70left.setFps(fps)
71right.setResolution(monoResolution)
72right.setCamera("right")
73right.setFps(fps)
74
75stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY)
76# LR-check is required for depth alignment
77stereo.setLeftRightCheck(True)
78stereo.setDepthAlign(rgbCamSocket)
79
80# Linking
81camRgb.video.link(rgbOut.input)
82left.out.link(stereo.left)
83right.out.link(stereo.right)
84stereo.disparity.link(disparityOut.input)
85
86camRgb.setMeshSource(dai.CameraProperties.WarpMeshSource.CALIBRATION)
87if alpha is not None:
88 camRgb.setCalibrationAlpha(alpha)
89 stereo.setAlphaScaling(alpha)
90
91# Connect to device and start pipeline
92with device:
93 device.startPipeline(pipeline)
94
95 frameRgb = None
96 frameDisp = None
97
98 # Configure windows; trackbar adjusts blending ratio of rgb/depth
99 rgbWindowName = "rgb"
100 depthWindowName = "depth"
101 blendedWindowName = "rgb-depth"
102 cv2.namedWindow(rgbWindowName)
103 cv2.namedWindow(depthWindowName)
104 cv2.namedWindow(blendedWindowName)
105 cv2.createTrackbar('RGB Weight %', blendedWindowName, int(rgbWeight*100), 100, updateBlendWeights)
106
107 while True:
108 latestPacket = {}
109 latestPacket["rgb"] = None
110 latestPacket["disp"] = None
111
112 queueEvents = device.getQueueEvents(("rgb", "disp"))
113 for queueName in queueEvents:
114 packets = device.getOutputQueue(queueName).tryGetAll()
115 if len(packets) > 0:
116 latestPacket[queueName] = packets[-1]
117
118 if latestPacket["rgb"] is not None:
119 frameRgb = latestPacket["rgb"].getCvFrame()
120 cv2.imshow(rgbWindowName, frameRgb)
121
122 if latestPacket["disp"] is not None:
123 frameDisp = latestPacket["disp"].getFrame()
124 maxDisparity = stereo.initialConfig.getMaxDisparity()
125 # Optional, extend range 0..95 -> 0..255, for a better visualisation
126 if 1: frameDisp = (frameDisp * 255. / maxDisparity).astype(np.uint8)
127 # Optional, apply false colorization
128 if 1: frameDisp = cv2.applyColorMap(frameDisp, cv2.COLORMAP_HOT)
129 frameDisp = np.ascontiguousarray(frameDisp)
130 cv2.imshow(depthWindowName, frameDisp)
131
132 # Blend when both received
133 if frameRgb is not None and frameDisp is not None:
134 # Need to have both frames in BGR format before blending
135 if len(frameDisp.shape) < 3:
136 frameDisp = cv2.cvtColor(frameDisp, cv2.COLOR_GRAY2BGR)
137 blended = cv2.addWeighted(frameRgb, rgbWeight, frameDisp, depthWeight, 0)
138 cv2.imshow(blendedWindowName, blended)
139 frameRgb = None
140 frameDisp = None
141
142 if cv2.waitKey(1) == ord('q'):
143 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.