RGB & Mono Encoding
Similar samples:
Demo
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4
5# Create pipeline
6pipeline = dai.Pipeline()
7
8# Define sources and outputs
9camRgb = pipeline.create(dai.node.ColorCamera)
10monoLeft = pipeline.create(dai.node.MonoCamera)
11monoRight = pipeline.create(dai.node.MonoCamera)
12ve1 = pipeline.create(dai.node.VideoEncoder)
13ve2 = pipeline.create(dai.node.VideoEncoder)
14ve3 = pipeline.create(dai.node.VideoEncoder)
15
16ve1Out = pipeline.create(dai.node.XLinkOut)
17ve2Out = pipeline.create(dai.node.XLinkOut)
18ve3Out = pipeline.create(dai.node.XLinkOut)
19
20ve1Out.setStreamName('ve1Out')
21ve2Out.setStreamName('ve2Out')
22ve3Out.setStreamName('ve3Out')
23
24# Properties
25camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
26monoLeft.setCamera("left")
27monoRight.setCamera("right")
28# Create encoders, one for each camera, consuming the frames and encoding them using H.264 / H.265 encoding
29ve1.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H264_MAIN)
30ve2.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H265_MAIN)
31ve3.setDefaultProfilePreset(30, dai.VideoEncoderProperties.Profile.H264_MAIN)
32
33# Linking
34monoLeft.out.link(ve1.input)
35camRgb.video.link(ve2.input)
36monoRight.out.link(ve3.input)
37ve1.bitstream.link(ve1Out.input)
38ve2.bitstream.link(ve2Out.input)
39ve3.bitstream.link(ve3Out.input)
40
41# Connect to device and start pipeline
42with dai.Device(pipeline) as dev:
43
44 # Output queues will be used to get the encoded data from the outputs defined above
45 outQ1 = dev.getOutputQueue(name='ve1Out', maxSize=30, blocking=True)
46 outQ2 = dev.getOutputQueue(name='ve2Out', maxSize=30, blocking=True)
47 outQ3 = dev.getOutputQueue(name='ve3Out', maxSize=30, blocking=True)
48
49 # The .h264 / .h265 files are raw stream files (not playable yet)
50 with open('mono1.h264', 'wb') as fileMono1H264, open('color.h265', 'wb') as fileColorH265, open('mono2.h264', 'wb') as fileMono2H264:
51 print("Press Ctrl+C to stop encoding...")
52 while True:
53 try:
54 # Empty each queue
55 while outQ1.has():
56 outQ1.get().getData().tofile(fileMono1H264)
57
58 while outQ2.has():
59 outQ2.get().getData().tofile(fileColorH265)
60
61 while outQ3.has():
62 outQ3.get().getData().tofile(fileMono2H264)
63 except KeyboardInterrupt:
64 # Keyboard interrupt (Ctrl + C) detected
65 break
66
67 print("To view the encoded data, convert the stream file (.h264/.h265) into a video file (.mp4), using commands below:")
68 cmd = "ffmpeg -framerate 30 -i {} -c copy {}"
69 print(cmd.format("mono1.h264", "mono1.mp4"))
70 print(cmd.format("mono2.h264", "mono2.mp4"))
71 print(cmd.format("color.h265", "color.mp4"))Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.