Script camera control
Demo
This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2import cv2
3import depthai as dai
4
5# Start defining a pipeline
6pipeline = dai.Pipeline()
7
8# Define a source - color camera
9cam = pipeline.create(dai.node.ColorCamera)
10
11# Script node
12script = pipeline.create(dai.node.Script)
13script.setScript("""
14 import time
15 ctrl = CameraControl()
16 ctrl.setCaptureStill(True)
17 while True:
18 time.sleep(1)
19 node.io['out'].send(ctrl)
20""")
21
22# XLinkOut
23xout = pipeline.create(dai.node.XLinkOut)
24xout.setStreamName('still')
25
26# Connections
27script.outputs['out'].link(cam.inputControl)
28cam.still.link(xout.input)
29
30# Connect to device with pipeline
31with dai.Device(pipeline) as device:
32 while True:
33 img = device.getOutputQueue("still").get()
34 cv2.imshow('still', img.getCvFrame())
35 if cv2.waitKey(1) == ord('q'):
36 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.