Script MJPEG server
This example can only run on OAK POE devices. You need bootloader on/above version 0.0.15. You can flash bootloader by running
python3 examples/bootloader/flash_bootloader.py.Demo
Command Line
1Serving at 192.168.1.193:8080
if you click on the here href, you will get the MJPEG video stream. For static image, you can check out Script HTTP server.This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4import time
5
6# Start defining a pipeline
7pipeline = dai.Pipeline()
8
9# Define a source - color camera
10cam = pipeline.create(dai.node.ColorCamera)
11# VideoEncoder
12jpeg = pipeline.create(dai.node.VideoEncoder)
13jpeg.setDefaultProfilePreset(cam.getFps(), dai.VideoEncoderProperties.Profile.MJPEG)
14
15# Script node
16script = pipeline.create(dai.node.Script)
17script.setProcessor(dai.ProcessorType.LEON_CSS)
18script.setScript("""
19 import time
20 import socket
21 import fcntl
22 import struct
23 from socketserver import ThreadingMixIn
24 from http.server import BaseHTTPRequestHandler, HTTPServer
25
26 PORT = 8080
27
28 def get_ip_address(ifname):
29 s = socket.socket(socket.AF_INET, socket.SOCK_DGRAM)
30 return socket.inet_ntoa(fcntl.ioctl(
31 s.fileno(),
32 -1071617759, # SIOCGIFADDR
33 struct.pack('256s', ifname[:15].encode())
34 )[20:24])
35
36 class ThreadingSimpleServer(ThreadingMixIn, HTTPServer):
37 pass
38
39 class HTTPHandler(BaseHTTPRequestHandler):
40 def do_GET(self):
41 if self.path == '/':
42 self.send_response(200)
43 self.end_headers()
44 self.wfile.write(b'<h1>[DepthAI] Hello, world!</h1><p>Click <a href="img">here</a> for an image</p>')
45 elif self.path == '/img':
46 try:
47 self.send_response(200)
48 self.send_header('Content-type', 'multipart/x-mixed-replace; boundary=--jpgboundary')
49 self.end_headers()
50 fpsCounter = 0
51 timeCounter = time.time()
52 while True:
53 jpegImage = node.io['jpeg'].get()
54 self.wfile.write("--jpgboundary".encode())
55 self.wfile.write(bytes([13, 10]))
56 self.send_header('Content-type', 'image/jpeg')
57 self.send_header('Content-length', str(len(jpegImage.getData())))
58 self.end_headers()
59 self.wfile.write(jpegImage.getData())
60 self.end_headers()
61
62 fpsCounter = fpsCounter + 1
63 if time.time() - timeCounter > 1:
64 node.warn(f'FPS: {fpsCounter}')
65 fpsCounter = 0
66 timeCounter = time.time()
67 except Exception as ex:
68 node.warn(str(ex))
69
70 with ThreadingSimpleServer(("", PORT), HTTPHandler) as httpd:
71 node.warn(f"Serving at {get_ip_address('re0')}:{PORT}")
72 httpd.serve_forever()
73""")
74
75# Connections
76cam.video.link(jpeg.input)
77jpeg.bitstream.link(script.inputs['jpeg'])
78
79# Connect to device with pipeline
80with dai.Device(pipeline) as device:
81 while not device.isClosed():
82 time.sleep(1)Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.