ON THIS PAGE

  • What is Luxonis Hub Agent?

What is Luxonis Hub Agent?

The Hub Agent is installed on your local machine and provides communication with Luxonis' cloud service. It can be installed on Linux-based devices, including low-power devices such as Raspberry Pi. Limitations include a minimum of 2GB of RAM, with 4+ GB strongly recommended, and a 64-bit operating system (Ubuntu or Raspi OS). Please see the detailed installation guide.Before installation, please ensure that all necessary rules are correctly set up on your firewall.The agent has a command line interface (CLI) . For management, you can use classic SSH access to the device. Another option is remote access via the Hub. Please navigate to device detail, where you'll find access to the Web Terminal.Configuration of the agent can be done via its page in the cloud. Please navigate to Settings on its detail page. More advanced settings are available through the configuration file. Details about this topic can be found here.Tips on how to solve problems can be found in the troubleshooting guide.