Install Luxonis Hub Agent
Requirements
The following operating systems are officially supported.Operating system | |
---|---|
Ubuntu (Desktop or Server) | 20.04, 22.04 |
Raspberry Pi OS | any version |
Only 64-bit operating systems are supported!
To determine whether your system is 32 or 64 bit use the
getconf LONG_BIT
command.Raspberry 5 supported operating systems
Since Ubuntu 22.04 LTS is not officially supported on the Raspberry Pi 5, it is necessary to use Raspberry Pi OS with this hardware.
Hardware
RAM / Memory | |
---|---|
Minimum | 2 GB |
Recommended | 4 - 8 GB |
Development | 8+ GB |
Expected storage use
Storage | |
---|---|
Agent | 500 MB (2x to enable updates) |
Average Application (docker image) | 500 MB - 2 GB |
Average Application (source) | <100 MB |
Average Application (model) | 5 MB - 500 MB |
Events (video /images/files) | depends on use case |
Installation of the agent
If your system meets requirements, to install the agent please follow guide on this page .Uninstallation of the agent
To uninstall the agent please connect to the device via SSH run following code and reboot your system:Command Line
1sudo robothub-uninstall
Requires root privileges