Configuration
Deprecation Notice
This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.
robotapp.toml. The file is located in root directory of the app. Here is an example one:Toml
1config_version = "2.0"
2
3[info]
4name = "{{{ APP_NAME }}}"
5description = "This is a generated description. Replace it with your own."
6
7[runtime]
8application = "app.py#Application"
9workdir = "/app"
10
11[runtime.runs_on]
12type = "image"
13name = "ghcr.io/luxonis/robothub-app-v2:2023.326.2033-rvc2-regular"
14
15[[configuration]]
16visual = "section"
17title = "Upload intervals"
18
19[[configuration]]
20key = "image_event_upload_interval_minutes"
21label = "Image event upload interval (minutes)"
22field = "num_range"
23step = 1
24min = 1
25max = 60
26initial_value = 1Reference
Root fields
config_version The version of the configuration file format. Currently, the only supported version is 2.0.Info
info section contains information about the app, such as its name and description.| Field | Description |
|---|---|
info.name | The name of the app. Currently unused. |
info.description | The description of the app. Currently unused. |
Runtime
runtime section configures the runtime environment of the app.| Field | Description |
|---|---|
runtime.application | The name of the Python file containing the app's main logic. The path is relative to the root directory. |
runtime.workdir | The working directory of the app. Defaults to /app. |
runtime.permissions | The permissions required to run the app. Defaults to [].An example:Toml |
runtime.runs_on | The runtime container in which the app will run.type = "image"The app will run in a container based on the specified image. The image is pulled before installation.An example:Toml |
Configuration
configuration section defines the install-time configuration of the app.Visual| Type | Description |
|---|---|
divider | The divider to use for the configuration section.An example: Toml |
section | The section to use for the configuration section.An example: Toml |
| Type | Description |
|---|---|
boolean | A boolean field.An example: Toml |
num_range | A number range field.An example: Toml |
choice | A choice field.An example: Toml |
text | A text field.An example: Toml |
time_range | A time range field.An example: Toml |
roi_rect4_selector | A ROI selector on live stream field. Defined by 2 points (x0, y0) and (x1, y1).An example: Toml |
roi_rect8_selector | A ROI selector on live stream field. Defined by 4 points (x0, y0), (x1, y1), (x2, y2), (x3, y3).An example: Toml |