Depth and Detection live view
Deprecation Notice
This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.
Description
Depth Detection and ProcessingBeyond object identification, the application performs depth detection and processing. This provides valuable information on the distance or spatial arrangement of the objects in the scene.Live Visualization on the HubThe combined functionalities of object and depth detection are presented through a live view on the Hub. This allows users to observe both the video stream with detected objects and the corresponding depth information, offering a comprehensive understanding of the scene.