Auto/Fixed Focus
Overview
| Parameter | Fixed-Focus (FF) | Auto-Focus (AF) |
|---|---|---|
| Vibration Tolerance | High | Low |
| Focus Range | 50 cm to infinity | 10 cm to infinity |
| Manual Focus | No - lens is glued | Yes - programmatically |
Vibration Tolerance
Fixed-Focus (FF) is better for handling high-vibration environments.Auto-Focus uses Voice Coil Motor (VCM) to move the magnet that is mounted to a free-moving lens. In high vibrations, this electromagnetic force is overpowered and the lens vibrates all over the place, causing blurry/weird/"jello" frames.Some applications, where of high-vibrations:- Drone
- Lawn mower
- Heavy machinery
- Harley Davidson motorcycles (which are notorious for their vibrations), etc.
Focus Range
Auto-Focus (AF) is best here. Fixed-Focus can see clearly from ~50 cm (~20 inches) to infinity, whereas Auto-Focus can see clearly from 10 cm (~4 inches) to infinity.Auto-Focus accomplishes this wider Depth of Field (DoF) by actually moving the lens to a different position (~255 different steps) to focus at specific distances. The Auto-Focus model can be manually controlled via API as well, in 1/256 steps (see below).Manual Focus
Auto-Focus cameras can be manually controlled via DepthAI API. You can set the focus value (0..255) either in:- Runtime, with example here you can use
,and.to change focus - At boot time, with the following Python code:
Python
1pipeline = dai.Pipeline()
2rgbCam = pipeline.create(dai.node.ColorCamera)
3rgbCam.initialControl.setManualFocus(100) # 0..255Recognizing focus type
If you aren't sure whether the OAK in front of you has Auto-Focus or Fixed-Focus color camera, you can recognize it by the silver metal ring on the Auto-Focus mechanism, as shown in the image below.
Another possibility would be to query this information using DepthAI API library:Python
1import depthai as dai
2with dai.Device() as device:
3 print(device.getConnectedCameraFeatures())hasAutofocusIC field will be 1 for the AF camera, and 0 for the FF camera. So in this case, our OAK-D camera is AF:Python
1[
2 {socket: CAM_A, sensorName: IMX378, width: 4056, height: 3040, orientation: AUTO, supportedTypes: [COLOR], hasAutofocus: 0, hasAutofocusIC: 1, name: color},
3 {socket: CAM_B, sensorName: OV9282, width: 1280, height: 800, orientation: AUTO, supportedTypes: [MONO], hasAutofocus: 0, hasAutofocusIC: 0, name: left},
4 {socket: CAM_C, sensorName: OV9282, width: 1280, height: 800, orientation: AUTO, supportedTypes: [MONO], hasAutofocus: 0, hasAutofocusIC: 0, name: right}
5]hasAutofocusfield is what is stored in EEPROM (can be incorrect) and is mostly there for backwards compatibility.hasAutofocusICfield is the actual value read from the camera module (VCM controller). This field is the one you should rely on.