# Blobconverter (legacy)

> **Note**
> This is a legacy tool. We suggest switching to [Luxonis Hub Conversion](https://docs.luxonis.com/cloud/hubai/model-registry/detailed-conversion.md) or using the Python API as described in the [migration guide](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/online/hubai.md).

## Overview

The BlobConverter is our [open-source tool](https://github.com/luxonis/blobconverter) that supports conversion to a MyriadX
(`.blob`) format compatible with RVC2 and RVC3 Luxonis devices. The tool is accessible through a web interface and an API. This
section guides you through all the conversion options.

## Conversion

### BlobConverter Web Interface

 * Go to the [BlobConverter website](https://blobconverter.luxonis.com/).
 * Select the OpenVINO version you wish to utilize. We will be using the latest version supported by BlobConverter, which is
   currently `2022.1`. For RAE and other devices with RVC3, you can simply pick RVC3. After choosing the version, indicate the
   model source. In our case, the ONNX Model, but it is also possible to upload your model in the IR format. Then click on
   `Continue`.

![Blobconverter menu](https://docs.luxonis.com/static/images/blobconverter-menu.webp)

 * Upload the ONNX file by clicking on `Choose file`.

![Blobconverter upload](https://docs.luxonis.com/static/images/blobconverter-upload.webp)

 * Additionally, before proceeding with the model conversion, you can customize [conversion parameters](#Advanced%20Settings) by
   clicking on `Advanced`.

![Blobconverter advanced](https://docs.luxonis.com/static/images/blobconverter-advanced.webp)

 * Finally, click on `Convert` and simply wait until the process is finished.

### BlobConverter Python

We offer BlobConverter as a Python package as well ([PyPI link](https://pypi.org/project/blobconverter/)). You can install it
using pip:

```bash
pip install blobconverter
```

Now you can convert your ONNX model to a blob with the specified conversion parameters.

```python
import blobconverter

blob_path = blobconverter.from_onnx(
    model="/path/to/model.onnx",
    data_type="FP16",
    shaves=6,
    version="2022.1"
)
```

You can check out more examples for conversion from different model sources
[here](https://github.com/luxonis/blobconverter/tree/master/cli#conversion-examples-python).

### BlobConverter API

Alternatively, you can use the BlobConverter API, which is particularly useful for automated workflows. This can be done by making
HTTP requests to the BlobConverter service with the necessary model and parameters. You can find more information on how to do
this by clicking on the `Use API` button at the top right corner of the website.

> **Note**
> Note: The BlobConverter tool can also be self-hosted. For guidance on this process, please refer to the instructions available in our [BlobConverter repository](https://github.com/luxonis/blobconverter/tree/master).

## Export Example

This guide will walk you through the process of exporting ResNet18, a widely-used deep neural network for image classification, to
a `.blob` file for deployment on OAK devices. We will use torchvision for accessing the pre-trained version of the model.

> **Note**
> For converting YOLO models, consider using [our specialized tool](https://tools.luxonis.com/) designed for this task. For detailed guidance on the YOLO conversion process, please visit [this documentation page](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/online/yolo.md).

### Exporting the Model to ONNX

First, we will export the ResNet18 model from PyTorch to the ONNX format.

```python
import torch
import torchvision.models as models

# Load the pretrained ResNet18 model from torchvision
resnet18 = models.resnet18(pretrained=True)

# Set the model to evaluation mode
resnet18.eval()

# Create a dummy input tensor matching the input shape of the model
dummy_input = torch.randn(1, 3, 224, 224)

# Export the model to an ONNX file
torch.onnx.export(
resnet18,
dummy_input,
'resnet18.onnx',
export_params=True,
opset_version=11,
input_names=['input'],
output_names=['output']
)
```

Parameters Explanation:

 * `export_params`: This flag ensures that the trained parameters are exported along with the model structure.
 * `opset_version`: Specifies the ONNX version to use. While we typically use version 11 to ensure compatibility with ResNet18's
   requirements, higher versions could also be applicable.
 * `input_names` and `output_names`: We use these flags to name the model's input and output nodes for clarity. In our example,
   the input node is named "input" and the output node "output".
 * After exporting, you'll get a file named "resnet18.onnx" as defined in the third argument.

### Convert ONNX to .blob Using BlobConverter

Instead of manually converting the ONNX file to OpenVINO IR and then compiling it, we'll use BlobConverter to handle both steps.

 * Go to the [BlobConverter website](https://blobconverter.luxonis.com/).
 * Choose the appropriate OpenVINO version, which for this example, is `2022.1`.
 * Upload the `.onnx` file and enter any necessary Model Optimizer parameters in the 'Advanced' settings.
 * `--data_type`: Set to 'FP16' for compatible precision with the VPU processor.
 * `--mean_values`: Set to [123.675, 116.28, 103.53]. These values correspond to the average of the red, green, and blue channels
   across all images in the ImageNet dataset (on which ResNet18 was trained).
 * `--scale_values`: Set to [58.395, 57.12, 57.375] which are the standard deviations of each channel. This scaling ensures that
   the range of pixel values in the input image matches the range in the training data, which is important for the model to
   perform correctly.
 * `--reverse_input_channels`: Use this flag to switch from BGR to RGB, since the `Camera` node outputs frames in the BGR format,
   and the model requires RGB images.
 * So at the end, the flags should look like this:

```bash
--data_type=FP16 --mean_values=[123.675,116.28,103.53] --scale_values=[58.395,57.12,57.375] --reverse_input_channels
```

 * Click `Convert` to start the conversion and then download the `.blob` file once the process is completed.

![ResNet18 Conversion](https://docs.luxonis.com/static/images/blobconverter-resnet.webp)

After following these instructions, you will get a `resnet18.blob` file that is ready for inference on OAK devices. The converted
model will expect images in the BGR format with pixel values ranging from 0 to 255. Then these will be scaled to a range of 0 to 1
and normalized using the flags we set.