Software Stack
DepthAI

ON THIS PAGE

  • AprilTags from camera
  • Demo
  • Pipeline
  • Source code

AprilTags from camera

Utilizes the AprilTag node to detect apriltag markers on the camera stream at 1080P. It outlines detected tags and their IDs on the screen. Check the AprilTags on 12MP frames example for potentially better detection results.

Demo

This example requires the DepthAI v3 API, see installation instructions.

Pipeline

Source code

Python
C++

Python

Python
GitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5import time
6
7with dai.Pipeline() as pipeline:
8    hostCamera = pipeline.create(dai.node.Camera).build()
9    aprilTagNode = pipeline.create(dai.node.AprilTag)
10    hostCamera.requestOutput((1920, 1080)).link(aprilTagNode.inputImage)
11    passthroughOutputQueue = aprilTagNode.passthroughInputImage.createOutputQueue()
12    outQueue = aprilTagNode.out.createOutputQueue()
13
14    color = (0, 255, 0)
15    startTime = time.monotonic()
16    counter = 0
17    fps = 0.0
18
19    pipeline.start()
20    while pipeline.isRunning():
21        aprilTagMessage = outQueue.get()
22        assert(isinstance(aprilTagMessage, dai.AprilTags))
23        aprilTags = aprilTagMessage.aprilTags
24
25        counter += 1
26        currentTime = time.monotonic()
27        if (currentTime - startTime) > 1:
28            fps = counter / (currentTime - startTime)
29            counter = 0
30            startTime = currentTime
31
32        passthroughImage: dai.ImgFrame = passthroughOutputQueue.get()
33        frame = passthroughImage.getCvFrame()
34
35        def to_int(tag):
36            return (int(tag.x), int(tag.y))
37
38        for tag in aprilTags:
39            topLeft = to_int(tag.topLeft)
40            topRight = to_int(tag.topRight)
41            bottomRight = to_int(tag.bottomRight)
42            bottomLeft = to_int(tag.bottomLeft)
43
44            center = (int((topLeft[0] + bottomRight[0]) / 2), int((topLeft[1] + bottomRight[1]) / 2))
45
46            cv2.line(frame, topLeft, topRight, color, 2, cv2.LINE_AA, 0)
47            cv2.line(frame, topRight,bottomRight, color, 2, cv2.LINE_AA, 0)
48            cv2.line(frame, bottomRight,bottomLeft, color, 2, cv2.LINE_AA, 0)
49            cv2.line(frame, bottomLeft,topLeft, color, 2, cv2.LINE_AA, 0)
50
51            idStr = "ID: " + str(tag.id)
52            cv2.putText(frame, idStr, center, cv2.FONT_HERSHEY_TRIPLEX, 0.5, color)
53
54            cv2.putText(frame, f"fps: {fps:.1f}", (200, 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, color)
55
56        cv2.imshow("detections", frame)
57        if cv2.waitKey(1) == ord("q"):
58            break

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.