# Benchmark NN

This example showcases how to use both the [BenchmarkOut
node](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/benchmark_out.md) and the
[BenchmarkIn](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/benchmark_in.md) node to measure the
performance of a NN model.

BenchmarkIn outputs messages as fast as possible, which is used to measure the performance of a NN model (by linking `BenchmarkOut
-> NeuralNetwork -> BenchmarkIn`).

## Demo

The `yolov6-nano` NN model should run at ~273 FPS on an OAK4 camera, and at ~67 FPS on an OAK camera.

```bash
Benchmark $ python3.9 benchmark_nn.py
FPS is 273.2430114746094
FPS is 273.161376953125
FPS is 273.22802734375
```

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- XLinkIn(5)
- BenchmarkOut (0)
- NeuralNetwork (1)
- BenchmarkIn (2)
- XLinkOut (6)

Pipeline connections:
- XLinkIn(5) -> BenchmarkOut (0) (out -> input)
- BenchmarkIn (2) -> XLinkOut (6) (report -> in)
- NeuralNetwork (1) -> BenchmarkIn (2) (out -> input)
- BenchmarkOut (0) -> NeuralNetwork (1) (out -> in)

## Source code

#### Python

```python
import depthai as dai
import numpy as np

# First prepare the model for benchmarking
device = dai.Device()
modelPath = dai.getModelFromZoo(dai.NNModelDescription("yolov6-nano", platform=device.getPlatformAsString()))
modelArhive = dai.NNArchive(modelPath)
inputSize = modelArhive.getInputSize()
type = modelArhive.getConfig().model.inputs[0].preprocessing.daiType

if type:
    try:
        frameType = getattr(dai.ImgFrame.Type, type)
    except AttributeError:
        type = None

if not type:
    if device.getPlatform() == dai.Platform.RVC2:
        frameType = dai.ImgFrame.Type.BGR888p
    else:
        frameType = dai.ImgFrame.Type.BGR888i

# Construct the input (white) image for benchmarking
img = np.ones((inputSize[1], inputSize[0], 3), np.uint8) * 255
inputFrame = dai.ImgFrame()
inputFrame.setCvFrame(img, frameType)

with dai.Pipeline(device) as p:
    benchmarkOut = p.create(dai.node.BenchmarkOut)
    benchmarkOut.setRunOnHost(False) # The node can run on host or on device
    benchmarkOut.setFps(-1) # As fast as possible

    neuralNetwork = p.create(dai.node.NeuralNetwork).build(benchmarkOut.out, modelArhive)

    benchmarkIn = p.create(dai.node.BenchmarkIn)
    benchmarkIn.setRunOnHost(False) # The node can run on host or on device
    benchmarkIn.sendReportEveryNMessages(100)
    benchmarkIn.logReportsAsWarnings(False)
    neuralNetwork.out.link(benchmarkIn.input)

    outputQueue = benchmarkIn.report.createOutputQueue()
    inputQueue = benchmarkOut.input.createInputQueue()

    p.start()
    inputQueue.send(inputFrame) # Send the input image only once
    while p.isRunning():
        benchmarkReport = outputQueue.get()
        assert isinstance(benchmarkReport, dai.BenchmarkReport)
        print(f"FPS is {benchmarkReport.fps}")
```

#### C++

```cpp
#include <atomic>
#include <csignal>
#include <depthai/depthai.hpp>
#include <iostream>
#include <opencv2/opencv.hpp>

std::atomic<bool> quitEvent(false);

void signalHandler(int) {
    quitEvent = true;
}

int main() {
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    // First prepare the model for benchmarking
    std::shared_ptr<dai::Device> device = std::make_shared<dai::Device>();

    dai::NNModelDescription modelDescription;
    modelDescription.model = "yolov6-nano";
    modelDescription.platform = device->getPlatformAsString();

    auto modelPath = getModelFromZoo(modelDescription);
    dai::NNArchive modelArchive(modelPath);
    auto inputSize = modelArchive.getInputSize().value();

    dai::ImgFrame::Type frameType;
    if(device->getPlatform() == dai::Platform::RVC2) {
        frameType = dai::ImgFrame::Type::BGR888p;
    } else {
        frameType = dai::ImgFrame::Type::BGR888i;
    }

    // Construct the input (white) image for benchmarking
    cv::Mat img(std::get<1>(inputSize), std::get<0>(inputSize), CV_8UC3, cv::Scalar(255, 255, 255));
    auto inputFrame = std::make_shared<dai::ImgFrame>();
    inputFrame->setCvFrame(img, frameType);

    dai::Pipeline pipeline(device);

    auto benchmarkOut = pipeline.create<dai::node::BenchmarkOut>();
    benchmarkOut->setRunOnHost(false);  // The node can run on host or on device
    benchmarkOut->setFps(-1);           // As fast as possible

    auto neuralNetwork = pipeline.create<dai::node::NeuralNetwork>();
    neuralNetwork->setNNArchive(modelArchive);

    auto benchmarkIn = pipeline.create<dai::node::BenchmarkIn>();
    benchmarkIn->setRunOnHost(false);  // The node can run on host or on device
    benchmarkIn->sendReportEveryNMessages(100);
    benchmarkIn->logReportsAsWarnings(false);

    // Linking
    benchmarkOut->out.link(neuralNetwork->input);
    neuralNetwork->out.link(benchmarkIn->input);

    auto outputQueue = benchmarkIn->report.createOutputQueue();
    auto inputQueue = benchmarkOut->input.createInputQueue();

    pipeline.start();
    inputQueue->send(inputFrame);

    while(pipeline.isRunning() && !quitEvent) {
        auto benchmarkReport = outputQueue->get<dai::BenchmarkReport>();
        std::cout << "FPS is " << benchmarkReport->fps << std::endl;
    }

    pipeline.stop();
    pipeline.wait();

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.