# Detection network Remap

This example demonstrates running YOLOv6 object detection on an RGB stream while simultaneously processing stereo depth data,
displaying bounding boxes on both the RGB and colorized depth frames.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- NeuralNetwork (2)
- XLinkOut (7)
- DetectionParser (3)
- XLinkOut (9)
- Camera(4)
- StereoDepth (6)
- XLinkOut (11)
- Camera(5)

Pipeline connections:
- StereoDepth (6) -> XLinkOut (11) (disparity -> in)
- Camera(5) -> StereoDepth (6) (0 -> right)
- Camera(4) -> StereoDepth (6) (0 -> left)
- NeuralNetwork (2) -> XLinkOut (7) (passthrough -> in)
- NeuralNetwork (2) -> DetectionParser (3) (passthrough -> imageIn)
- NeuralNetwork (2) -> DetectionParser (3) (out -> in)
- DetectionParser (3) -> XLinkOut (9) (out -> in)
- Camera(0) -> NeuralNetwork (2) (0 -> in)

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai

# Create pipeline
with dai.Pipeline() as pipeline:
    colorSockets = pipeline.getDefaultDevice().getConnectedCameras(dai.CameraSensorType.COLOR)
    colorSocket = colorSockets[0] if colorSockets else dai.CameraBoardSocket.CAM_A
    cameraNode = pipeline.create(dai.node.Camera).build(colorSocket)
    detectionNetwork = pipeline.create(dai.node.DetectionNetwork).build(cameraNode, dai.NNModelDescription("yolov6-nano"))
    labelMap = detectionNetwork.getClasses()
    depth = pipeline.create(dai.node.Depth).build(dai.node.Depth.Algorithm.AUTO, None)

    qRgb = detectionNetwork.passthrough.createOutputQueue()
    qDet = detectionNetwork.out.createOutputQueue()
    qDepth = depth.depth.createOutputQueue()

    pipeline.start()

    def displayFrame(name: str, frame: dai.ImgFrame, imgDetections: dai.ImgDetections):
        color = (0, 255, 0)
        assert imgDetections.getTransformation() is not None
        if(frame.getType() == dai.ImgFrame.Type.RAW16):
            cvFrame = dai.utility.colorizeDepthFrame(frame).getCvFrame()
        else:
            cvFrame = frame.getCvFrame()
        for detection in imgDetections.detections:
            # Get the shape of the frame from which the detections originated for denormalization
            normShape = imgDetections.getTransformation().getSize()

            # Create rotated rectangle to remap
            # Here we use an intermediate dai.Rect to create a dai.RotatedRect to simplify construction and denormalization
            rotRect = dai.RotatedRect(dai.Rect(dai.Point2f(detection.xmin, detection.ymin), dai.Point2f(detection.xmax, detection.ymax), True).denormalize(normShape[0], normShape[1]), 0)
            # Remap the detection rectangle to target frame
            remapped = imgDetections.getTransformation().remapRectTo(frame.getTransformation(), rotRect)
            # Remapped rectangle could be rotated, so we get the bounding box
            bbox = [int(l) for l in remapped.getOuterRect()]
            cv2.putText(
                cvFrame,
                labelMap[detection.label],
                (bbox[0] + 10, bbox[1] + 20),
                cv2.FONT_HERSHEY_TRIPLEX,
                0.5,
                255,
            )
            cv2.putText(
                cvFrame,
                f"{int(detection.confidence * 100)}%",
                (bbox[0] + 10, bbox[1] + 40),
                cv2.FONT_HERSHEY_TRIPLEX,
                0.5,
                255,
            )
            cv2.rectangle(cvFrame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), color, 2)
        # Show the frame
        cv2.imshow(name, cvFrame)

    while pipeline.isRunning():
        inRgb: dai.ImgFrame = qRgb.get()
        inDet: dai.ImgDetections = qDet.get()
        inDepth: dai.ImgFrame = qDepth.get()
        hasRgb = inRgb is not None
        hasDepth = inDepth is not None
        hasDet = inDet is not None
        if hasRgb:
            displayFrame("rgb", inRgb, inDet)
        if hasDepth:
            displayFrame("depth", inDepth, inDet)
        if cv2.waitKey(1) == ord("q"):
            pipeline.stop()
            break
```

#### C++

```cpp
#include <csignal>
#include <iostream>
#include <opencv2/opencv.hpp>
#include <string>
#include <vector>

#include "depthai/depthai.hpp"

std::atomic<bool> quitEvent(false);

void signalHandler(int) {
    quitEvent = true;
}

// Helper function to display frames with detections
void displayFrame(const std::string& name,
                  std::shared_ptr<dai::ImgFrame> frame,
                  std::shared_ptr<dai::ImgDetections> imgDetections,
                  const std::vector<std::string>& labelMap) {
    cv::Scalar color(0, 255, 0);
    cv::Mat cvFrame;

    if(frame->getType() == dai::ImgFrame::Type::RAW16) {
        cvFrame = dai::utility::colorizeDepthFrame(*frame).getCvFrame();
    } else {
        cvFrame = frame->getCvFrame();
    }

    if(!imgDetections || !imgDetections->transformation.has_value()) {
        // std::cout << "No detections or transformation data for " << name << std::endl;
        cv::imshow(name, cvFrame);
        return;
    }

    const auto& sourceTransform = *(imgDetections->transformation);
    const auto& targetTransform = frame->transformation;

    for(const auto& detection : imgDetections->detections) {
        auto normShape = sourceTransform.getSize();

        dai::Rect rect(dai::Point2f(detection.xmin, detection.ymin), dai::Point2f(detection.xmax, detection.ymax), true);
        rect = rect.denormalize(static_cast<float>(normShape.first), static_cast<float>(normShape.second));
        dai::RotatedRect rotRect(rect, 0);

        auto remapped = sourceTransform.remapRectTo(targetTransform, rotRect);
        auto bbox = remapped.getOuterRect();

        cv::putText(cvFrame,
                    labelMap[detection.label],
                    cv::Point(static_cast<int>(bbox[0]) + 10, static_cast<int>(bbox[1]) + 20),
                    cv::FONT_HERSHEY_TRIPLEX,
                    0.5,
                    cv::Scalar(255, 255, 255));
        cv::putText(cvFrame,
                    std::to_string(static_cast<int>(detection.confidence * 100)) + "%",
                    cv::Point(static_cast<int>(bbox[0]) + 10, static_cast<int>(bbox[1]) + 40),
                    cv::FONT_HERSHEY_TRIPLEX,
                    0.5,
                    cv::Scalar(255, 255, 255));
        cv::rectangle(cvFrame,
                      cv::Point(static_cast<int>(bbox[0]), static_cast<int>(bbox[1])),
                      cv::Point(static_cast<int>(bbox[2]), static_cast<int>(bbox[3])),
                      color,
                      2);
    }
    cv::imshow(name, cvFrame);
}

int main() {
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    dai::Pipeline pipeline;

    auto colorSockets = pipeline.getDefaultDevice()->getConnectedCameras(dai::CameraSensorType::COLOR);
    auto colorSocket = colorSockets.empty() ? dai::CameraBoardSocket::CAM_A : colorSockets.front();
    auto cameraNode = pipeline.create<dai::node::Camera>();
    cameraNode->build(colorSocket);

    auto detectionNetwork = pipeline.create<dai::node::DetectionNetwork>();
    dai::NNModelDescription modelDescription;
    modelDescription.model = "yolov6-nano";
    detectionNetwork->build(cameraNode, modelDescription);
    auto labelMap = detectionNetwork->getClasses().value_or(std::vector<std::string>{});

    auto depth = pipeline.create<dai::node::Depth>();
    depth->build(dai::node::Depth::Algorithm::AUTO);

    auto qRgb = detectionNetwork->passthrough.createOutputQueue();
    auto qDet = detectionNetwork->out.createOutputQueue();
    auto qDepth = depth->depth().createOutputQueue();

    pipeline.start();

    while(pipeline.isRunning() && !quitEvent) {
        auto inRgb = qRgb->tryGet<dai::ImgFrame>();
        auto inDet = qDet->tryGet<dai::ImgDetections>();
        auto inDepth = qDepth->tryGet<dai::ImgFrame>();

        bool hasRgb = inRgb != nullptr;
        bool hasDepth = inDepth != nullptr;
        bool hasDet = inDet != nullptr;

        if(hasRgb && hasDet) {
            displayFrame("rgb", inRgb, inDet, labelMap);
        }
        if(hasDepth && hasDet) {
            displayFrame("depth", inDepth, inDet, labelMap);
        }

        if(cv::waitKey(1) == 'q') {
            pipeline.stop();
            break;
        }
    }

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.