# Detection network Replay

This example demonstrates using DepthAI's RemoteConnection to stream and visualize YOLOv6 object detection results and video
frames from a replayed video file.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- XLinkIn(5)
- NeuralNetwork (2)
- DetectionParser (3)
- XLinkOut (6)

Pipeline connections:
- XLinkIn(5) -> NeuralNetwork (2) (out -> in)
- DetectionParser (3) -> XLinkOut (6) (out -> in)
- NeuralNetwork (2) -> DetectionParser (3) (passthrough -> imageIn)
- NeuralNetwork (2) -> DetectionParser (3) (out -> in)

## Source code

#### Python

```python

#!/usr/bin/env python3
import depthai as dai
from pathlib import Path
from argparse import ArgumentParser

scriptDir = Path(__file__).resolve().parent
examplesRoot = (scriptDir / Path('../')).resolve()  # This resolves the parent directory correctly
models = examplesRoot / 'models'
videoPath = models / 'construction_vest.mp4'

parser = ArgumentParser()
parser.add_argument("--webSocketPort", type=int, default=8765)
parser.add_argument("--httpPort", type=int, default=8082)
parser.add_argument("-i", "--inputVideo", default=videoPath, help="Input video name")
args = parser.parse_args()

remoteConnector = dai.RemoteConnection(webSocketPort=args.webSocketPort, httpPort=args.httpPort)
# Create pipeline
with dai.Pipeline() as pipeline:
    replay = pipeline.create(dai.node.ReplayVideo)
    replay.setReplayVideoFile(Path(args.inputVideo))
    detectionNetwork = pipeline.create(dai.node.DetectionNetwork).build(
        replay, dai.NNModelDescription("yolov6-nano")
    )

    remoteConnector.addTopic("detections", detectionNetwork.out, "img")
    remoteConnector.addTopic("images", replay.out, "img")

    pipeline.start()
    remoteConnector.registerPipeline(pipeline)

    while pipeline.isRunning():
        key = remoteConnector.waitKey(1)
        if key == ord("q"):
            print("Got q key from the remote connection!")
            break
```

#### C++

```cpp
#include <csignal>
#include <depthai/depthai.hpp>
#include <depthai/remote_connection/RemoteConnection.hpp>
#include <iostream>

#include "depthai/modelzoo/Zoo.hpp"

// Signal handling for clean shutdown
static bool isRunning = true;
void signalHandler(int signum) {
    isRunning = false;
}

int main(int argc, char** argv) {
    // Default port values
    int webSocketPort = 8765;
    int httpPort = 8082;

    // Register signal handler
    std::signal(SIGINT, signalHandler);

    // Create RemoteConnection
    dai::RemoteConnection remoteConnector(dai::RemoteConnection::DEFAULT_ADDRESS, webSocketPort, true, httpPort);

    // Create Pipeline
    dai::Pipeline pipeline;
    auto replay = pipeline.create<dai::node::ReplayVideo>();
    replay->setReplayVideoFile(VIDEO_PATH);

    // Create and configure Detection Network
    auto detectionNetwork = pipeline.create<dai::node::DetectionNetwork>()->build(replay, dai::NNModelDescription{"yolov6-nano"});

    // Set up topics for remote connection
    remoteConnector.addTopic("detections", detectionNetwork->out);
    remoteConnector.addTopic("images", replay->out);
    pipeline.start();

    remoteConnector.registerPipeline(pipeline);
    // Main loop
    while(isRunning && pipeline.isRunning()) {
        int key = remoteConnector.waitKey(1);
        if(key == 'q') {
            std::cout << "Got 'q' key from the remote connection!" << std::endl;
            break;
        }
    }

    std::cout << "Pipeline stopped." << std::endl;
    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.