# Host Display

This example demonstrates how to use a `HostDisplay` node within a DepthAI pipeline to display frames obtained from the device
using OpenCV. The `HostDisplay` node is a custom host node that receives image frames from the DepthAI pipeline and displays them
on the host machine using OpenCV's `imshow` function.

The examples serves as an alternative to manually calling `.get()` on pipeline queues to retrieve frames and display them using
OpenCV. Instead, the `HostDisplay` node handles the frame retrieval and display process, making it easier to visualize the output
of the pipeline. It is the most basic example of a custom host node.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- XLinkOut (3)

Pipeline connections:
- Camera(0) -> XLinkOut (3) (0 -> in)

## Source Code

#### Python

```python
import depthai as dai
import cv2

class HostDisplay(dai.node.HostNode):
    def build(self, frameOutput: dai.Node.Output):
        self.link_args(frameOutput) # Has to match the inputs to the `process` method

        # This sends all the processing to the pipeline where it's executed by the `pipeline.runTasks()` or implicitly by `pipeline.run()` method.
        # It's needed as the GUI window needs to be updated in the main thread, and the `process` method is by default called in a separate thread.
        self.sendProcessingToPipeline(True)
        return self

    def process(self, message: dai.ImgFrame):
        cv2.imshow("HostDisplay", message.getCvFrame())
        key = cv2.waitKey(1)
        if key == ord('q'):
            print("Detected 'q' - stopping the pipeline...")
            self.stopPipeline()

# with dai.Pipeline() as p:
p = dai.Pipeline()
with p:
    camera = p.create(dai.node.Camera).build()
    hostDisplay = p.create(HostDisplay).build(camera.requestOutput((300, 300)))

    p.run() # Will block until the pipeline is stopped by someone else (in this case it's the display node)
```

#### C++

```cpp
#include <atomic>
#include <csignal>
#include <iostream>
#include <memory>
#include <opencv2/opencv.hpp>

#include "depthai/depthai.hpp"

std::atomic<bool> quitEvent(false);

void signalHandler(int) {
    quitEvent = true;
}

// Custom host node for display
class HostDisplay : public dai::node::CustomNode<HostDisplay> {
   public:
    HostDisplay() {
        sendProcessingToPipeline(true);
    }

    std::shared_ptr<dai::Buffer> processGroup(std::shared_ptr<dai::MessageGroup> message) override {
        if(quitEvent) {
            stopPipeline();
            return nullptr;
        }
        if(message == nullptr) return nullptr;

        auto frame = message->get<dai::ImgFrame>("frame");
        if(frame == nullptr) return nullptr;

        cv::imshow("HostDisplay", frame->getCvFrame());
        int key = cv::waitKey(1);
        if(key == 'q') {
            std::cout << "Detected 'q' - stopping the pipeline..." << std::endl;
            stopPipeline();
        }

        return nullptr;
    }
};

int main() {
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    // Create device
    std::shared_ptr<dai::Device> device = std::make_shared<dai::Device>();

    // Create pipeline
    dai::Pipeline pipeline(device);

    // Create nodes
    auto camera = pipeline.create<dai::node::Camera>()->build();
    auto output = camera->requestOutput(std::make_pair(300, 300));

    // Create display node
    auto display = pipeline.create<HostDisplay>();
    output->link(display->inputs["frame"]);

    // Start pipeline
    pipeline.run();

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.