# Depth Align

This example shows how to align the stereo depth map to the RGB frame to get RGB-D frames.

## Demo

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- ImageAlign (5)
- Sync (4)
- Camera(1)
- StereoDepth (3)
- Camera(2)

Pipeline connections:
- ImageAlign (5) -> Sync (4) (outputAligned -> depth_aligned)
- StereoDepth (3) -> ImageAlign (5) (depth -> input)
- Camera(2) -> StereoDepth (3) (0 -> right)
- Camera(1) -> StereoDepth (3) (0 -> left)
- Camera(0) -> ImageAlign (5) (0 -> inputAlignTo)
- Camera(0) -> Sync (4) (0 -> rgb)

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
import time
from datetime import timedelta
FPS = 25.0

RGB_SOCKET = dai.CameraBoardSocket.CAM_A
LEFT_SOCKET = dai.CameraBoardSocket.CAM_B
RIGHT_SOCKET = dai.CameraBoardSocket.CAM_C

class FPSCounter:
    def __init__(self):
        self.frameTimes = []

    def tick(self):
        now = time.time()
        self.frameTimes.append(now)
        self.frameTimes = self.frameTimes[-10:]

    def getFps(self):
        if len(self.frameTimes) <= 1:
            return 0
        return (len(self.frameTimes) - 1) / (self.frameTimes[-1] - self.frameTimes[0])

pipeline = dai.Pipeline()

platform = pipeline.getDefaultDevice().getPlatform()

# Define sources and outputs
camRgb = pipeline.create(dai.node.Camera).build(RGB_SOCKET)
left = pipeline.create(dai.node.Camera).build(LEFT_SOCKET)
right = pipeline.create(dai.node.Camera).build(RIGHT_SOCKET)
stereo = pipeline.create(dai.node.StereoDepth)
sync = pipeline.create(dai.node.Sync)
if platform == dai.Platform.RVC4:
    align = pipeline.create(dai.node.ImageAlign)

stereo.setExtendedDisparity(True)
sync.setSyncThreshold(timedelta(seconds=1/(2*FPS)))

rgbOut = camRgb.requestOutput(size = (1280, 960), fps = FPS, enableUndistortion=True)
leftOut = left.requestOutput(size = (640, 400), fps = FPS)
rightOut = right.requestOutput(size = (640, 400), fps = FPS)

# Linking
rgbOut.link(sync.inputs["rgb"])
leftOut.link(stereo.left)
rightOut.link(stereo.right)
if platform == dai.Platform.RVC4:
    stereo.depth.link(align.input)
    rgbOut.link(align.inputAlignTo)
    align.outputAligned.link(sync.inputs["depth_aligned"])
else:
    stereo.depth.link(sync.inputs["depth_aligned"])
    rgbOut.link(stereo.inputAlignTo)

queue = sync.out.createOutputQueue()

rgbWeight = 0.4
depthWeight = 0.6

def updateBlendWeights(percentRgb):
    """
    Update the rgb and depth weights used to blend depth/rgb image

    @param[in] percent_rgb The rgb weight expressed as a percentage (0..100)
    """
    global depthWeight
    global rgbWeight
    rgbWeight = float(percentRgb) / 100.0
    depthWeight = 1.0 - rgbWeight

# Connect to device and start pipeline
with pipeline:
    pipeline.start()

    # Configure windows; trackbar adjusts blending ratio of rgb/depth
    windowName = "rgb-depth"

    # Set the window to be resizable and the initial size
    cv2.namedWindow(windowName, cv2.WINDOW_NORMAL)
    cv2.resizeWindow(windowName, 1280, 720)
    cv2.createTrackbar(
        "RGB Weight %",
        windowName,
        int(rgbWeight * 100),
        100,
        updateBlendWeights,
    )
    fpsCounter = FPSCounter()
    while True:
        messageGroup = queue.get()
        fpsCounter.tick()
        assert isinstance(messageGroup, dai.MessageGroup)
        frameRgb = messageGroup["rgb"]
        assert isinstance(frameRgb, dai.ImgFrame)
        frameDepth = messageGroup["depth_aligned"]
        assert isinstance(frameDepth, dai.ImgFrame)

        # Blend when both received
        if frameDepth is not None:
            cvFrame = frameRgb.getCvFrame()
            # Colorize the aligned depth
            alignedDepthColorized = dai.utility.colorizeDepthFrame(frameDepth).getCvFrame()
            # Resize depth to match the rgb frame
            cv2.imshow("Depth aligned", alignedDepthColorized)

            if len(cvFrame.shape) == 2:
                cvFrameUndistorted = cv2.cvtColor(cvFrame, cv2.COLOR_GRAY2BGR)
            blended = cv2.addWeighted(
                cvFrame, rgbWeight, alignedDepthColorized, depthWeight, 0
            )
            cv2.putText(
                blended,
                f"FPS: {fpsCounter.getFps():.2f}",
                (10, 30),
                cv2.FONT_HERSHEY_SIMPLEX,
                1,
                (255, 255, 255),
                2,
            )
            cv2.imshow(windowName, blended)

        key = cv2.waitKey(1)
        if key == ord("q"):
            break
```

#### C++

```cpp
#include <atomic>
#include <chrono>
#include <cmath>
#include <csignal>
#include <deque>
#include <iostream>
#include <opencv2/opencv.hpp>
#include <optional>
#include <string>
#include <vector>

#include "depthai/depthai.hpp"

std::atomic<bool> quitEvent(false);

void signalHandler(int) {
    quitEvent = true;
}

constexpr float FPS = 25.0f;

const dai::CameraBoardSocket RGB_SOCKET = dai::CameraBoardSocket::CAM_A;
const dai::CameraBoardSocket LEFT_SOCKET = dai::CameraBoardSocket::CAM_B;
const dai::CameraBoardSocket RIGHT_SOCKET = dai::CameraBoardSocket::CAM_C;

// FPS Counter class
class FPSCounter {
   public:
    void tick() {
        auto now = std::chrono::steady_clock::now();
        frameTimes.push_back(now);
        while(frameTimes.size() > 10) {
            frameTimes.pop_front();
        }
    }

    float getFps() {
        if(frameTimes.size() <= 1) return 0.0f;
        auto duration = std::chrono::duration_cast<std::chrono::duration<float>>(frameTimes.back() - frameTimes.front()).count();
        return (frameTimes.size() - 1) / duration;
    }

   private:
    std::deque<std::chrono::steady_clock::time_point> frameTimes;
};

// Global blend weights
float rgbWeight = 0.4f;
float depthWeight = 0.6f;

// Trackbar callback
void updateBlendWeights(int percentRgb, void*) {
    rgbWeight = static_cast<float>(percentRgb) / 100.0f;
    depthWeight = 1.0f - rgbWeight;
}

int main() {
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    dai::Pipeline pipeline;

    // Create and configure nodes
    auto camRgb = pipeline.create<dai::node::Camera>();
    camRgb->build(RGB_SOCKET);
    auto left = pipeline.create<dai::node::Camera>();
    left->build(LEFT_SOCKET);
    auto right = pipeline.create<dai::node::Camera>();
    right->build(RIGHT_SOCKET);
    auto stereo = pipeline.create<dai::node::StereoDepth>();
    auto sync = pipeline.create<dai::node::Sync>();

    // Check if platform is RVC4 and create ImageAlign node if needed
    auto platform = pipeline.getDefaultDevice()->getPlatform();
    std::shared_ptr<dai::node::ImageAlign> align;
    if(platform == dai::Platform::RVC4) {
        align = pipeline.create<dai::node::ImageAlign>();
    }

    stereo->setExtendedDisparity(true);
    sync->setSyncThreshold(std::chrono::duration<int64_t, std::nano>(static_cast<int64_t>(1e9 / (2.0 * FPS))));

    // Configure outputs
    auto rgbOut = camRgb->requestOutput(std::make_pair(1280, 960), dai::ImgFrame::Type::NV12, dai::ImgResizeMode::CROP, FPS, true);
    auto leftOut = left->requestOutput(std::make_pair(640, 400), std::nullopt, dai::ImgResizeMode::CROP, FPS);
    auto rightOut = right->requestOutput(std::make_pair(640, 400), std::nullopt, dai::ImgResizeMode::CROP, FPS);

    // Link nodes
    rgbOut->link(sync->inputs["rgb"]);
    leftOut->link(stereo->left);
    rightOut->link(stereo->right);

    if(platform == dai::Platform::RVC4) {
        stereo->depth.link(align->input);
        rgbOut->link(align->inputAlignTo);
        align->outputAligned.link(sync->inputs["depth_aligned"]);
    } else {
        stereo->depth.link(sync->inputs["depth_aligned"]);
        rgbOut->link(stereo->inputAlignTo);
    }

    // Create output queue
    auto queue = sync->out.createOutputQueue();

    // Create and configure windows
    const std::string windowName = "rgb-depth";
    cv::namedWindow(windowName, cv::WINDOW_NORMAL);
    cv::resizeWindow(windowName, 1280, 720);
    cv::createTrackbar("RGB Weight %", windowName, nullptr, 100, updateBlendWeights);
    cv::setTrackbarPos("RGB Weight %", windowName, static_cast<int>(rgbWeight * 100));

    FPSCounter fpsCounter;

    // Start pipeline
    pipeline.start();

    while(pipeline.isRunning() && !quitEvent) {
        auto messageGroup = queue->get<dai::MessageGroup>();
        fpsCounter.tick();

        auto frameRgb = messageGroup->get<dai::ImgFrame>("rgb");
        auto frameDepth = messageGroup->get<dai::ImgFrame>("depth_aligned");

        if(frameDepth != nullptr) {
            cv::Mat cvFrame = frameRgb->getCvFrame();

            // Colorize depth
            cv::Mat alignedDepthColorized = dai::utility::colorizeDepthFrame(*frameDepth).getCvFrame();
            cv::imshow("Depth aligned", alignedDepthColorized);

            // Convert grayscale to BGR if needed
            if(cvFrame.channels() == 1) {
                cv::cvtColor(cvFrame, cvFrame, cv::COLOR_GRAY2BGR);
            }

            // Blend frames
            cv::Mat blended;
            cv::addWeighted(cvFrame, rgbWeight, alignedDepthColorized, depthWeight, 0, blended);

            // Add FPS text
            cv::putText(blended, "FPS: " + std::to_string(fpsCounter.getFps()), cv::Point(10, 30), cv::FONT_HERSHEY_SIMPLEX, 1, cv::Scalar(255, 255, 255), 2);

            cv::imshow(windowName, blended);
        }

        if(cv::waitKey(1) == 'q') {
            break;
        }
    }

    pipeline.stop();
    pipeline.wait();

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.