Undistort camera stream
This example shows how you can use Camera node to undistort wide FOV camera stream. Camera node will automatically undistortstill
, video
and preview
streams, while isp
stream will be left as is.Demo
Pipeline
Source code
Python
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6# Create pipeline
7with dai.Pipeline() as pipeline:
8 # Define source and output
9 cam = pipeline.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B)
10 croppedQueue = cam.requestOutput((300,300), resizeMode=dai.ImgResizeMode.CROP, enableUndistortion=True).createOutputQueue()
11 stretchedQueue = cam.requestOutput((300,300), resizeMode=dai.ImgResizeMode.STRETCH, enableUndistortion=True).createOutputQueue()
12 letterBoxedQueue = cam.requestOutput((300,300), resizeMode=dai.ImgResizeMode.LETTERBOX, enableUndistortion=True).createOutputQueue()
13
14 # Connect to device and start pipeline
15 pipeline.start()
16 while pipeline.isRunning():
17 croppedIn = croppedQueue.get()
18 assert isinstance(croppedIn, dai.ImgFrame)
19 cv2.imshow("cropped undistorted", croppedIn.getCvFrame())
20
21 stretchedIn = stretchedQueue.get()
22 assert isinstance(stretchedIn, dai.ImgFrame)
23 cv2.imshow("stretched undistorted", stretchedIn.getCvFrame())
24
25 letterBoxedIn = letterBoxedQueue.get()
26 assert isinstance(letterBoxedIn, dai.ImgFrame)
27 cv2.imshow("letterboxed undistorted", letterBoxedIn.getCvFrame())
28
29 if cv2.waitKey(1) == ord("q"):
30 break
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.