# NN Archive Superblob

The example showcases loading a YOLOv6-Nano superblob model from the model zoo, configuring a neural network node with a 416x416
RGB camera input, and processing detection and passthrough outputs.

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Pipeline

Pipeline nodes:
- Camera(0)
- NeuralNetwork (1)
- XLinkOut (4)
- XLinkOut (2)

Pipeline connections:
- NeuralNetwork (1) -> XLinkOut (4) (passthrough -> in)
- NeuralNetwork (1) -> XLinkOut (2) (out -> in)
- Camera(0) -> NeuralNetwork (1) (0 -> in)

## Source code

#### Python

```python
#!/usr/bin/env python3

import time
import depthai as dai

# We will download a blob NNArchive from the model zoo
# Pick your own model from
modelDescription = dai.NNModelDescription()
modelDescription.model = "yolov6-nano"
modelDescription.platform = "RVC2"

# Download model from zoo and load it
archivePath = dai.getModelFromZoo(modelDescription, useCached=True)
archive = dai.NNArchive(archivePath)

# Archive knows it is a blob archive
assert archive.getModelType() == dai.ModelType.SUPERBLOB

# Therefore, getSuperBlob() is available
assert archive.getSuperBlob() is not None

# There is no blob or other model format available
assert archive.getBlob() is None
assert archive.getOtherModelFormat() is None

# You can access any config version
v1config: dai.nn_archive.v1.Config = archive.getConfig()

# Print some config fields
print("-" * 10)
print("Config fields:")
print(f"\tConfig version: {v1config.configVersion}")
print(f"\tModel heads: {v1config.model.heads}")
print(f"\tModel inputs: {v1config.model.inputs}")
print(f"\tModel metadata: {v1config.model.metadata}")
print(f"\tModel outputs: {v1config.model.outputs}")
print("-" * 10)

with dai.Pipeline() as pipeline:
    # Color camera node
    camRgb = pipeline.create(dai.node.Camera).build()
    outCam = camRgb.requestOutput((416, 416), dai.ImgFrame.Type.BGR888p)

    # Neural network node
    blob = archive.getSuperBlob().getBlobWithNumShaves(6)
    neuralNetwork = pipeline.create(dai.node.NeuralNetwork)
    neuralNetwork.setBlob(blob)
    neuralNetwork.setNumInferenceThreads(2)

    # Linking
    outCam.link(neuralNetwork.input)

    nnDetectionQueue = neuralNetwork.out.createOutputQueue()
    nnPassthroughQueue = neuralNetwork.passthrough.createOutputQueue()

    pipeline.start()

    while pipeline.isRunning():
        in_nn = nnDetectionQueue.get()
        in_nnPassthrough = nnPassthroughQueue.get()
        print("Data received")
        time.sleep(0.1)
```

#### C++

```cpp
#include <atomic>
#include <chrono>
#include <csignal>
#include <iostream>
#include <memory>
#include <thread>

#include "depthai/depthai.hpp"
#include "depthai/openvino/OpenVINO.hpp"

// Global flag for graceful shutdown
std::atomic<bool> quitEvent(false);

// Signal handler
void signalHandler(int signum) {
    quitEvent = true;
}

int main() {
    // Set up signal handlers
    signal(SIGTERM, signalHandler);
    signal(SIGINT, signalHandler);

    try {
        // Get model from zoo
        dai::NNModelDescription modelDesc;
        modelDesc.model = "yolov6-nano";
        modelDesc.platform = "RVC2";
        auto archivePath = dai::getModelFromZoo(modelDesc, true);  // true to use cached if available, otherwise re-download

        // Load NN archive
        dai::NNArchive archive(archivePath);

        // Verify archive type and properties
        if(archive.getModelType() != dai::model::ModelType::SUPERBLOB) {
            throw std::runtime_error("Archive is not a superblob type");
        }

        if(!archive.getSuperBlob()) {
            throw std::runtime_error("SuperBlob should not be null for superblob type");
        }

        if(archive.getBlob()) {
            throw std::runtime_error("Blob should be null for superblob type");
        }

        // Get config and print some fields
        auto config = archive.getConfig<dai::nn_archive::v1::Config>();
        std::cout << "----------" << std::endl;
        std::cout << "Config fields:" << std::endl;
        std::cout << "\tConfig version: " << config.configVersion.value() << std::endl;
        std::cout << "\tModel heads: " << config.model.heads.value().size() << std::endl;
        std::cout << "\tModel inputs: " << config.model.inputs.size() << std::endl;
        std::cout << "\tModel outputs: " << config.model.outputs.size() << std::endl;
        std::cout << "----------" << std::endl;

        // Create pipeline
        dai::Pipeline pipeline;

        // Color camera node
        auto camRgb = pipeline.create<dai::node::Camera>()->build();
        auto camOut = camRgb->requestOutput(std::make_pair(416, 416), dai::ImgFrame::Type::BGR888p);

        // Neural network node
        auto neuralNetwork = pipeline.create<dai::node::NeuralNetwork>();
        neuralNetwork->setBlob(archive.getSuperBlob()->getBlobWithNumShaves(6));
        neuralNetwork->setNumInferenceThreads(2);

        // Linking
        camOut->link(neuralNetwork->input);

        // Create output queues
        auto qDet = neuralNetwork->out.createOutputQueue();
        auto qPassthrough = neuralNetwork->passthrough.createOutputQueue();

        // Start pipeline
        pipeline.start();

        while(pipeline.isRunning() && !quitEvent) {
            auto inDet = qDet->get<dai::NNData>();
            auto inPassthrough = qPassthrough->get<dai::ImgFrame>();

            if(inDet != nullptr) {
                std::cout << "Detection data received" << std::endl;
            }

            if(inPassthrough != nullptr) {
                std::cout << "Passthrough frame received" << std::endl;
            }

            std::this_thread::sleep_for(std::chrono::milliseconds(100));
        }

        // Cleanup
        pipeline.stop();
        pipeline.wait();

    } catch(const std::exception& e) {
        std::cerr << "Error: " << e.what() << std::endl;
        return 1;
    }

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.