DepthAI
  • DepthAI Components
    • AprilTags
    • Benchmark
    • Camera
    • Calibration
    • DetectionNetwork
    • Events
    • FeatureTracker
    • Gate
    • HostNodes
    • ImageAlign
    • ImageManip
    • IMU
    • Misc
    • Model Zoo
    • NeuralDepth
    • NeuralNetwork
    • ObjectTracker
    • PointCloud
    • RecordReplay
    • RGBD
    • Script
    • SpatialDetectionNetwork
    • SpatialLocationCalculator
    • StereoDepth
    • Sync
    • VideoEncoder
    • Visualizer
    • Warp
    • RVC2-specific
  • Advanced Tutorials
  • API Reference
  • Tools
Software Stack

ON THIS PAGE

  • Pipeline
  • Source code

Basalt VIO

Supported on:RVC2
The example creates a pipeline to capture 640x400 stereo camera frames at 60 FPS and IMU data at 200 Hz, processes them with BasaltVIO for visual odometry, and streams the resulting transformations and images to a RerunNode for real-time visualization.This example requires the DepthAI v3 API, see installation instructions.

Pipeline

Source code

Python

Python
GitHub
1import signal
2import time
3import depthai as dai
4from rerun_node import RerunNode
5# Create pipeline
6
7with dai.Pipeline() as p:
8    fps = 60
9    width = 640
10    height = 400
11    # Define sources and outputs
12    left = p.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_B, sensorFps=fps)
13    right = p.create(dai.node.Camera).build(dai.CameraBoardSocket.CAM_C, sensorFps=fps)
14    imu = p.create(dai.node.IMU)
15    odom = p.create(dai.node.BasaltVIO)
16
17    rerunViewer = p.create(RerunNode)
18    imu.enableIMUSensor([dai.IMUSensor.ACCELEROMETER_RAW, dai.IMUSensor.GYROSCOPE_RAW], 200)
19    imu.setBatchReportThreshold(1)
20    imu.setMaxBatchReports(10)
21
22    # Linking
23    left.requestOutput((width, height)).link(odom.left)
24    right.requestOutput((width, height)).link(odom.right)
25    imu.out.link(odom.imu)
26    odom.passthrough.link(rerunViewer.inputImg)
27    odom.transform.link(rerunViewer.inputTrans)
28    p.start()
29    while p.isRunning():
30        time.sleep(0.01)

C++

1#include "depthai/depthai.hpp"
2#include "rerun_node.hpp"
3
4int main() {
5    using namespace std;
6
7    // Create pipeline
8    dai::Pipeline pipeline;
9    int fps = 60;
10    int width = 640;
11    int height = 400;
12    // Define sources and outputs
13    auto left = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_B, std::nullopt, fps);
14    auto right = pipeline.create<dai::node::Camera>()->build(dai::CameraBoardSocket::CAM_C, std::nullopt, fps);
15    auto imu = pipeline.create<dai::node::IMU>();
16    auto odom = pipeline.create<dai::node::BasaltVIO>();
17
18    auto rerun = pipeline.create<RerunNode>();
19    imu->enableIMUSensor({dai::IMUSensor::ACCELEROMETER_RAW, dai::IMUSensor::GYROSCOPE_RAW}, 200);
20    imu->setBatchReportThreshold(1);
21    imu->setMaxBatchReports(10);
22
23    // Linking
24    left->requestOutput(std::make_pair(width, height))->link(odom->left);
25    right->requestOutput(std::make_pair(width, height))->link(odom->right);
26    imu->out.link(odom->imu);
27    odom->transform.link(rerun->inputTrans);
28    odom->passthrough.link(rerun->inputImg);
29
30    pipeline.start();
31    pipeline.wait();
32}

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.