Multiple Scripts Sync
Similar samples:
Demo
Command Line
1~/depthai-python/examples/Sync $ python3 sync_scripts.py
2Start
3Received s1 with timestamp 0:00:02.420089
4Received s2 with timestamp 0:00:02.461076
5Time interval between messages: 40.987ms
6----------
7Received s1 with timestamp 0:00:03.422108
8Received s2 with timestamp 0:00:03.367069
9Time interval between messages: 55.039ms
10----------
11Received s1 with timestamp 0:00:05.426088
12Received s2 with timestamp 0:00:05.481086
13Time interval between messages: 54.998ms
14----------
15Received s1 with timestamp 0:00:06.428106
16Received s2 with timestamp 0:00:06.387129
17Time interval between messages: 40.977ms
18----------Source code
Python
PythonGitHub
1import depthai as dai
2import time
3from datetime import timedelta
4
5pipeline = dai.Pipeline()
6
7script1 = pipeline.create(dai.node.Script)
8script1.setScript("""
9from time import sleep
10
11while True:
12 sleep(1)
13 b = Buffer(512)
14 b.setData(bytes(4 * [i for i in range(0, 128)]))
15 b.setTimestamp(Clock.now())
16 node.io['out'].send(b)
17""")
18
19script2 = pipeline.create(dai.node.Script)
20script2.setScript("""
21from time import sleep
22
23while True:
24 sleep(0.3)
25 b = Buffer(512)
26 b.setData(bytes(4 * [i for i in range(128, 256)]))
27 b.setTimestamp(Clock.now())
28 node.io['out'].send(b)
29""")
30
31sync = pipeline.create(dai.node.Sync)
32sync.setSyncThreshold(timedelta(milliseconds=100))
33
34xout = pipeline.create(dai.node.XLinkOut)
35xout.setStreamName("xout")
36
37sync.out.link(xout.input)
38
39script1.outputs["out"].link(sync.inputs["s1"])
40script2.outputs["out"].link(sync.inputs["s2"])
41
42# script1.outputs["out"].link(xout.input)
43
44with dai.Device(pipeline) as device:
45 print("Start")
46 q = device.getOutputQueue("xout", maxSize=10, blocking=True)
47 while True:
48 grp = q.get()
49 for name, msg in grp:
50 print(f"Received {name} with timestamp {msg.getTimestamp()}")
51 print(f"Time interval between messages: {grp.getIntervalNs() / 1e6}ms")
52 print("----------")
53 time.sleep(0.2)How it Works
- Initialize a DepthAI pipeline.
- Create two Script nodes, each generating and sending data buffers at different intervals.
- Set up a Sync node with a synchronization threshold.
- Link the outputs of the Script nodes to the Sync node.
- Start the pipeline and continuously receive synchronized data from the Script nodes.
- Print the received data along with timestamps and the interval between messages.
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.