Build from Source
Install dependencies
Command Line
1sudo wget -qO- https://raw.githubusercontent.com/luxonis/depthai-ros/main/install_dependencies.sh | sudo bashsudo apt install libopencv-devif you don't have rosdep installed and not initialized please execute the following steps:Command Line
1sudo apt install python3-rosdep
2sudo rosdep init
3rosdep updateSetting up procedure
dai_ws as the name for a new folder, as it will be our depthai ros workspace.Command Line
1mkdir -p dai_ws/src
2cd dai_ws/src
3git clone --branch kilted https://github.com/luxonis/depthai-ros.git
4cd ..
5rosdep install --from-paths src --ignore-src -r -y
6source /opt/ros/$ROS_DISTRO/setup.bash
7MAKEFLAGS="-j1 -l1" colcon build
8source install/setup.bashIf you are using a lower end PC or RPi, standard building may take a lot of RAM and clog your PC. To avoid that, you can use
build.sh command from your workspace (it just wraps colcon commands):Command Line
1./src/depthai-ros/build.shDocker
Building
Command Line
1docker build --build-arg USE_RVIZ=1 -t depthai-ros .BUILD_SEQUENTIAL=1 to build packages one at a time, it should take longer, but use less RAM.RUN_RVIZ arg means rviz will be installed inside docker. If you want to run it you need to also execute following command (you'll have to do it again after restarting your PC):Command Line
1xhost +local:dockerCommand Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai-rosCommand Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai-ros [CMD]- bash (it will allow you to browse files and make modifications to the code and rebuild it)
- zsh (other shell that is installed that has some advantages over bash)
- roslaunch depthai_ros_driver camera.launch (this is just an example, any launch file will work here) A side note here, launch files in depthai_ros_driver have some default parameters set by .yaml files inside the driver. You can either edit them inside the container itself, or you can make a .yaml file on your host (let's say
/home/YOUR_USERNAME_HERE/params/example_config.yaml) and pass it as an argument to the executable, as follows:
Command Line
1docker run -it -v /dev/:/dev/ -v /home/YOUR_USERNAME_HERE/params:/params --network host --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai-ros ros2 launch depthai_ros_driver driver.launch.py params_file:=/params/example_config.yaml- Install it by running the container in bash/zsh mode
- Modify the Dockerfile so that it's installed during building - you'll have to rebuild the container after that.
- Run base camera node in our container and RTABMap separately on host/ in a separate container (see the launch file on what parameters/topic names need to be changed when running separately).