# Base Image (oakapp-base)

The base image is a minimal Docker image that provides the necessary environment for running complex OAK4 Apps. It includes Python
3.12 and other essential libraries, allowing developers to build and deploy applications on OAK4 cameras. Key components of the
base image include:

 * `nginx` - a proxy used to serve static files or handle requests to the app's frontend. It exposes both the DAI WebSocket and
   the frontend on the same port. This is important, especially for access via IP address. Encoded streams are available only via
   HTTPS, and the only way to enable HTTPS for device access via IP is to use a self-signed certificate. Browsers allow only one
   self-signed certificate per IP, so `nginx` creates a reverse proxy for the frontend and DAI WebSocket, which internally run on
   different ports but must be publicly exposed on a single port with one certificate.
 * `oak_webrtc` - a tool for WebRTC communication, used to provide remote access to the app via the `*.luxonis.app domain`. It
   uses WebRTC to establish a connection between the app and the viewer, allowing for real-time streaming of video and other data.
   It can connect directly on a local network and should handle up to 400 Mbps throughput when network capacity allows.
   Communication via WebSocket is limited by browser performance and network bandwidth, but it can handle 1 Gbps+ without issues.
 * `python 3.12` - Python is used for the backend of the app, which utilizes DAI v3. Please note that DAI itself is installed in
   the application; an example of requirements file is here:
   [requirements.txt](https://github.com/luxonis/oak-examples/blob/main/custom-frontend/open-vocabulary-object-detection/backend/requirements.txt).

# Examples

## Default App

You can check it in this definition [oakapp.toml](https://github.com/luxonis/oak-examples/blob/main/apps/default-app/oakapp.toml).
Key parts are as follows:

```toml
identifier = "com.example.apps.default-app"
entrypoint = ["/entrypoint.sh", "python3", "-u", "/app/main.py"]
app_version = "1.1.0"
assign_frontend_port = true
```

 * `identifier` - the name of the app in Java-like format (with dots as separators). Please note that the identifier must be
   unique in the Hub, so it is recommended to use your team name as a prefix.
 * `entrypoint` - an array of strings (a command in argv format). This is the command executed when the app starts. The base
   image's `/entrypoint.sh` starts its supporting services and runs the supplied backend command, `python3 -u /app/main.py`.
   Passing the backend command to `/entrypoint.sh` allows the app to shut down gracefully when stopped.
 * `app_version` - the version of the app. It is recommended to use semantic versioning.
 * `assign_frontend_port` - if true, the app will be assigned a frontend port, which is then used by the internal `nginx` server
   to serve the frontend files. If false, the app will not get a frontend port assigned and will not be able to serve any frontend
   files on the standard port. The agent running on OAK4 handles port assignment, and a unique port is assigned to each app, so it
   is not necessary to specify the port in the `oakapp.toml` file.

```toml
prepare_container = [
    { type = "COPY", source = "./requirements.txt", target = "./requirements.txt" },
    { type = "RUN", command = "python3.12 -m pip install -r /app/requirements.txt --break-system-packages"}
]
```

This section defines the steps to prepare the container for the application. It includes copying the `requirements.txt` file into
the container and installing the required Python packages using `pip`. This ensures that all necessary dependencies are available
when the application starts. Additionally, it guarantees that dependencies are installed only once or as needed when the `oakctl
app run` command is executed.

```toml
[base_image]
api_url = "https://registry-1.docker.io"
service = "registry.docker.io"
oauth_url = "https://auth.docker.io/token"
auth_type = "repository"
auth_name = "luxonis/oakapp-base"
image_name = "luxonis/oakapp-base"
image_tag = "1.3.0"
```

> **Note**
> Starting from Luxonis OS 1.40.0, the preferred way of specifying a custom base image is the new compact syntax:

```toml
base_image = "luxonis/oakapp-base:1.3.0"
```

You can use any Docker image (supporting ARM64 architecture if you are running apps on OAK4) as a base for your application, but
it is recommended to use the `luxonis/oakapp-base` image, as it is specifically designed for OAK4 Apps and includes all necessary
dependencies and configurations.

The backend source is [main.py](https://github.com/luxonis/oak-examples/blob/main/apps/default-app/main.py), launched by the
`entrypoint` command above. Python is included in the base image, so it is not necessary to install it again.

## Open Vocabulary Object Detection

This is a more complex example that uses all features. The app definition is available here:
[oakapp.toml](https://github.com/luxonis/oak-examples/blob/main/custom-frontend/open-vocabulary-object-detection/oakapp.toml). Key
differences from the previous example are:

```toml
entrypoint = ["/entrypoint.sh", "python3", "-u", "/app/backend/src/main.py"]
prepare_build_container = [{type = "RUN", command = "bash -c 'curl -o- https://raw.githubusercontent.com/nvm-sh/nvm/v0.40.3/install.sh | bash && . \"$HOME/.nvm/nvm.sh\" && nvm install 24'"}]

[static_frontend]
dist_path = "./frontend/dist"

[static_frontend.build]
source_path = "./frontend"
steps = ["bash -c 'cd /app/frontend/src && export NODE_OPTIONS=--max-old-space-size=4096 && . $HOME/.nvm/nvm.sh && npm install && npm run build'"]
```

Instead of the Visualizer, which is part of DAI and used in the previous example, this example uses a custom frontend built with
React.js. It uses `nvm` to install Node.js version 24 and then builds the frontend application. The frontend build is performed in
the `static_frontend.build` section, where `npm` is used to install dependencies and build the application. This build is
performed on the device as well, so running `oakctl app run .` is enough to build the entire app, including the frontend.

 * `dist_path` - the path to the built frontend application; this is where the built files are located after the build process is
   finished. It is recommended to follow the structure in this example, with one folder for the backend and another for the
   frontend. This is not required, but it helps keep the structure clean and organized.
 * `source_path` - the path to the source code of the frontend application; this is where the source code is located before the
   build process starts.
 * `steps` - an array of strings, each representing a command that will be executed in the container to build the frontend
   application. In this case, `npm` is used to install dependencies and build the application. The `NODE_OPTIONS` environment
   variable is set to increase the memory limit for Node.js, helping to avoid out-of-memory errors during the build process. The
   frontend uses the React.js library `@luxonis/depthai-viewer-common`, which provides high-level components for rendering streams
   and annotations, and enables communication with the backend using WebSocket for direct access and WebRTC for remote access via
   the `*.luxonis.app domain`.