# Configuration (oakapp.toml)

Within each app's directory, there must be a `oakapp.toml` file that contains static app's metadata and build steps. Metadata
includes the app's identifier and version. Build steps are commands that are executed in the container to build or run the app.
Example `oakapp.toml` file:

```toml
# (Required) App Identifier
identifier = "com.luxonis.python_demo"
# (Required) App Entrypoint
entrypoint = ["bash", "-c", "python3 /app/main.py"]

# (Optional) Prepare container commands
# Here is the place where you can install all the dependencies that are needed at run-time
prepare_container = [
    { type = "COPY", source = "requirements.txt", target = "requirements.txt" },
    { type = "RUN", command = "apt-get update" },
    { type = "RUN", command = "apt-get install -y python3-pip" },
    { type = "RUN", command = "pip3 install -r /app/requirements.txt --break-system-packages" },
]

# (Optional) Prepare build dependencies
# Here is the place where you can install all the dependencies that are needed at build-time
prepare_build_container = [
    # Example: npm, gcc, ...
]

# (Optional) Additional commands after all the app files are copied to the container
build_steps = []
```

## Configuration Fields

### App Metadata

 * `identifier` - name of the app in Java-like format (with dots as separators; e.g., `com.my_company.my_app`) * `com.luxonis`
   namespace is reserved for official apps
    * `com.example` namespace is not recommended for production apps
 * `app_version` - version of the app in format `major.minor.patch` (e.g., `1.0.0`)

### App Build and Runtime Configuration

 * `entrypoint` - array of strings (a command in argv format)
 * `cwd` - (optional, default is `/` ) current working directory for the container
 * `shell` - (optional, default is `["/bin/bash", "-c"]` ) shell to use for executing `build_steps`, `entrypoint`, and `RUN`
   commands in `prepare_container` and `prepare_build_container` sections
 * `app_dir_name` - (optional/advanced, default is `app` ) directory inside the container where the app files are copied; use only
   if you already use this directory name for something else
 * `stop_grace_period` - (optional, default is `10s`) time duration to be used as a grace period during any `app stop` operation;
   `oak-agent` tries to stop apps by sending a `SIGTERM` first, and only after the grace period has passed a `SIGKILL` issued if
   the app is still running
 * `restart_policy` - (optional, default is `never`) controls whether `oak-agent` restarts the app after its process exits

> **Shell Form vs Executable Form**
> Similarly to Docker, all the commands can be specified in executable form (array of strings) or in shell form (single string). For `entrypoint` we strongly recommend using executable form.

> **Termination signal handling**
> Similarly to most container runtimes, the process running inside an app container is responsible for correctly handling `SIGTERM`.

### Automatic App Restart

Use `restart_policy` to recover an app automatically when its process exits.

```toml
restart_policy = "on-failure:3"
```

| Value | Behavior |
| --- | --- |
| `never` | Do not restart the app automatically. This is the default. |
| `always` | Restart the app after every exit, including a successful exit. |
| `on-failure` | Restart the app after an unsuccessful exit, with no retry limit. |
| `on-failure:<count>` | Restart the app at most `<count>` times after unsuccessful exits. |

### App Layers

Similar to Docker, an app is built in multiple layers:

 1. Base Image layer (specified in `base_image` section)
 2. Runtime layer (built in `prepare_container` section)
 3. Build layer (built in `prepare_build_container` section; this layer is disconnected from runtime layer after build)
 4. App layer (all the files from the app's directory and the `build_steps` are executed here)

> **Note**
> In Docker terminology, each of these layers corresponds to a single `RUN` instruction in a Dockerfile. This allows for efficient caching while avoiding common pitfalls.

Next to App layer, there are two additional parallel layers:

 * Static Frontend layer (if specified in `static_frontend` section)
 * DepthAI Models Cache layer (if specified in `depthai_models` section)

If any of these layers change, all the subsequent layers are rebuilt. Parallel layers are rebuilt independently of each other as
they do not have mutual dependencies.

#### Base Image

The default base image is `debian/bookworm-slim`, pulled from `registry-1.docker.io`. It can be changed by specifying the
`base_image` field, several formats are supported:

```toml
base_image = "debian:bookworm-slim" # Default
base_image = "luxonis/oakapp-base:1.2.5"
```

> **Recommendation**
> For DepthAI OAK Apps, we recommend our [Base Image](https://docs.luxonis.com/software-v3/oak-apps/base-image.md) that includes most of the dependencies you may need.

#### Using a Custom Base Image

If you already develop with Docker, you can reuse that work in OAK Apps by pointing `base_image` to your own image. This is useful
when you want to iterate on OS packages, runtimes, or shared dependencies in a familiar Docker workflow first, and then package
the final app with `oakapp.toml`.

This can also be a good fit when you are developing a reusable base environment and want to share it across multiple apps. Use a
custom base image for stable, shared environment setup, and use `prepare_container` and `prepare_build_container` for app-specific
runtime and build steps.

To use a different image as the base layer, define it in `oakapp.toml` like this:

```toml
base_image = "your-org/your-image:tag"
```

By default, images are pulled from Docker Hub, but you can also point `base_image` to a different registry:

```toml
base_image = "ghcr.io/your-org/your-image:tag"
```

If you want to use a base image from a private repository, you can authenticate within `oakctl`:

```sh
oakctl registry login <registry_url>
```

Credentials are stored securely in the system keyring and never leave the machine where `oakctl registry login` is run on. When
performing an image pull, a short-lived authentication token is generated by the registry using the stored credentials, then such
token is the only auth info that is transferred to the device.

Once authentication is no longer necessary, credentials can be cleared with:

```sh
oakctl registry logout <registry_url>
```

> **Docker Hub unauthenticated pulls**
> `oak-agent` does unauthenticated pulls from image registries by default. After repeated pulls, or when building from a shared network, registries such as Docker Hub may reject the request because of their anonymous pull rate limit. If that happens, the build can fail with an error similar to this:

```sh
oakctl command failed:
   0: Received an error RPC response: Failed to build application container:
      Image download failed: OCI registry client received an error:
      APIError(ErrorList { errors: [Error { code: "TOOMANYREQUESTS", message:
      "You have reached your unauthenticated pull rate limit.
      https://www.docker.com/increase-rate-limit", detail: Null }] })
```

To avoid this, either use `oakctl registry login` or see [Self-Hosting a Container
Registry](#Self-Hosting%20a%20Container%20Registry).

#### Self-Hosting a Container Registry

To avoid Docker Hub rate limits, you can self-host a container registry and point `base_image.api_url` to it during development.

Run a registry that is reachable from the device:

```bash
docker run --rm -d -p 5000:5000 --name registry registry:2
```

Build and push an image to the local registry:

```sh
echo "FROM ubuntu:26.04" > ./Dockerfile
docker buildx build --platform linux/arm64 -t myapp-base:latest --load .
docker tag myapp-base:latest localhost:5000/myapp-base:latest
docker push localhost:5000/myapp-base:latest
```

Use the base image in the oakapp. Add the `base_image` field in `oakapp.toml` like this:

```toml
base_image = "http://registry-ip:5000/your-image:tag"
```

Keep in mind that the app is built on the device, so the registry must be accessible from the device. The API URL has to point to
the device's network-accessible address. For the uploaded image to work on an OAK4 device it has to be uploaded as a linux/arm64
image.

#### Runtime And Build Layer

Both `prepare_container` and `prepare_build_container` are arrays of commands that are executed in the container to prepare the
respective layers. The only difference is that the build layer is not present at runtime.

The available command types are:

 * `RUN` - run a command in the container

```toml
prepare_container = [
    { type = "RUN", command = "apt-get update" },
    { type = "RUN", command = "apt-get install -y python3-pip" },
]
```

 * `COPY` - copy a file from the app's directory to the container sooner than in the App layer. This is useful for copying
   dependency files like `requirements.txt`. It is not necessary to copy the actual app files here, as they are copied later in
   the App layer. * `source` - path to the source file relative to the app's directory on the host
    * `target` - path to app directory inside the container (relative to `app_dir_name` if specified)

```toml
prepare_container = [
    { type = "COPY", source = "requirements.txt", target = "requirements.txt" },
]
```

#### App Layer

First, all the files from the app's directory are copied to the container (into `app_dir_name` if specified). Then, the commands
in `build_steps` are executed in order.

 * `build_steps` - steps to build an application or other preparation commands to be executed (array of strings)

```toml
build_steps = [
    "g++ -o /app/my_app /app/main.cpp",
    "chmod +x /app/my_app",
]
```

You can ignore files from being copied to the container by adding a `.oakappignore` file to your app's directory. The syntax is
similar to `.gitignore`. Example:

```plaintext
# Ignore all .log files
*.log
# Ignore node_modules/ directory
node_modules/
```

### Mounts

Mounts allow you to link directories or devices from the device running the app into the app's container. You cannot mount
directories from the host this way. Mounts that are required must be present at both build time and run time.

 * `required_mounts`, `required_devices` - mounts that are required - if not present on startup of container, the app is stopped
   with error

Syntax is `source[:target[:options]]`; defaults:

 * source=target
 * options="rbind,rw"
 * All mount paths must be absolute. Relative paths are rejected for `required_mounts`, `required_devices`, `optional_mounts`,
   `optional_devices`, and `additional_mounts` (`source`/`target`).

Example:

```toml
required_mounts = [
    "/data/my-storage:/app/storage:rw,rbind",
]
```

 * `optional_mounts`, `optional_devices` - if not present of startup of container, these mounts are ignored
 * `additional_mounts` ( `source` , `target` , `type` , `options` , `required` ) array of objects, see below for example:

```toml
additional_mounts = [
    { source = "/run/user/1000/pulse", target = "/run/user/1000/pulse", type = "none", options = [
        "rbind",
        "rw",
    ], required = true },
    { source = "/home/root/.config/pulse/cookie", target = "/root/.config/pulse/cookie", type = "none", options = [
        "bind",
        "ro",
    ], required = true },
]
```

 * `additional_build_mounts` - same as `additional_mounts`, but only for build time; these mounts are not present at runtime

#### Device access

Individual device nodes listed in `required_devices` and `optional_devices` automatically receive read, write, and mknod (`rwm`)
permissions. Duplicate device source paths or container target paths are rejected.

For example, forward a serial device into the container:

```toml
required_devices = ["/dev/ttyUSB0:/dev/serial0"]
```

Use `optional_devices` when the app can start without the device. Optional entries that are missing at startup are skipped.

`allowed_devices` controls device permissions independently of mounts. Explicit rules are applied after the automatic grants, so
they can restrict access. Each entry in `allowed_devices` requires an explicit `allow` (`true` or `false`); `access` defaults to
`rwm` and can contain `r` (read), `w` (write), and `m` (mknod).

Select a device by its absolute path on the device running the app:

```toml
required_devices = ["/dev/ttyUSB0:/dev/serial0"]
allowed_devices = [
    { path = "/dev/ttyUSB0", allow = false, access = "wm" },
]
```

This example mounts the device at `/dev/serial0` and restricts it to read access. The `path` in an access rule always refers to
the host device path, even when its container target differs.

A path rule must refer to a character or block device. Set `optional = true` to skip the rule with a warning when that path is
missing at startup:

```toml
optional_devices = ["/dev/ttyUSB0"]
allowed_devices = [
    { path = "/dev/ttyUSB0", optional = true, allow = true, access = "rw" },
]
```

A skipped rule is not applied automatically if the device appears later. `optional` is only valid with `path`.

Alternatively, select devices by `type` (`c` for character devices, `b` for block devices, or `a` for all devices), `major`, and
`minor`. Major and minor numbers accept an integer or `"*"`:

```toml
allowed_devices = [
    { type = "c", major = 189, minor = "*", allow = true, access = "rw" },
]
```

Do not combine `path` with `type`, `major`, or `minor`. Access rules grant permissions; they do not mount a device into the
container. Use `required_devices` or `optional_devices` to make the device node available there.

> **Tip: Mount the entire /dev directory**
> To expose all device nodes to your app, mount `/dev` with `required_mounts` and allow access to all device types and numbers:

```toml
required_mounts = ["/dev:/dev:rw,rbind"]
allowed_devices = [
    { type = "a", major = "*", minor = "*", allow = true, access = "rwm" },
]
```

This grants the app read, write, and mknod access to all devices on the host. Prefer individual device mounts and access rules
when your app only needs specific devices.

### Static frontend

Static frontend layer allows you to build and serve a static web frontend alongside your app. See [example on
GitHub](https://github.com/luxonis/oak-examples/blob/main/custom-frontend/open-vocabulary-object-detection/oakapp.toml).

 * `static_frontend` * `dist_path` - path to the built frontend files (relative to the app's directory on the host) * `build`
   (optional) - build configuration for the frontend * `source_path` - path to the frontend source files
          * `steps` - array of commands to build the frontend

```toml
[static_frontend]
dist_path = "./frontend/dist" # path to the built frontend files

[static_frontend.build]
source_path = "./frontend" # path to the frontend source files
steps = ["cd /app/frontend/src && npm install && npm run build"]
```

 * `assign_frontend_port` - if set to true, an available port will be assigned to `OAKAPP_STATIC_FRONTEND_PORT` environment
   variable inside the container; this can be used even if `static_frontend` is not specified

```toml
assign_frontend_port = true
```

 * `static_frontend_dir_name` (optional/advanced; default is `static_frontend`) - directory inside the container where the static
   frontend files are mounted (will be stored in `OAKAPP_STATIC_FRONTEND_PATH` environment variable); use only if you already use
   this directory name for something else

### DepthAI Models Cache

This section allows you to specify a folder with DepthAI models in `*.yaml` format that will be cached inside the container during
build time. This way, you can create apps that work offline without the need to download models at runtime.

 * `depthai_models` * `yaml_path` - path to the DepthAI models folder in `*.yaml` format
    * `use_only_cache` - if set to true, only the cached models will be used, and no new models will be downloaded at runtime
      (sets `DEPTHAI_ZOO_INTERNET_CHECK` environment variable)

```toml
depthai_models = { yaml_path = "./backend/src/depthai_models" }
```

 * `depthai_models_dir_name` (optional/advanced; default is `depthai_models`) - directory inside the container where the DepthAI
   models are mounted; use only if you already use this directory name for something else

### Environment Variables and Build Arguments

Environment variables are set for runtime only.

```toml
[env]
MY_ENV_VAR = "some_value"
ANOTHER_ENV_VAR = "another_value"
```

Build arguments are set only during build time and are not available at runtime.

```toml
[arg]
MY_BUILD_ARG = "some_build_value"
ANOTHER_BUILD_ARG = "another_build_value"
```

Both environment variables and build arguments have lower precedence than the variables set by the user in command line (`oakctl
app run --env MY_ENV_VAR=value`).